Just 12.5 mm wide, the repeater power supply and input isolation amplifier MCR-Ex-SL RPSSI-2I belonging to the MACX Analog Ex product line of Phoenix Contact can be used to simultaneously supply two logic units with a 0/4…20 mA analog signal from a hazardous zone. This is HART compatible.
Monthly Archives: October 2011
Phoenix Contact Datalogger+ – The Choice is YOURS!
From |Public utilities and refuse disposal plants are usually equipped with numerous external stations that must be connected to a central control system. In the case of water management for example, these are pumping stations, rainwater overflow tanks, wells or even complete system plants such as sewage treatment plant and waterworks.
White Paper: Wireless Solutions in Automation
From |So do you want to reduce installation, assembly and maintenance costs? Then convince yourself of highly efficient communication solutions based on wireless signal transmission.
Lake Level Monitoring at Bishan Park via SMS
From |Bishan Park with it’s attractive lakes and bridges, colourful shrubs and lush greenery, is one of the largest and most popular parks in Singapore. Complete with cycling and running tracks and a delightful playground, it appeals to sports enthusiasts and children with boundless energy.
Beautiful lakes and shaded lawns offer some of the best scenic spots for picnics and family gatherings. Other features of the park include a Garden Spa, community gardens, an inline skates rental outlet and several F&B outlets.
Photovoltaic Plug Connector Featuring a Large Conductor Cross-Section
From |The custom-assembly Sunclix plug connector (available up to 16 mm²) from Phoenix Contact makes it possible to contact conductor cross-sections from 6 mm² to 16 mm².
It was developed to answer the needs of ever-larger PV units in which the distance between module or string and the generator junction boxes or inverters is steadily increasing. Conductors with a large cross-section are required to minimize the transfer loss in the solar cable.
Fast Compact Controller with Integrated Ethernet Interface
From |As a result of the integrated floating-point unit for quickly processing floating point numbers, the ILC 190 ETH 2TX controller from Phoenix Contact is especially suitable for fast closed-loop controls and basic motion applications. It can also be used for large applications thanks to its 1MB program memory.
Gigabit Modular Switch Now with Routing Function
From |The Gigabit Modular Switch from Phoenix Contact now also supports the layer 3 function in order to route communications between individual subnetworks.
As industrial networks are becoming increasingly more complex, it makes sense to segment them and split them up into different networks in order to secure the appropriate level of data availability.
Industrial PC Becomes a Control System
From |Now, a standard industrial PC can handle any control task. The PC Worx RT Basic software PLC from Phoenix Contact transforms any industrial PC into a fully fledged control system. Programming, visualization, and control can therefore be combined in just one device.
Junction Box for Crystalline or Thin-Film Photovoltaic Modules
From |The new photovoltaic module junction boxes from Phoenix Contact for crystalline or thin-film photovoltaic modules have been developed to supplement the Sunclix product range at the module interface.
Our developers paid special attention to automation and process safety. Using the junction boxes contributes to the optimization of module production processes.
Terminal Blocks for 1000-V DC Applications in the Photovoltaic Sector
From |The new STME 6-DIO HV compact spring cage diode terminal from Phoenix Contact protects thin-film modules against back currents. The diode terminals with 5 A and a cut-off voltage of 100 V DC are especially suited to photovoltaic applications.