The portfolio of Lean Managed Switches from Phoenix Contact’s Factory Line range of products has been expanded to include several types of switches that are preset for Ethernet/IP.
Efficient Setpoint Output via Compact Automation Terminals
From |With its narrow design, the analog Inline terminal IB IL AO 2/UI-PAC from Phoenix Contact is a compact alternative for outputting current and voltage signals. This analog terminal is just 12 mm wide, has two channels, and offers precision and performance at an affordable price.
Industrial-Grade Operator Panels for Basic Applications
From |Phoenix Contact rounds out its range of web-based operator panels with 10- and 15-inch versions. This means that more display area is available for visualizing basic applications.
The larger display area has the advantage that fewer process diagrams have to be configured to display all operating data. For operator panels with small displays, information is distributed across various process diagrams.
Fiber Optic Patch Cables with High Flexibility
From |Phoenix Contact is expanding its glass fiber optics product line to include the M12 circular plug connector. Now it is possible to fit indoor, flex and outdoor cables in variable lengths with all available connectors. In addition to our standard products, we also offer customized solutions tailored to our customers’ individual requirements.
Fast Profibus Extender with Surge Protection
From |The new Profibus extender from Phoenix Contact enables straightforward integration of remote Profibus devices at data rates of up to 1.5 Mbps. The extender has two DSL connections per device. This means that in addition to point-to-point connections the extender can also be used to easily establish line structures with up to 30 devices.
I/O Communication Terminal Integrates Profibus Devices
From |The IB IL PB-MA-PAC inline I/O communication terminal now enables the integration of Profibus devices into the Phoenix Contact automation solution.
A Visit to Newater
From |30th Nov 2011 marks a special and important day for Phoenix Contact (SEA) Pte Ltd. What is so important and special? Hear this, we hosted 4 VIPs from Germany who are, Mr Frank Stuehrenberg, our Executive Board Member, Mr Ulrich Leidecker, our General Manager of Phoenix Contact Deutschland GmbH, Mr Hanno Hardt, Director Media of publish-industry, Mr Thomas Rilke, Director Metropolitan Solutions at Singapore Newater Visitor Center.
Case Study: Malaysia Water Authority (Selangor)
From |Malaysia has experienced substantial economic development since the 1980s, resulting in increasing water demands in the commercial and industrial development centres. The Selangor / Kuala Lumpur region which is the political, commercial and industrial centre of the nation is the most important focus for these high demands which are expected to continue their rapid growth into the 21st century.
Acquiring, Monitoring, and Communicating Energy Data
From |With the Basic and Flex energy data loggers, Phoenix Contact is offering package solutions that contain all components users require for configuring a data acquisition system. The packages are based on standard industrial components with integrated GSM/GPRS modem.
Thanksgiving Meals-On-Wheels
From |My hero Warren Buffett has been promoting philanthropy these two years and I was very happy to be given the opportunity to do my bit for society with Phoenix Contact!