Two active Quint Oring redundancy modules are new in the Phoenix Contact product range. They increase the operational reliability by monitoring the redundant power supply solution from the output voltages of the power supplies through the power supply wiring up to the load, as well as the decoupling section up to the load current.
Preassembled RJ45 Patch Cable for Profinet
From |Phoenix Contact has now developed an RJ45 crimp connector for Profinet. Profinet cables with conductor cross sections of AWG 22 can be used as preassembled patch cables when using this connector.
Intelligent Uninterruptible Power Supply for the Control Cabinet
From |A new generation of uninterruptible power supplies now supplements the Quint Power product family from Phoenix Contact. Five new modules that can be snapped onto mounting rails are now available: For 24 V loads, the Quint UPS-IQ uninterruptible power supply has output currents of 5, 10, 20, and 40 A – and for loads with an input voltage of 85 up to 264 V AC, the Quint UPS-IQ supplies an output power of 500 VA.
Cost-Optimized Telecontrol
From |For data transfer via GPRS, Phoenix Contact offers Open Data Port (ODP), an intelligent solution to monitor and manage telecontrol stations. The advantages of this solution lie in the reliable data transfer, the use of standard PLC and modem components, as well as standard industrial interfaces and protocols.
Intrinsically Safe Isolation Amplifier with Two Electrically Isolated Outputs
From |Just 12.5 mm wide, the repeater power supply and input isolation amplifier MCR-Ex-SL RPSSI-2I belonging to the MACX Analog Ex product line of Phoenix Contact can be used to simultaneously supply two logic units with a 0/4…20 mA analog signal from a hazardous zone. This is HART compatible.
Phoenix Contact Datalogger+ – The Choice is YOURS!
From |Public utilities and refuse disposal plants are usually equipped with numerous external stations that must be connected to a central control system. In the case of water management for example, these are pumping stations, rainwater overflow tanks, wells or even complete system plants such as sewage treatment plant and waterworks.
White Paper: Wireless Solutions in Automation
From |So do you want to reduce installation, assembly and maintenance costs? Then convince yourself of highly efficient communication solutions based on wireless signal transmission.
Lake Level Monitoring at Bishan Park via SMS
From |Bishan Park with it’s attractive lakes and bridges, colourful shrubs and lush greenery, is one of the largest and most popular parks in Singapore. Complete with cycling and running tracks and a delightful playground, it appeals to sports enthusiasts and children with boundless energy.
Beautiful lakes and shaded lawns offer some of the best scenic spots for picnics and family gatherings. Other features of the park include a Garden Spa, community gardens, an inline skates rental outlet and several F&B outlets.
Photovoltaic Plug Connector Featuring a Large Conductor Cross-Section
From |The custom-assembly Sunclix plug connector (available up to 16 mm²) from Phoenix Contact makes it possible to contact conductor cross-sections from 6 mm² to 16 mm².
It was developed to answer the needs of ever-larger PV units in which the distance between module or string and the generator junction boxes or inverters is steadily increasing. Conductors with a large cross-section are required to minimize the transfer loss in the solar cable.
Fast Compact Controller with Integrated Ethernet Interface
From |As a result of the integrated floating-point unit for quickly processing floating point numbers, the ILC 190 ETH 2TX controller from Phoenix Contact is especially suitable for fast closed-loop controls and basic motion applications. It can also be used for large applications thanks to its 1MB program memory.