The M12 hybrid connector from Phoenix Contact is the first hybrid connector in the market with a compact design fit to address industrial applications.
Category Archives: Device Connectors
Connection Concepts for Pre-Assembled Encoders
From |Phoenix Contact presents a complete product line that offers new connection concepts to address the requirements of the new encoder generation. The two-part modular system comprises the M12 connection block and a rectangular flange. The dimensions of the rectangular flange are harmonized with the existing rotary encoder housings, so that encoder manufacturers do not have to redesign their devices.
600V Power Connector with UL Approval
From |Suitable for the ME and ME MAX family of housings from Phoenix Contact, and in addition to the classic plug connections for 250 V, the GMSTBO 2.5 HV high-power base strips with matching GMSTBT 2.5 HV screw plugs are now available for compact device applications in the area of power electronics.
Double-Level Plug Connectors for Many Connections in Restricted Spaces
From |The low-profile double-level DFMC/DMC plug connector system from Phoenix Contact allows up to 40 connections to be established in a small space.
Reliable Outdoor Cabling
From |Phoenix Contact is offering a new line of signal and data plug connectors that can be used outdoors.
Continue reading
Keep Cool!
From |Its January and this is probably the only month in Singapore that we do see much of the Sun. I am starting to miss the warmth from the sunlight.
I don’t think much of us would enjoy the scorching sun in the month of March and April either. However, as much as projects goes, installation of the Solar panels takes place all year round.
Home Fix-it: Cable Extension with Phoenix Contact QUICKON Connectors
From |Good day!
Have you been faced with a situation in which you needed to extend your cable length without having to replace your existing one? This situation is quite common especially for customers in the machine building and material handling industry.
Taking into consideration that industrial standards require joints to be water- and dust-proof, the very thought of replacing a short cable and re-laying it with a longer cable can seem daunting. Not only is it a waste of material , it is also a waste of time which equates to significant cost over time.
I would like to share my personal hands-on experience with you. Two years ago, after moving into my new apartment, I was faced with a need to extend the wire for my fan as the wire given by the manufacturer was too short . At the same time I needed it to be water-proof, as I wanted to ensure that water did not seep into the joint when the floor was being mopped.

As I had a couple of samples on my hand and I decided to use a Phoenix Contact QUICKON cable connector.
With the clearly written instructions from the manual that came with the standard package, I managed to join the two cables in less than five minutes. Sharing similar concerns as any of our customers would have, more skeptical of my own technical skills than of the insulation displacement technology, I turned on the fan and voila. The power flowed flawlessly and I was enjoying the breeze from the fan, bringing a smile to my face.
httpv://www.youtube.com/watch?v=M3YudXpogZ0
Till date I am still enjoying the cool breeze from my fan, powered by Phoenix Contact. Maybe it is about time to do another home project, how about a smart home system with the touch panel and controllers?