Category Archives: Device Connectors

electronica 2014: World’s leading trade fair

From |

electronica 2014: World’s leading trade fair

 

images (4)

 

 

 

This unique industry event presents the state of the art in innovative electronics – a diverse range of components, pioneering hardware and software solutions and complete systems and applications – on 143,000 m² of exhibition space.

It all revolves around the latest hot topics such as electromobility, energy effciency and sustainability.

Continue reading

Push-In Technology – Closer than You Think!

From |

Push-In Technology was developed by Phoenix Contact in 1978. The very first modular terminal block, the FK 1,5 with a direct plug-in spring connection, designed to offer installation engineers an easy and safe conductor connection method used this technology.

Due to its handling and compact design, the FK 1,5 is still found in elevator engineering, machine and system construction even today! Just like the FK 1,5, the concept of Push in Technology still exists and is going strong today – because it improves the way we do things…. even in our daily lives!

Read on to find out how.

Continue reading

Not just another RJ45 connector

From |

A Boss of a company had just awarded a million dollar project to a contractor for Ethernet Communication upgrading.

The contractor was happy as he knew how easy it was to supply a point to point Ethernet connection for the project and he asked the owner these questions during the project discussion.

Contractor: “How many Ethernet points do you need?”
Owner: “Erm…. I think about 10,000points”

Contractor: “How long is the distance from point to point?”
Owner: “Erm…. Actually I’m not sure yet”

Continue reading

Phoenix Contact E-Mobility Connectivity – The Basics

From |

Emobility Basics

 With attitudes leaning towards lower carbon emissions, electric cars are slowly gaining popularity around the world.

Plug-in charging systems from Phoenix Contact set new standards in power supply to electric vehicles. Whether charging on an AC network or fast DC charging – the AC and DC charging connectors from Phoenix Contact are safe, reliable, and user friendly.

Continue reading

E-Mobility – Electric Vehicle Connector Standards

From |

Electrical mobility is one of the growth markets and a decisive factor when integrating energy systems based on renewable energy. Electric vehicles are continuing to gain in importance; a development which is reflected in the ambitious targets many governments have set to curb CO2 emissions. While not a mainstream mode of propulsion yet, the development of a widespread charging infrastructure in conjunction with renewable energy will pave the way for a mobile future. Continue reading

New insulator-free PCB terminals for high currents

From |

Phoenix Contact’s PTSPL 6 single-pin PCB terminals without insulating inserts facilitate easy and secure connections up to 41 A directly on the circuit board and without any voltage restrictions. The terminal can be fitted automatically as part of the SMT process and soldered using THR technology. Continue reading

Connection versatility with Phoenix Contact

From |

Whether you choose the screw, spring-cage or insulation displacement connection method, Phoenix Contact always provides the highest level of quality. You can choose the worldwide standard:  the versatile screw connection. This connection method combines a large contact surface with high contact force and is a completely maintenance-free, easy, and gentle conductor connection. Continue reading