Phoenix Contact has a wide range of products and services to help machine manufacturers increase their competitiveness. The cost effectiveness, quality, flexibility, and performance of the machines are of critical importance in this regard.
Author Archives: Jiang
Installation terminals with Screw Connection Technology
From |Phoenix Contact’s new generation of UTI installation terminals is tailored to the requirements of electrical installation and distributor construction.
The Evolution of Heavy Duty Connectors
From |Looking for Heavy Duty Connectors? Saving Cost? Flexible Cable Outlet Direction? Quick and easy assembly? Look no more as the new Heavycon EVO from Phoenix Contact have what you need. Continue reading
Rotary switches for use in the field of energy technology
From |Phoenix Contact has moved one step closer to become a complete switch cabinet component provider with the introduction of CAM switch!
The product range of compact rotary switches up to 20 A has been designed for the switch programs which are available for application in energy technology.
Time for a NEW TOOL
From |Stripping, fitting with a ferrule and crimping are carried out in one work step.
The entire process is completed in approximately two seconds and the next conductor can be inserted for processing.
Watch out for this tool !
The POWER is NOW
From |The PTPOWER 95 family will be the first high-current terminal block with Push-In technology for direct plugging in the market.
The comfortable direct plugging of cable is now possible for larger cross-sections of 25 mm² to 95 mm².
The eccentric allows a simple handling without risk of injury.
Stay on and come back for more information.
Now the time to reveal the power! Click on the link below for more information:
Flexibility for Wiring Emergency Lighting
From |With a width of 5.2 mm, Phoenix Contact’s compact PTB 2,5 three-level terminal blocks provide high flexibility when wiring emergency lighting.
In commercial buildings, standard lighting is often also used as emergency lighting, which provides flexibility, for example, when modifying building utilization.
Introducing Thermomark Roll Printer
From |THERMOMARK ROLL printer is used for media on a roll – in either configured or continuous format – such as shrink sleeves, wire wraps and adhesive labels.
Compact Disconnect Terminal Blocks with Automatic Converter Protection
From |Phoenix Contact now offers pluggable measuring transducer disconnect terminal blocks with a disconnect element that can swivel.
The compact PTME 6 series is designed for wire cross-sections up to 6 mm² / 10 mm² and uses the standardized bridge, marking, and test accessories of the ‘Clipline complete’ modular terminal block system.
Introducing the Bluemark Cled
From |The new Bluemark Cled from Phoenix Contact makes labeling standard UniCard materials for marking terminals, conductors, and devices as easy as printing on paper.