Whenever an industrial PC has to be installed in the field along a manufacturing line for operator interaction, it has to be panel mounted onto an enclosure for ingress protection against dust and/or water.
This is because the typical industrial PC is designed with IP65 only on the front face where the screen is and IP20 at the rear resulting in the need of an enclosure to protect the rear.