The Innovation Fair has ended, however the euphoria of the successful event still lingers! Here are some snapshots of the event.
Monthly Archives: June 2012
Preview: The first ever Innovation Fair from Phoenix Contact
From |
Innovation Fair 2012 is a compilation of Phoenix Contact latest technology and future market trend. This latest technology translates innovative products and solutions that are beneficial to a wide spectrum of industries.
Compact Signal Routing in Power Systems
From |The new pluggable 4-level routing terminals PT 2.5-4L/1P and…/2P from Phoenix Contact provide universal signal distribution options within compact control systems and plant sections.
HMI Devices for Graphic-Intensive Applications
From |Phoenix Contact has expanded its HMI product line to include a new performance class: the TP 5000 series. In addition to the high-performance Intel® Atom™ 1.6 GHz CPU, these devices set themselves apart as a result of their wealth of functions.
Web-Based On-site Operation: Storing visualization on the controller (Part 3)
From |Easy Linking to the Controller
All operating and fault conditions recorded at the I/O level are passed to the BAVL library, thus reducing the required project planning effort for the user. Variables can optionally be flagged in the application programming for linking to the specific project visualization.
Selective Power Distribution with Innovative New Circuit Breakers
From |The new electronic and thermomagnetic circuit breakers from Phoenix Contact offer all of the system benefits that are important for quick and easy installation. They reliably protect devices from surges and short circuits, even when long cables are used.
M17 Plug Connecters in Miniature Format for Power Ratings up to 630 Volt
From |With the M17 compact series of round plug connectors, Phoenix Contact has reduced the size of its standard connectors. The diameter of the cable connector was reduced by 2.6 mm to 18.7 mm; the total length was also reduced by about 15 percent.
Terminal Blocks for Energy Management
From |Phoenix Contact offers three terminal block types for the distribution, measurement, and switching of energy: