Malaysia has experienced substantial economic development since the 1980s, resulting in increasing water demands in the commercial and industrial development centres. The Selangor / Kuala Lumpur region which is the political, commercial and industrial centre of the nation is the most important focus for these high demands which are expected to continue their rapid growth into the 21st century.
Yearly Archives: 2011
Acquiring, Monitoring, and Communicating Energy Data
From |With the Basic and Flex energy data loggers, Phoenix Contact is offering package solutions that contain all components users require for configuring a data acquisition system. The packages are based on standard industrial components with integrated GSM/GPRS modem.
Thanksgiving Meals-On-Wheels
From |My hero Warren Buffett has been promoting philanthropy these two years and I was very happy to be given the opportunity to do my bit for society with Phoenix Contact!
Active Redundancy Modules Decouple, Monitor, and Control
From |Two active Quint Oring redundancy modules are new in the Phoenix Contact product range. They increase the operational reliability by monitoring the redundant power supply solution from the output voltages of the power supplies through the power supply wiring up to the load, as well as the decoupling section up to the load current.
Preassembled RJ45 Patch Cable for Profinet
From |Phoenix Contact has now developed an RJ45 crimp connector for Profinet. Profinet cables with conductor cross sections of AWG 22 can be used as preassembled patch cables when using this connector.
Intelligent Uninterruptible Power Supply for the Control Cabinet
From |A new generation of uninterruptible power supplies now supplements the Quint Power product family from Phoenix Contact. Five new modules that can be snapped onto mounting rails are now available: For 24 V loads, the Quint UPS-IQ uninterruptible power supply has output currents of 5, 10, 20, and 40 A – and for loads with an input voltage of 85 up to 264 V AC, the Quint UPS-IQ supplies an output power of 500 VA.
Cost-Optimized Telecontrol
From |For data transfer via GPRS, Phoenix Contact offers Open Data Port (ODP), an intelligent solution to monitor and manage telecontrol stations. The advantages of this solution lie in the reliable data transfer, the use of standard PLC and modem components, as well as standard industrial interfaces and protocols.
Intrinsically Safe Isolation Amplifier with Two Electrically Isolated Outputs
From |Just 12.5 mm wide, the repeater power supply and input isolation amplifier MCR-Ex-SL RPSSI-2I belonging to the MACX Analog Ex product line of Phoenix Contact can be used to simultaneously supply two logic units with a 0/4…20 mA analog signal from a hazardous zone. This is HART compatible.
Phoenix Contact Datalogger+ – The Choice is YOURS!
From |Public utilities and refuse disposal plants are usually equipped with numerous external stations that must be connected to a central control system. In the case of water management for example, these are pumping stations, rainwater overflow tanks, wells or even complete system plants such as sewage treatment plant and waterworks.
White Paper: Wireless Solutions in Automation
From |So do you want to reduce installation, assembly and maintenance costs? Then convince yourself of highly efficient communication solutions based on wireless signal transmission.