Author Archives: Dania Liswi

Most read articles in 2015 [Industrial automation]

From |

Top 6 most read articles in 2015

First of all, are you still working on closing the books of 2015? Well, you are not alone! Just before we start bringing 2016 news to you, we thought to share with you some of the top old news.

The new generation of safety relays: PSRmini

PSR Mini - Most read articlesOur new PSRmini safety relays are rather the narrowest safety relays in the world with the performance of a large safety relay. Phoenix Contact developed the relay technology in the centerpiece of the new PSRmini device. The compact 6 mm wide elementary relay design offers tried-and-tested safety, because of the force-guided contacts. Hence, the numerous technological details make it reliable as safety technology should be. It is its robustness, reliability, and diagnostic capability that sets it apart from a standard elementary relay.

Find out more

Surge protection reinvented

SEC - Most read articles

Lightning and surge protection for the power supply is now extremely powerful and durable. This is made possible due to the new Safe Energy Control (SEC) technology with impact-free spark gap from Phoenix Contact.

Find out more

 

 

New DC/DC converters for the energy sector

DC/ DC Converter - Most read articlesThe new DC/DC converters of the QUINT POWER product range are particularly suitable for applications in the energy sector. Independent supply systems can be established and monitored in a preventative manner due to the electrical isolation between the input and output voltage. All DC/DC converters, power supplies, and redundancy modules of the QUINT POWER product range support power boost, which continually supplies 1.25-fold nominal current.

Find out more

Continue reading →

Monitor and Configure UPS systems Intelligently

From |

The UPS-CONF software

Monitor and configure UPS systems from Phoenix Contact using the UPS-CONF software. The new version features more functions and various improvements.

UPS-CONF enables UPS systems to be monitored and configured conveniently and clearly Firstly, UPS-CONF is a management software to configure and monitor QUINT-UPS devices, that come with the IQ technology. This technology with continuous battery monitoring and intelligent management provides you with information about the charging state, remaining runtime, and service life of your battery at all times. Intelligent communication informs you when a situation becomes critical. Eventually, this reduces the amount of maintenance involved and increases your system availability.

Continue reading →

Virtual power plants communication standard

From |

Phoenix Contact is implementing the communication standard for virtual power stations

VHPreadyTo begin with, Nuclear power plants will no longer exist in the future. By 2050, 80% of our electricity is expected to be generated by using renewable energy sources. These sources include wind parks, photovoltaic systems, hydroelectric power plants and biogas plants. A large number of individual energy generators however, means that the power grid will have to change in the future. This is how electricity generation and especially electricity distribution works today.

On the positive side, the industry forum VHPready (Virtual Heat & Power) is implementing the communication standard for virtual power stations. This standard is the basis for virtual power plants in which volatile renewable energy generators network in such a way that guarantees consistent energy supply to society and industry. As one of the founding members of this industry forum, Phoenix Contact takes part in developing the standard in collaboration with leading industry experts. This is a very positive perspective for the future. Continue reading →

Multifunctional crimping tool for taped ferrules [4 in 1]

From |

Multifunctional Crimping Tool – CRIMPFOX 4IN1

The CRIMPFOX 4IN1 range has multifunctional crimping pliers for processing conductors and ferrules. Using only one tool, you can implement various work steps: cutting, stripping, twisting and crimping. Moreover, the newly integrated 4-step pressure lock also enables use in industry.multifunctional crimping pliers

  • Fast handling
  • High comfort
  • Increased efficiency
  • High process safety
  • User friendly
  • High durability

Using only one tool, you can implement various work steps: multifunctional crimpingCutting, stripping, twisting and crimping.

CRIMPFOX 4IN1 has multifunctional crimping pliers for processing conductors and ferrules.

Cutting, stripping, twisting and crimping can quickly be realized due to the effective positioning of work stations.

High Comfort: Time and cost saving due to an integrated twisting unit. The tool does not need to be put aside when twisting the wire.

Increased efficiency: Time and cost saving due to pre-positioned (endless) ferrules in combination with a self-adjusting crimping and stripping system.

Continue reading →

Managed Switches | Industrial Ethernet | IEC 61850

From |

Managed Switches in accordance with IEC 61850

IEC 61850 places special requirements on network components. High ambient conditions apply for use in the energy area, which are specified in IEC 61850-3. For instance, our new managed switches have FO ports with ST connection and complete our Industrial Ethernet portfolio in accordance with IEC 61850.

managed switchesWhat are the main advantages?

  • Can be used under the harshest electromagnetic, electrostatic, and climatic ambient conditions.
  • Reliable, error-free data transmission over long distances, thanks to FO technology.
  • Redundant, replaceable power supply and special operating voltages.
  • Fast redundancy mechanisms for high availability.
  • High port density in one rack unit for low space requirements in the control cabinet.

To learn more about our managed switches, please visit our website here

Network infrastructure according to IEC 61850

IEC61850 - managed switches

A reliable and permanent power supply is essential for every industrial company. Over a quarter of the world’s population still has no access to electricity. From now until 2030, energy consumption in countries such as China, India or Brazil is expected to grow disproportionately. Rising energy costs, the scarcity of resources, CO2 emissions, and the associated climate change are global factors.

In order to overcome these challenges, a review of the energy infrastructure field is required, together with new system approaches such as the intelligent power grid, known as the Smart Grid. Therefore, the IEC 61850 international series of standards and communication based on Ethernet technology are an important basis for this review.

Continue reading →

Industrial relay system for all relay applications

From |

Industrial relay system for all relay applications

RIFLINE complete is our industrial relay system used to implement all standard relay applications. System handling is particularly easy thanks to push-in technology and other features.

RIFLINE complete industrial relay system with push-in connection technology

Firstly, the area of application ranges from coupling and timer relays through to the small power contactor replacement. Nevertheless, it differs from other product ranges with regard to its functionality, handling, range of products, and quality. Comparatively, the modules range from narrow 6.2 mm coupling relays to a replacement for small power contactors.

The most powerful relay can switch voltages up to 400 V. Similarly, the relay system with universal plug-in design supports high machine and system availability. Not to mention that the relays can be replaced quickly during maintenance work.

Easy wiring (left), easy potential distribution (center), and easy extension (right)

Easy wiring (left), easy potential distribution (center), and easy extension (right)

  • Easy wiring
    Thanks to push-in connection technology. This enables quick, tool-free wiring.
  • Easy potential distribution
    With plug-in bridges from the CLIPLINE complete system accessories.
  • Easy extension
    With the plug-in, multifunctional timer module. You can select three time functions in a time range from 0.5 seconds to 100 minutes.

In short, watch this animation video to see the advantages of the system

https://youtu.be/jzG_POv6A_I

Welcome To PHOENIX CONTACT Middle East Blog!

From |

Hello World! Welcome to the Phoenix Contact Middle East Blog!

Firstly, we are here to bring to you fresh content, whether you are our beloved customer, partner, employee or just another person who have heard about us. Have the latest industry news, product information, technologies and applications delivered right to your inbox. Welcome to our Blog!

Burj Khalifa View - Welcome to Phoenix ContactAs much as that, need I say more?

Oh yes, we are Phoenix Contact, a world leader for electronic components, systems and solutions in the field of electrical engineering, electronics and automation. We offer a broad range of products, from modular terminal blocks to control software, for your electrical engineering and automation tasks.

https://www.youtube.com/watch?v=KduXEOU2GLk

Are you living somewhere in the Middle East or Northeast Africa? This is great news! Now you have the chance to read the latest news and updates about products and solutions for this region. Also, you can personally meet our team of experts in the local events we participate in.

In conclusion, click the Subscribe button and get the latest updates on our blog right to your inbox.

In addition, you can also receive our monthly e-Newsletters that are especially relevant to you by subscribing here.