Monthly Archives: January 2017

SOLARCHECK RSD wins the GIT Security Award

From |

The automatic SOLARCHECK RSD photovoltaic panel shutdown has won the GIT Security Award

The automatic SOLARCHECK RSD photovoltaic panel shutdown won the GIT Security Award in the Fire & Explosion Protection, Industrial Safety category.

The coveted prize in safety technology is awarded each year by the magazines GIT Sicherheit, GIT Security, and messtec drives Automation on behalf of publisher Wiley-VCH.

Electrical safety in photovoltaic systems: in 95% of systems the panels are connected to strings in series. This can generate potentially lethal DC voltages of up to 1000 V. Disconnection to protect against electric shock is difficult. Occupational health and safety can only be guaranteed if each individual panel is disconnected automatically. SOLARCHECK RSD safely shuts down your system during installation, maintenance or in hazardous situations. A safe state is achieved without intervention by an electrician. Even those who are not familiar with the safety rules and dangers, such as roofers or cleaning personnel, are protected.

Find out why the SOLARCHECK RSD makes working on photovoltaic systems so safe