Monthly Archives: July 2026

How to Build Resilient Industrial Networks in a Cyber-Risk Era

From |

The Growing Cybersecurity Challenge in Industrial Networks

As industrial systems become increasingly digital, they are unlocking new levels of efficiency and flexibility. But this transformation comes at a cost: greater exposure to cyberattacks. What was once limited to IT environments now directly affects operational technology (OT), putting production continuity and infrastructure reliability at risk in modern industrial network cybersecurity environments.

To address this growing threat landscape, cybersecurity is no longer optional—it’s becoming a regulatory requirement. Frameworks such as the IEC 62443 standards, along with European regulations like the NIS 2 Directive and the Cyber Resilience Act (CRA), are setting clear expectations for how industrial organizations must secure their systems. These regulations extend responsibility beyond critical infrastructure to include much of the industrial value chain, while also requiring security measures to be verifiable across a product’s lifecycle.

From Compliance to Industrial Network Cybersecurity in Practice

Regulatory frameworks such as NIS 2 and the Cyber Resilience Act are shaping how industrial cybersecurity is implemented across the value chain.

Meeting regulatory requirements is only the starting point. The bigger challenge lies in translating these standards into real, effective protection on the ground.

Industrial networks are made up of multiple interconnected components, each playing a role in maintaining security. Managed switches, security routers, and wireless infrastructure together form the backbone of modern industrial communication. But as connectivity increases—especially with remote access and wireless technologies—so does the number of potential entry points for attackers.

And the risks aren’t always obvious. Over time, misconfigurations, outdated firmware, or unsecured interfaces can quietly create vulnerabilities. In long lifecycle environments, these gaps can go unnoticed until they become critical.

Continue reading →