Tag Archives: connectors

Miniature Connectors

From |

Small yet high-powered connectors

Application specific and miniaturized connectors have come on rapidly. Fueling this rapid change is a combination of advances in technology. The control cabinets are getting smaller. This in turn reduces the available space for the devices and their boards. In addition, the functional density of devices is steadily increasing. Thus, PCB connectors must also be based on the new size specifications.

What we can offer

Phoenix Contact has launched two new 2.54 mm printed circuit board connectors: the FMC 0.5 and DFMC 0.5 connectors. It is designed to meet the miniature & quick connection requirement, boasting a compact plastic housing and push-in spring connection. The direct connection is possible for solid and flexible conductors with or without wire end ferrules. The wiring can be easily released without the aid of a screwdriver and the connectors can hold conductors with cross sections from 0.14 to 0.5 mm².

Figure 1. Low height profile – the FMC 0.5 connector family offers a push-in spring connection with spring opener.

This connector makes it ideal for designers who face the challenge of keeping up with the trend towards miniaturization.

The FMC 0.5 connector is a single-row connector with a height of only 5.4 mm whereas the DFMC 0.5 connector is a double-row connector with a low height of only 10.5 mm. Plugs in the same grid with push-in spring connection and spring openers that were previously available on the market were twice as high. Both connectors follow the trend of miniaturization – and the associated trend towards a high contact density in a small space.

https://www.youtube.com/watch?v=K0C_x4vATnI

It is designed for automated soldering processes (SMD and THR soldering processes). The two product families’ pin headers are made of LCP (liquid crystal polymer) plastic to withstand the high temperatures in the convection oven.

The applications for the two new connectors are extremely versatile. Possible target groups include measurement and control technology, automation technology and energy technology. Conceivable applications include controllers and inverters. The focus of the application areas is on industrial applications where signals are transmitted to the PCB.

Conclusion – the answer to new market requirements

The new FMC 0.5 and DFMC 0.5 plug connectors and the associated pin headers from Phoenix Contact meet the market requirements in the field of printed circuit board connection technology. Device manufacturers now get powerful connectors that require little space on the circuit board and in the device. For the end customer, the connectors also provide a quick, easy and convenient connection option. Processing in highly automated SMD processes is not a problem, and a gold-plated contact system provides additional security for the transmission of signals in industrial environments.

If you would like a sample board, or would like to know more, don’t hesitate to contact us at marketing@phoenixcontact.com.sg!

Future Proofing Industry Seminar in Yangon, Myanmar

From |

Our slogan: “Inspiring Innovations”. It embodies what we do – Phoenix Contact never fails to come up with new and innovative products for the industry. As such, we are honored to be one of the market leaders and trendsetters of our industry.

Together with our partner in Myanmar, Synopsis Technology, we were proud to have brought you the “Future Proofing Industry” Seminar, held on the 31st of May 2018 at Lotte Hotel Yangon.

Seminar Poster

Alongside the topic of driving innovations, the main highlight of this “Future Proofing Industry” seminar was to introduce new applications and products for the education sector in Myanmar. It is of paramount importance to help the future engineers be ready for the industry.

Within the short time span of a day, we were elated that we had the opportunity to share our company history and actual success stories across South East Asia. Aside from that, we managed to introduce our innovative products as well.

First speaker: Mr Jiang

Our first speaker, Mr Jiang, who is also our Solution Manager, spoke about our new Industrial Cloud and Networking products for the first half of the seminar. Ideas and experiences were shared with the attendees.

Second speaker: Mr Maw Kon

The second speaker of the day was Mr Maw Kon, who is from Phoenix Contact Myanmar. He introduces our bread and butter products – the various connectors ranging from Terminal blocks to heavy duty connectors.

Third and final speaker: Mr Gary

Our last speaker, Mr Gary, never fails to draw the attentions of the attendees when it comes to introducing our surge protection devices. Live demonstrations and interactive activities were carried out and our attendees were all having a blast.

Last but not least, there was a mini competition held during the seminar.  All the attendees were encouraged to participate in the #futureproofingseminar and @phoenixcontactsea photoshoots. All they needed to do was to just take a photo during the seminar and upload them on their Facebook with the hashtag #futureproofingseminar together with a tag @phoenixcontactsea! The winner of the seminar was announced via our official Facebook page!

Safe and Reliable Power

From |

Upon mentioning PCB connection or PCB connectors, one of the first things that usually come to mind is an Electronics board for various applications. When electronics are involved, most manufacturers of connectors cater their designs to digital applications for modern devices such Smartphones, Tablets, Laptops, LED TVs, Set-Top Box and simple remote controllers.

For the above mentioned, design engineers, electronics designers, field application engineers, sales engineers and module designers often overlook the challenges or requirements needed for Industrial Electronics.

Most PCB or Industrial Control boards in Industrial Electronics are required to take-in high levels of in raw current, for the heavy duty tasks of operating motors, sensors and measuring equipment needed on modern devices.

New generation versions of Vision Inspection, Test System, Pick & Place, Bonding, Dicing, Conveyors and Ovens, utilizes loads that go up to 60A and 80A AC Voltage.

Typically, such high current capacity demands stringent safety features and equipment to be rigorously tested in high temperatures to ensure reliability and safety, in order to prevent catastrophic breakdowns of such systems.

From Phoenix Contact’s vast array of devices, Combicon Power is tried and tested to be the most suitable and reliable High Power Connector available in the market. Phoenix Contact’s Combicon Power are certified in UL, VDE and EAC, to ensure standards are in place giving customers ease of mind when adopting Combicon Power.

Combicon Power

Phoenix Contact’s MKDS 10, MKDSP 10HV, IPC 16, PC 16, PC 4, PC 5, HDFK and UW, were all adopted and used in two of the most notable Test and Management MNCs in Malaysia, in the Test and Measurement Systems produced by these MNC.

When your applications, products or modules are Power Hungry, and yet you need a safe, proven and reliable Power Connectors, Combicon Power is the answer to your needs and concerns.

Feel free to contact us to find out more!

Back to Basics – Basicline Series

From |

Phoenix Contact is well known for its terminal blocks and connectors. Phoenix Contact’s success was also partially attributed to its Back to Basics campaign, which aimed to drive the business to meet all market requirements.

One particular Back to Basics product series worth mentioning is the basicline series – great quality connectors and terminal blocks that are also cost competitive.

The basicline series had helped many Phoenix Contact customers to have reliable and robust connectors at affordable pricing. This enabled customers to produce devices that are both cost competitive and reliable.

Many customers that have faced challenges in producing cost competitive devices for building automation, door access, security etc. are satisfied with what basicline has to offer.

In addition, basicline has helped to solve problems arising from using Asian-branded connectors with lower quality and reliablity issues.

Below is an example of a basicline series product.

Advantages

  • Tin plated surface contact prevents rust overtime and provides consistent current rating
  • Non-frisky plastic housing and strong PA 66 provide robust and reliable usage
  • Strong price to performance ratio
  • Available in 3.50mm, 3.81mm, 5.00mm and 5.08mm pitch
  • Pluggable connectors and terminal block
  • Comes in green, black and grey. For other colours, kindly contact our salesperson
  • Optional marking and profiling
  • Available in 2 – 16 poles
  • Pluggable header available in horizontal and vertical positions

Interested to find out more? Contact us at marketing@phoenixcontact.com.sg!

The Push-in Terminal Block Evolution

From |

From the most reliable UK – Universal Screw terminal blocks to advance spring technology terminal blocks, Phoenix Contact has successfully developed and produced terminal blocks over the past90 years.

As terminal block innovation is the heart and soul of our company, Phoenix Contact never fails our customers with new terminal block innovations over the decades.

Continue reading

Easy and Reliable Connections

From |

VDay2014_Header

When it comes to reliable signal and power transmission in harsh industrial applications, circular connectors are at the heart of the electrical connection technology.

In recent years, the requirements placed on plug-in connection technology have become increasingly diverse.

Continue reading

E-Mobility – Electric Vehicle Connector Standards

From |

Electrical mobility is one of the growth markets and a decisive factor when integrating energy systems based on renewable energy. Electric vehicles are continuing to gain in importance; a development which is reflected in the ambitious targets many governments have set to curb CO2 emissions. While not a mainstream mode of propulsion yet, the development of a widespread charging infrastructure in conjunction with renewable energy will pave the way for a mobile future. Continue reading

Home Fix-it: Cable Extension with Phoenix Contact QUICKON Connectors

From |

Good day!

Have you been faced with a situation in which you needed to extend your cable length without having to replace your existing one? This situation is quite common especially for customers in the machine building and material handling industry.

Taking into consideration that industrial standards require joints to be water- and dust-proof, the very thought of replacing a short cable and re-laying it with a longer cable can seem daunting. Not only is it a waste of material , it is also a waste of time which equates to significant cost over time.

I would like to share my personal hands-on experience with you. Two years ago, after moving into my new apartment, I was faced with a need to extend the wire for my fan as the wire given by the manufacturer was too short . At the same time I needed it to be water-proof, as I wanted to ensure that water did not seep into the joint when the floor was being mopped.

Quickon cable connectors , 1642153
As I had a couple of samples on my hand and I decided to use a Phoenix Contact QUICKON cable connector.

With the clearly written instructions from the manual that came with the standard package, I managed to join the two cables in less than five minutes. Sharing similar concerns as any of our customers would have, more skeptical of my own technical skills than of the insulation displacement technology, I turned on the fan and voila. The power flowed flawlessly and I was enjoying the breeze from the fan, bringing a smile to my face.

httpv://www.youtube.com/watch?v=M3YudXpogZ0

Till date I am still enjoying the cool breeze from my fan, powered by Phoenix Contact. Maybe it is about time to do another home project, how about a smart home system with the touch panel and controllers?