Step Power power supplies from Phoenix Contact achieve a high energy efficiency in their class. A 48 V AC power supply is now available in a housing that is just 18 mm wide.
Transportation Solution Demostration by Phoenix Contact
From |Does the rain cause disturbance to your wireless transmission? How about installing the wireless device inside a glass cover box? Does it help? Watch the video to get your answer and also see what Phoenix Contact have to offer for your Transportation solution!
Xplore Automation Award 2012
From |One of our EDUNet partners in Singapore, ITE College East has submitted an entry to Xplore Automation Award. Their submission, entitled “Learning PLC in an Authentic Learning Environment” can be viewed below.
Intelligent Energy Data and Motor Management
From |Phoenix Contact combines distributed I/O stations and interface modules to create a seamless and integrated solution for energy and motor management. Whatever the requirement – be it the monitoring of the active power of server cabinets in a data processing center, energy-saving monitoring and switching of motors in production plants, or the management of standby functions in machines – all of these tasks can now be solved even more intelligently.
Universal Temperature Transducer with Switching Outputs
From |Phoenix Contact’s new universal temperature transducers belonging to the MACX Analog family of isolating amplifiers have been developed and produced in accordance with the functional safety standard in all steps of the product lifecycle. The modules include a signal input for a resistance thermometer, thermo elements, resistance-based transmitter, potentiometer, millivolt sources, as well as for customer-specific characteristics.
Case Study: Singapore Lower Seletar Reservoir equipped with Phoenix Contact Spring Terminal Block
From |Calm and peaceful, Lower Seletar Reservoir Park is a pleasant place for leisure strolls or jogs. Benches along the edge of the reservoir offer great spots from which to enjoy the turquoise waters and the balmy breeze.
Today, PUB allowed sailing at Lower Seletar Reservoir and this was done in collaboration with the Singapore Sports Council (SSC) and the Seletar Country Club, as well as a fishing jetty (maintained by PUB) that extends its fun to fishing enthusiasts.
How can Phoenix Contact Wireless Technology help YOU?
From |Our range of products for wellhead automation includes wireless technology, power supplies, surge protection and industrial controllers – all of which work together to create a single-vendor solution to increase your productivity and reduce your cost.
Stop Accidents before they stop you!
From |CT(Current transformer) Terminals are used primarily in the energy/electrical power utility industry. When the current in a circuit is too high to directly apply to test or measuring instruments, a CT reduces the current proportional to the current in the circuit.
Case Study: Provincial Water Authority (Remote Pump Control System via SMS Technology)
From |Thailand’s Provincial Waterworks Authority alias “PWA” fully owned by the Thai Government, are responsible for the collection, production, distribution and reclamation of water in provincial Thailand. Driven by a vision to ensure all citizens of Thailand receive clean drinking water from all parts of Thailand.
EASY Control with Phoenix Contact
From |EASY compact controller systems with variety of options
The easy automation solution offers the customer a unique, inexpensive price/performance ratio as well as the possibility of higher flexibility and modularity at the same time.