Category Archives: Marking & Installation

Easier Maintenance, Easier Troubleshooting with Phoenix Contact

From |

If you were to connect one or more wires, you may simply think of connecting them from one point to another. Well, you can do that technically. However, things could get messier than expected.

Image from: https://www.flickr.com/photos/belleville/59234524/in/photostream/

YES, without any prior planning on how wires are to be connected and a proper design of control cabinet layout, you may face the cable jungle, just like what you see in the photo. If you have to perform maintenance or troubleshooting on the control cabinets, this will possibly be one of your worst nightmares! It’s not only about complexity of your job but also your safety.

Not to worry, we are here to help!

Firstly, terminal blocks could be positioned in your control cabinet layout design. Terminal blocks, as a central termination point between the field wiring, provide you an easy and convenient method to group and/or distribute the wirings. This means terminal blocks could provide you with a neater control cabinet with cables.

The wide product range of terminal blocks can be found in Phoenix Contact and you can choose based on your requirements and standards.

Once terminal blocks are in your control cabinets, you can finally escape from the cable jungle. Troubleshooting should be much easier for you to manage now than ever before.

Image from: https://smartcsm.com/25-of-the-worst-electrical-panels-weve-ever-seen

Do you still think that your control cabinet is messy?

You may see the disorganised cables running around the area unmanaged. It might even look dangerous.

If this is what you see, it’s time to use cable ducts.

Even for cable ducts, Phoenix Contact provides many different types according to different situations and environments. The wide range of cable ducts enable flexible and optimum use of available space in your control cabinets.

Your working space will be significantly less cluttered with the use of terminal blocks and cable ducts now. All you need to do for maintenance and troubleshooting will then be straightforward and trouble-free.

Wait! Don’t bounce off yet! We have one more suggestion for easier maintenance, easier troubleshooting with Phoenix Contact. Let’s do a ‘Spot the Difference’ exercise! Can you find the difference between the two photos below?

Apart from messier layouts, the main difference is missing labels. Did you manage to spot those? During testing and troubleshooting, you may realise that you can’t differentiate the cables, especially when they are routed from same location. The labels will be able to help you figure out where each cable is from just by looking at the control cabinet; you won’t have to manually route back where the cable is from. Labelling not only for the wires but for the terminal blocks and other components will benefit you for your routine maintenance and repairs. Easy identification of all the components will reduce your time and effort on handling the control cabinets.

Phoenix contact has launched a series of marking materials and printers. Our printers are made user friendly with ‘simply easy’ motto. Our marking materials are developed with printing services that are widely available for:

  • Terminal blocks (not limited to Phoenix contact terminal blocks)
  • Wires (self-adhesive, clip type & with binder type)
  • Equipment (control panels, equipment tag, temp resist/proof labels, etc.)
  • Plant markings (warning labels)

Your worries and challenges for maintenance and troubleshooting of your control cabinets can now be tackled with ease.

Redefining Laser Marking

From |

Phoenix Contact would like to introduce a facelift version of our laser printing machine, TOPMARK NEO.

It is back, more compact, more economical and with more effective software!

Phoenix Contact provides both the printer as well as the material that you need. In a one stop solution, it saves you the trouble of searching for different vendors for your process. Within the footprint of 180 by 180mm, it is able to engrave on materials such as aluminium, stainless steel, Transply-ABS, UCT terminal cards, and polyacrylate! We have more than 620 materials for you to choose from.

Topmark NEO has a footprint of 580mm X 615mm, weighing no more than 50 kg and qualified as a Class 1 Laser machine. At the side, it has a HMI device for direct printing or connecting it through a laptop where you can create your templates or printings too.

The story doesn’t end here, even if you are not interested to get the printer itself. If you need just the marking, no problem! Phoenix Contact provides the printing services for all of them. Contact us now at marketing@phoenixcontact.com.sg if you would like to know more about it!

Funny Warnings

From |

JUST FOR LAUGHS

We might think that warning labels are rather mandatory, rather standard, rather rigid, so much so that there is nothing to talk about…

But hey, have you really noticed all the warning labels around, and some of the interesting ones that are hanging around?

#1 Do not put plastic bag over your head

It might sound absurd… But there are many incidents that happened due to these plastic bags!

#2 Do not squat on the toilet bowl, that’s incorrect!

Well…. Let’s all be considerate and do it the ‘correct’ way.

#3 Beginner Driver

This is to be very sure that all the drivers behind you are aware that you just started out.

Or… does it help you to drive horribly and overtake cars?!

#4 Don’t touch my car

Touching the car might cause death… so be careful and stay away!

#5 Maintaining eye contact for more than 2 seconds is disrespectful

I guess it is meant to prevent fights arousing from staring contests… But if I talk to you without looking at you… is it also disrespectful?

The similarity between all these funny labels that you have seen above is that they are very customizable. The wordings and pictures are non-standard, and in fact, creative to catch attention from people.

With that said, do you know that Phoenix Contact labels can be printed to be anything that you want? Phoenix Contact has software (Project Complete) that can be downloaded free, and within the program, you can design it to your own way, be it funny, unique or specific, it can all be customized to your needs.

We have our free software (Project Complete) that allows you to bring in pictures and type your own text. You can design your label any ways that you like!

Feel free to contact us at marketing@phoenixcontact.com.sg to find out more!

5 Reasons Why Thermofox is a Must-have

From |

Phoenix Contact is proud to have our handy printer where you can label your panels/wires anywhere, any time. And here are 5 good reasons why you should own one today.

  1. Convenience

It is more than just a labeller; it brings you the convenience that you need such that you can carry it everywhere you go. Weighing as light as 650 grams, compact in size, this handy and portable printer gives you all your printing needs with ease. Additionally, it comes with accessories for you to carry it everywhere you go!

  1. Variety of prints

Printing of sticker labels is nothing interesting… It is the most basic material that a printer can print our sticker labels on. We have catered for different textures such as rough or curved surfaces. On top of sticker labels, our handheld printer can print self-laminating wire markers as well as shrink sleeves wire markers! This is really a small printer with a big capacity of printing varieties.

  1. Power efficient

This is the only handheld labeller in the world that you will find “ECO-MODE” inside! Once the printer detects that it is running low on battery, it will automatically enable this eco mode, which allows printing at a slower speed but of equally good quality.

It comes with a rechargeable battery in the full Thermofox set, or can be fitted with 6 normal AA batteries.

  1. Smart keyboard

This printer has a smart keyboard with an alphanumeric number pad. It has easily understandable buttons such as “symbols”, “templates”, “print” and “preview” that can be selected from the printer. The buttons are made such that they are self-intuitive and anyone will know how to use it without prior training needed.

  1. Resistance of the markings after printing

The last thing you would want is that all your labels start fading away and you being left with an unclear label. You can try scratching the prints or pouring some water or oil on it, but trust me, the ink will still be in a good condition!

Our prints are qualified with certain test industry standards to assure the quality of each and every single print. In fact, we have test laboratories!

If you would like to know more about Thermofox, feel free to contact us at marketing@phoenixcontact.com.sg!

Marking Materials for Solar Photovoltaic Application

From |

With the implementation of large scale solar projects in Malaysia, there are more and more inquiries on special marking materials for cable marking, equipment marking, and plant marking that can withstand long hours of sunlight and harsh environments.

If you ever come across such a request from the project consultants or clients, Phoenix Contact marking materials are what you are looking for. We have various product offers that are UV-resistant and weather resistant, ranging from stainless steel to aluminium to high-quality thermoplastic polyether urethane.

Here are two examples of solar cable markers with different types of printing methods.

1) Stainless Steel and Aluminium markers:

Phoenix Contact LS-WMTB product range is available in stainless steel (V4A) or aluminium. It provides simple and fast installation with cable binders. This marker is suitable for the most demanding industrial requirements because it not only fulfils the harsh requirement in the solar industry, but it can also be applied in areas that require high resistance against salt water, chloride, and solvents.

With the use of modern laser technology, it creates highly resistant and permanent markings on these markers.

Examples of stainless steel cable markers

2) Polyether Urethane (PUR) markers:

An example of a polyether urethane cable label

An example of a polyether urethane cable label

Phoenix Contact WMTB HF range of product is suitable for both indoor and outdoor applications. It is made of high-quality thermoplastic polyether urethane, halogen-free and flame-retardant material, with high tensile strength that is able to adapt to the bending of the cable conductors.

WMTB HF comes with an exciting selection of colours, from the commonly-used white, to yellow, red, blue, and green. Unlike the stainless steel marker, WMTB HF is printed using thermal transfer technology.

Other than the marking materials, Phoenix Contact also offers UV-resistant cable ties that work with the markers, as well as high quality printers with laser and thermal transfer technology. Please feel free to contact the Phoenix Contact sales team if you wish to know more about these products.

Three Good Reasons Why You Should TRADE IN Your Printer

From |

Phoenix Contact has a wide variety of printing systems, capable of meeting all sorts of marking requirements, ranging from terminal markings, wire & cable markings, equipment labels and plant markings!

Terminal Marking

Terminal Marking

Wire & Cable Markings

Wire & Cable Markings

Equipment Marking

Equipment Marking

Plant Marking

Plant Marking

Label On-the-go

 

Every label requirement you need for your panels, inventory, workshop or even wiring is possible with our variety of printers in place! Print at your own convenience and save the hassle of pre-ordering them. You can also customize our printers to cater to your own specific printing needs, avoiding wastage due to unused or wrong labels!

 

What’s more is that Phoenix Contact is having a TRADE IN scheme now!

Three Good Reasons Why You Should TRADE IN Your Printer:

  1. Get the most bang for your buckAll your marking needs for rolls and cards

Why not save your company some money if you can let go of your old printer, in exchange for a discount off the new one? The trade in scheme is meant to give customers more incentive to purchase a new printer from us! Speak to your local sales representative to get more information on how much discount you can get off your printer when you trade in yours now!

  1. Upgrade your current technology

High Volume Printing

Have you been using your printer for many years, unaware of how much technology has progressed? Printing speed has increased tremendously over the years, not to mention the quality of prints! So, if you are wondering if it is time to get a better printer for greater efficiency, it is still not too late! The trade in scheme is the perfect platform for you to enquire more about the technology that goes into Phoenix Contact printers.

  1. Save the environment

Instead of chucking your old printer in a corner, taking up space and collecting dust, we welcome all your used printers to Phoenix Contact, and you even get a discount when you purchase one from us!

If you still insist on disposing of your old printer, there are tons of toxins inside printers that hurt the environment! So, start thinking about our trade in scheme and do your part to save the earth!

Click here now if you are interested to get a trade in!

Product identification – Can you survive without any?

From |

The need for product identification is not new. Since the early days of civilization, due to a lack of technological advancements, products traded and sold were identified in different ways. Clay jars, crates and sacks were distinguished through the shape of the vessels or unique markings made on them for identification purposes.

Dating back to 6000 BC, barter trading was the main system for the exchange of goods and services; this was before the invention of money.

By F.S. Church, published in Harper’s Weekly, January 17, 1874, p. 61. [Public domain]

The Need for Product Identification

Over time, the situation then transitioned into exchanging money for goods. With the evolution of business into mass production, previous methods of identification were not sustainable as  products now needed to be identified through category, name and description.

Similar to the evolution of street names, housing numbers, or even zip/postal codes, the invention of such identification allowed people to easily identify where they were going. Consequently, with ever-increasing inventories of parts and products, manufacturers and stores required new control mechanisms to track their status. Product identification became important in business in terms of logistics and data analysis.

After knowing the brief history for production identifications, we have seen these requirements for marking and identification evolve tremendously and can be found in almost every aspect of our modern day life or business.

What is tagging and marking like these days?

Today, our tagging & marking typically need to serve 5 key purposes

  • Product Identity
    The most basic and important purpose of labels is that it has to convey information on its identity mainly for tracking and tracing purposes. This can be in the form of descriptions, revisions, serial numbers or lot numbers. Another key identification purpose, especially in the Food & Beverage Industry, is to state the Manufacturing Start/Expiry date. Some labels would also need to include specific types of information as required by government legislation.
  • Security Risks
    Labels play a crucial role to reduce security risks due to the proper identification written on it. When there is a need to prevent any unauthorized opening of the packaging, there can also be tamper resistance labels to avoid such happenings.Labels could also have authentication seals such as serial number, barcodes, RFID, to reduce the risk of forgery or tampering.
    Product Identification - Tamperproof EMLS Label
  • Marketing
    The use of labels can also be for persuasion to encourage potential buyers to purchase a product. This is usually done with the use of graphic designs, attractive words and titles to entice the buyers. Most commonly, designed to reflect the brand’s message and speciality.
    Product identification - Stainless Steel self-adhesive label
  • User-Convenience
    Labels can contain information that could help the user/buyer by conveying instructions on handling, usage, display or sale.
  • Quantity Information
    Quantity is another important piece of information that would typically be required on labels. It tells the buyer or user the number of item in a covered packaging without the need to open up the package.

An ideal label concept would allow a product to be able traceable from the hands of an end user all the way backwards through delivery, manufacturing, raw material processes and to the point where supplies of raw material are identified.

With these said, if you require such a labeling system, Phoenix Contact has the perfect solution to provide you such printing mechanics. Our range of printers can provide the optimal labels that you require. “Clip Project Marking”, our labeling software, allows you to create your own product identifications by adding letters, numbers, barcodes, symbols, logos and pictures!

From there, you can print with the range of printers and over 3000 different materials catered for different uses and surfaces! Leave us your contact details at marketing@phoenixcontact.com.sg to learn more about Phoenix Contact Printing system.

Cut, Strip and Crimp – Tools to Ease Your Cabling Pains

From |

Today, we enjoy the fruit of technology as we turn on our television, air-conditioner, lights or our smart devices. Have we thought about what are the nitty-gritty details that have led to our enjoyment in this day and age?

What is common amongst all this technology is the need for electricity, and more importantly, what carries electricity around are wires.  Wires and cables are the root that carries electricity all round; it allows current to flow from one point to another. What is often missed out is the hard work spent by the electricians who, behind the scenes, manages this labyrinth of wires.

Messy cables

Photo by: Derek (https://www.flickr.com/photos/dcmorton/2446443103)

Cutting, Stripping and Crimping are steps that are very familiar to our electricians. However, they are not just merely steps; but in fact, they are techniques that we need to offer much respect to the electricians who handle them. Providing the right tools for the job makes it even more crucial to ensure they put their techniques into the right place.

Cutting, Stripping and Crimping of wires sound easy and effortless. However, using it on a daily basis requires the tool to be designed more than just a normal tool. Phoenix Contact takes ergonomics, usability into consideration and provides the optimal tools for its end users.

Tools to Cut, Strip & Crimp

Cut – CUTFOX 18

Phoenix Contact Tools - CUTFOX 18
  1. Safety Lock
    Safety is a true concern in a workplace, and every effort to keep the workplace safe is extremely important. Slip guards are attached in our cutter which keeps the blades closed.
  2. Less Fatigue
    Spring-loaded pliers opens up automatically, which means users spend lesser energy. With the pivot near the cutting edge, it provides optimum power transfer.
  3. Cutting Quality
    Cut your wires perfectly with the special curved metal giving your wires a nice and squeeze-free cut.
  4. Reliable Material
    The steel material of the cutter has gone through heat and surface treatment ensuring your tool to be long lasting and corrosion resistant.
  5. Comfort
    Consisting of both soft and hard parts, meant for the best comfort for any hands. The curved designed of the handles and the angled head for the ultimate ergonomics.

Strip – WIREFOX 10

Phoenix Contact Tools - WIREFOX 10
  1. Easy Adjustment
    Depth of the blades can be easily adjusted as required. Length of the stripped length can also be easily adjusted with the small measurement ruler and the stopper in place.
  2. Flexibility
    Interchangeable knife cassette gives you the option for all different wire sizes as required. One casing for all wire sizes!
  3. Stopper
    A wire stopper equipped in the knife cassette helps you to position your wire at the stripping length you need.
  4. Convenient Cutter
    Equipped with a cutter at the side, it gives you the convenience to cut your wires any time.
  5. Comfort
    Consisting of both soft and hard parts, meant for the best comfort for any hands. The curved designed of the handles and the angled head meant for the best stripping experience.

Crimp – CRIMPFOX CENTRUS 6S

Phoenix Contact Tools - CRIMPFOX CENTRUS 6S
  1. Multi Range Die
    Self-adjusting principals of the die covers a large cross section (0,14 – 6mm²), so you can use one tool for most of your needs.
  2. Good and Complete Crimp
    Built in ratchet mechanism is the key for a good crimp as it doesn’t allow the pliers to open until the process is complete. In this way, it ensures a proper and complete crimp.
  3. No need for recalibration
    Due to the special die closing process and its ball bearings, it reduces wearing out. Thus, eliminating the time and effort you need for re-calibration.
  4. Less effort
    Equipped with a rotating crimp mechanism, together with the tool size, ensures an optimum power transmission. In other words, you use less energy!
  5. Comfort
    Consisting of both soft and hard parts, meant for the best comfort for any hands. Its small size of 18cm tall, 6.5cm wide, and weighing at 380g serves as a compact and handy tool. The optimal positioning of the pivots gives the smallest opening handle angle in the market. Not forgetting the soft non-slip pressure pad supports your force transmission, so you can, for example, have it sit against a table surface!

After introducing the key features and ergonomically designs of our Phoenix Contact tools, would you like to experience it first hand on its comfort and ease of usage?

Cut, Strip & Crimp Toolkit Promotion

Get a “Cut, Strip & Crimp” Toolset kit today with our current promotion in Phoenix Contact!  For more information on the promotion, just leave us your contact details at marketing@phoenixcontact.com.sg and we will get back to you soon.

Manufacturing Expo 2017

From |

We would like to invite you to join us in at Manufacturing Expo 2017 located in Thailand, Bangkok, BITEC, from 21 to 24 June 2017. Manufacturing Expo is one of the biggest manufacturing exhibitions in South East Asia. It comprises of 7 sub-shows. We will be located at Automotive Manufacturing, under Singapore Pavilion (3D15)..

One of the most thriving industries in Thailand, Automotive adopts industry 4.0 to boost the production efficiency. Moving with the industry trend, Phoenix Contact would like to take this opportunity to showcase our capability on smart connectivity for smart factories as well as Phoenix Contact very own Industrial Internet of Things (IIOT) solution.

Being an innovative company, we strive to increase productivity and efficiency with cutting edge connection technologies. Quick connection technologies were incorporated into our connectors as well.

For example,

Push-in

Push-In Connector

Insulation Displacement Connection (IDC)

Insulation Displacement Connection (IDC)

Piercecon for high density (up to 17 positions)

Piercecon Connection

Besides signal, M12 connector is also used in transmitting data such as Ethernet and Profinet as well as power (AC/DC). Phoenix Contact is able to provide a complete solution from device connectors to field cablings.

Signal, Data, Power

Industry 4.0 requires the transmission of more signal, data and power than ever. Phoenix Contact circular hybrid connector provides an All-in-One solution.

HEAVYCON Modular

Using Heavycon Modular, signal, data and power can be mix and match easily in one connector. It also provides the flexibility for future expansion and modification

HEAVYCON Surface Mount

Besides copper based data connectors, we also have a complete solution for fibre optics according to your requirements.

Fibre Optic Data Connectors

Interested to know more about the applications of the products mentioned above? Come join us at Manufacturing Expo. Our sales team will be happy to assist you. Express your interest by helping us to fill up the survey form to receive a mystery gift.

CUT, STRIP and CRIMP wires with no effort

From |

Cut, Strip and Crimp Wires – Electrical wiring is integral in any building construction, electrical maintenance or rewiring works.

In today’s highly competitive market, businesses are looking for efficient shortcuts to hasten the task on hand.

If a particular task can be completed half the time at half the cost (or manpower), businesses can definitely reap the advantages.

QUALITY + CONSISTENCY

Problems facing Electricians and Technicians

Often the case for anyone and everyone, productivity is key in maintaining good client relationships and pair that with consistency, your business could go a long way.

Whether it’s in building construction, electrical maintenance or anything which requires electricity, there’s one thing that gets on everybody’s nerve – Wires. Wires, cables, cords or lines – Whatever you call them, they can be a menace.

“Of course I know what I’m doing. I’m an engineer”.

Cutting, Stripping and Crimping wires.

It’s a painstaking and laborious task. Admit it, we know.  Even with extreme patience and discipline, there’s no other way around it.

Wire maintenance is a known problem and the task can be daunting especially for large scale projects.

Using conventional tools (or primitive ones) such as pliers, wire strippers and wire crimpers takes little or no effort if it’s just a small scale task but it could be a nightmare for electricians and engineers especially if they have to complete a rewiring task for the whole building!

“Martin, we have a wiring issue” (Courtesy: Warner Bros)

Here at Phoenix Contact our mission is not to just produce innovative stuff but, we want to bear your pains.

By understanding engineering pains could we then build better things to solve common problems.

Ok, before we identify the problems, let’s take a look at the current tools we have today:

Cutting Wires

Recognize this guy?

Tools from the stone age.

If you’re a technician or electrician this would already be an extension of your arms. This is a wire cutter and no rocket science needed. It cuts wires.

If you’re cutting wires for a living you know that it’s a pretty much a simple task. Snip and you cut the wires into two. But what if you have to cut long stretches of wires at the exact lengths.

Now imagine if you have to cut rolls and rolls of electrical cables at specific measurements within a limited timeframe.

Stripping Wires

Okay, so if you’re not into cutting wires, surely you would have to strip wires right?

At some point when you’re dealing with electrical cables, you may need to strip them.

Here comes this dude here:

You can surely find this tool in a museum

Maybe you can picture yourself cutting spools of wires. After all, anyone could do it with a pair of scissors or penknife.

But how about stripping wires?

Stripping wires require more dedication and accuracy. Not only do you need to be extra careful to not break the sensitive insides of the wire, you also need to apply delicate pressure to tear apart the rubber insulation.

You’ve imagined cutting rolls and rolls of wire. Now imagine stripping rolls and rolls of wire.

Talk about having a bad day.

Crimping Wires

If you’re dealing with electricity, or in general wires, you would know that cutting and stripping wires are just the tip of the iceberg.

We haven’t got to the fun part yet – Wire Crimping!

Manual Crimping is a hassle

Cutting seems like child’s play while stripping take a little more effort. But there’s just no denying that crimping keeps you awake at night.

Crimping wires is an art form that requires extreme dedication. If done wrongly you’ll be having a loose ferrule and that’s not good if you have a rewiring job with thousands of wires terminating at various points.

Locating just that loose wire (or bad crimping job) amongst the thousand of termination points could be a hassle and could double the effort. And using a manual crimping tool could be child’s play at first but after awhile you’ll get hand aches and sore fingers.

Complicated and hard work right?

Anyone could crimp a wire but to crimp multiple wires is just insane. The next thing you know, you’ll be looking like this man over here:

“Come with me if you want to Crimp”. (Courtesy: Orion Pictures)

So if we were to sum it up, imagine if you have to CUT, STRIP and CRIMP rolls and rolls of wires. Even if you outsource the job, it’s going to cost you.

Other than cost, you also have to factor in the time taken to cut wires (ensuring they’re evenly cut into exact lengths), crimp (to ensure they’re securely attached to the ferrules) and strip them (being careful enough to not cut more than intended) – Phew!

Cost and time aside, you’re also facing safety issues and also ensuring quality so that your client becomes a returning client each and every time.

Solutions to Everyday Problems

As said earlier, we hear your pains and then translate that into solutions.

Over at Phoenix Contact we have introduced revolutionary productivity tools to solve your wiring woes (all at a fraction of the cost!).

We present to you the A-Team for Wire Maintenance! (Drumroll….)

Bad boys, bad boys…Whatchu gonna do

The CUTFOX10 (The wirecutter)

The CUTFOX10 cuts almost any wire and is ideal for heavy duty cable trimming activities. With a user-friendly display and safety mechanism, the CUTFOX10 is built for speed and usability.

 

Steps on using the CUTFOX10:

    1. All one needs to do is placed the wires onto the rollers of the CUTFOX10 and then close the covers.
    2. Set the desired length and quantity on the user-friendly display (and it comes in multiple languages so do learn a new foreign language or two).

  1. Once you press the Start button (which is the green button – how convenient!), the CUTFOX10 will cut the desired length and required quantities of your wires. It’s that simple!

Features Benefits
  • HUD display
  • No prior knowledge needed to operate
  • Cuts conductor, cables and similar profiles
  •  Cuts wires in a matter of seconds
  • Easy operation
  • Automatically cuts to the desired length with a push of a button

 

The WF1000 (The stripper)

Don’t let the name fool you. This weapon is a must have in your arsenal for stripping cables, even those with special insulation types. Since it is built to specifically strip wires, the WF1000 also does partial stripping and also ensures that pressure points on sensitive insulation are avoided. With just a touch of a button, you can strip cables with diameters ranging from 0.08mm² to 6 mm².

Again, we make it in such a way that you can use the machine in 3 easy steps:

    1. All one needs to do is turn the knob to the desired diameters (we even provide the dimensions on top of the machine for quick reference).

    1. Once you’re happy with the configuration, insert those wires into the WF1000.

  1. Enjoy the detailed cut, you deserve it (it’s actually only 2 steps but we’ll make step 3 serves as a reminder of your success).

Features Benefits
  • Wire dimension diagram on machine
  • Fast reference without requiring third party reference
  • Easy to operate controls – knobs for diameter adjustments
  • Strips wires with precision without physical strength
  •  Built for wire stripping in mind
  • Strips almost any type of wires, even those heavy insulated ones

 

The CF500 (The Crimp)

While the WF1000 strips, the CF500 was made to Crimp wires. With a range of crimping die dimensions, it crimps various types of cables. With a build in protective cover and step pedal for easy operation, the CF500 is designed for safety and convenience.

 

By now you should already know that we simplify the usage within 3 simple steps:

    1. Apply the correct die for the crimping job. As seen in the picture below, it only takes 45 seconds with the use of our specialized Hex Key (you heard that right, only 45 seconds).

    1. Once the desired die has been bolted, attached the enclosure to ensure maximum safety when using the device (without the protective cover attached,the machine would cease to operate). With the die and enclosure secured, you then need to press the buttons on the display.

  1. Once you’re satisfied with the configuration, it’s time to crimp! Insert the wire into the mouth of the die and let your feet do the pressing (with our crimping tools, we let your hands do other important tasks – like having a sandwich while your foot does the labor).

 

And there you go folks! You have your wires crimped at half the time and half the effort (or should I say, quarter the time, quarter the effort). Say goodbye to working overtime.

Features Benefits
  • Build in display and buttons
  • Crimps within seconds, with a simple touch of a button
  • Safety enclosure
  • Won’t operate if the enclosure or the die is loose.
  •  Multiple die for multiple crimping jobs
  •  List of accesories and compatibility with various ferrule designs

 

So in summary we’ve got tools that cut, strip and crimp your wires, turning meaningless chores into passionate hobbies.

BUT WAIT! There’s more!

In some cases, you might need strip and crimp at the same time and utilizing two different machines could take time (and it might cost you to have two separate machines).

Well, we hear you! Say no more!

The CF1000 (2 in 1 Strip/Crimp Behemoth)

While Phoenix Contact carries two different devices for Stripping and Crimping, with the CF1000, it incorporates both activities into a single powerful machine.  The user-friendly interface and easy operation make daunting task seemed effortless. The CF1000 is built to withstand heavy duty and prolong usages.

 

This monster of a machine can be summed up in 3 easy steps (never more, never less):

    1. Depending on whether you’re stripping or crimping, you can just flip the appropriate switches (there are only two options so no room for mistakes there) and then set the knob to the desired diameter for stripping.

    1. If you’re stripping, you could insert the wires in the hole and witness magic happen before your eyes. If you’re crimping and stripping, you need to dump the ferrules in the turbine-like bowl at the top of the machine. And then, naturally, magic happens when you insert the wire into the hole.

  1. And you’re done! Once the wires have been inserted (either stripping or crimping), you’ll get the end result.

Features Benefits
  • Easy navigation
  •  Option to Crimp or Strip wires in seconds
  •  1000 conductors can be processed an hour
  • Easy to use, no prior knowledge needed
  •  Built for heavy duty, long hours
  •  Comes with accessories to meet your industrial demands

 

The CF3000 (2 in 1 Strip/Crimp on-the-go)

Unlike the CF1000, Phoenix Contact’s CF3000 model is made with mobility in mind. While the CF1000 is ideal for industrial usage, the CF3000 allows both Stripping and Crimping on the go. Users only need to feed the reel of ferrules and the CF3000 will crimp/strip cables within a matter of seconds – just like a machine gun.

 I’ll show you (no stranger here. In 3 easy steps):

    1. Open the safety hatch and slide the safety panel. Insert the box of ferrules of your choice on to the safety panel shown below.

    1. Just like bullets on a machine gun, load the ferrules (or ammo as I call it) into the feed fixture as shown below. Once you’ve load the ferrules till you no longer can, that means you’re good to go.

  1. With the ferrules primed and ready, it’s time to put this baby to the test. Close the safety hatch and then you can start inserting the wires into the hole shown below. Be amaze at how fast the wires are being stripped and crimped.

Features Benefits
  • Portable and lightweight
  • Easy to use, no prior knowledge needed
  • 1200 conductors can be processed an hour
  • Option to Crimp or Strip wires in seconds
  •  Safe and secure usage
  • Comes with different ferrules and accessories for on the go wire maintenance

FOOD FOR THOUGHT: The CF1000 and The CF3000 may not look identical but their functions are similar, they both Strip and Crimp your cable within seconds. The only difference is that the CF1000 is great for industrial usage and requires a compression tank fitted into the machine. The CF3000, however, requires only electricity.

With that said, the CF3000 requires manual insertion of the ferrules to start the crimping process, whereas with the CF1000, you can pour in a whole box of ferrules and the job can commence.

So you see folks if you have any wire woes look no further. Phoenix Contact has the solution.

With business picking up you need to ensure that you concentrate more on customer servicing and the actual wiring job rather than menial task such as cutting, stripping and crimping wires.

Our products are made in Germany so expect the best in terms of quality and precision. They’re also built for safety and easy usage so anyone can get a head start.

Why Phoenix Contact’s Productivity Tools?

  • Saves time and effort – by relying on technology to automate task.
  • Provides consistent quality– preset your measurements and let the machines cut, strip and crimp to precise results.
  • User-friendly – Electricians, Technicians and even students have used our tools.

 

Schools and laboratories have used it, building contractors have used it, major global companies have used it and now, you could too!

*Psst…Did we say that it’s on promotion now?

For more information on our products, visit our promotional website below:

Cut, Strip, Crimp Promotion