A powerful UMTS router is now available with the new 3G modem
belonging to the Industrial Modem Line from Phoenix Contact. With its data transfer rate of up to 7.2 Mbit/s, it can be used in applications that demand
fast data transmission.
Category Archives: Industrial Electronics
Intelligent UPS for Industrial Applications
From |New intelligence for high system availability: Featuring IQ technology,uninterruptible power supplies (UPS) from Phoenix Contact ensure for the first time ever 100% power supply reliability when the line supply fails.
Measuring Devices for Energy Management: Measuring – Monitoring – Communicating
From |The new EMpro energy measuring devices from Phoenix Contact
acquire and monitor electrical parameters of systems and machines. Using
these network-capable devices, all measured data are centrally and locally
available.
New I/O Modules and Expanded Functional Scope in the SafetyBridge System
From |The new SafetyBridge I/O modules from Phoenix Contact
expand the SafetyBridge system when it comes to flexibility,
functionality, and application areas.
Safety Intergrity Level in Relation to Performance Level
From |I would like to share my experience which I encountered during my recent safety training to a customer in Malaysia. The topic was on Safety in Machine which the core topic was on the New Standard EN ISO 13849-1 which will be the successor to EN 954-1 ( EN954-1 will be invalid from 28-Dec-2011 )
I realized that 80% of the time I was explaining on the newly introduce Performance Level (PL) and Safety Integrity Level (SIL). During the discussion, there was a question from an engineer.
“In this case, in future we will all use the highest Safety Integrity Level (SIL) say SIL3 or SIL4 and our system will be good and safe”
Go Lean with Phoenix Contact managed switches!
From |New Compact Lean managed switches from the Factory Line product range of PHOENIX CONTACT are compatible with fiber-optic networks and offer special management features!
Protecting the IT Computer Centre
From |The protection concept for IT equipment must be able to handle both partial lightning currents and surge voltages, and requires customization appropriate to the data transmission system used.
FIREWALL! – Your trusted industrial security solution partner
From |Introducing the FL MGuard RS Firewall from Phoenix Contact that provides an industry firewall/router solution for individual protection of distributed automation systems.
Surge Voltage Protection for Field Equipment
From |SURGETRAB surge voltage protection devices are for all commonly used standard signals that are installed directly to the field equipment. This type of installation saves time and money, and an additional connection box for accommodating surge voltage protection is no longer necessary.
Losing the Wire, NOT the signal!
From |This week is a very exciting week for me; something very nice was loaned to me from Germany. This new babies of mine (well, at least for these 2 months) are these 2 wireless vehicles.