Category Archives: Industrial Electronics

Fast Profibus Extender with Surge Protection

From |

The new Profibus extender from Phoenix Contact enables straightforward integration of remote Profibus devices at data rates of up to 1.5 Mbps. The extender has two DSL connections per device. This means that in addition to point-to-point connections the extender can also be used to easily establish line structures with up to 30 devices.

Continue reading

Active Redundancy Modules Decouple, Monitor, and Control

From |

Two active Quint Oring redundancy modules are new in the Phoenix Contact product range. They increase the operational reliability by monitoring the redundant power supply solution from the output voltages of the power supplies through the power supply wiring up to the load, as well as the decoupling section up to the load current.

Continue reading

Intelligent Uninterruptible Power Supply for the Control Cabinet

From |

A new generation of uninterruptible power supplies now supplements the Quint Power product family from Phoenix Contact. Five new modules that can be snapped onto mounting rails are now available: For 24 V loads, the Quint UPS-IQ uninterruptible power supply has output currents of 5, 10, 20, and 40 A – and for loads with an input voltage of 85 up to 264 V AC, the Quint UPS-IQ supplies an output power of 500 VA.

Continue reading

Gigabit Modular Switch Now with Routing Function

From |

The Gigabit Modular Switch from Phoenix Contact now also supports the layer 3 function in order to route communications between individual subnetworks.

As industrial networks are becoming increasingly more complex, it makes sense to segment them and split them up into different networks in order to secure the appropriate level of data availability.

Continue reading

New String Current Monitoring Increases Efficiency of Photovoltaic Installations

From |

The new Solarcheck monitoring system from Phoenix Contact is a new reliable instrument for monitoring string currents in large-scale photovoltaic installations. The easy-to-integrate system detects losses in power caused by dirty or damaged panels. This enables targeted remedial measures to be taken so as to increase system availability and thus revenues.

Continue reading