Malaysia has experienced substantial economic development since the 1980s, resulting in increasing water demands in the commercial and industrial development centres. The Selangor / Kuala Lumpur region which is the political, commercial and industrial centre of the nation is the most important focus for these high demands which are expected to continue their rapid growth into the 21st century.
Category Archives: Controllers
Acquiring, Monitoring, and Communicating Energy Data
From |With the Basic and Flex energy data loggers, Phoenix Contact is offering package solutions that contain all components users require for configuring a data acquisition system. The packages are based on standard industrial components with integrated GSM/GPRS modem.
Cost-Optimized Telecontrol
From |For data transfer via GPRS, Phoenix Contact offers Open Data Port (ODP), an intelligent solution to monitor and manage telecontrol stations. The advantages of this solution lie in the reliable data transfer, the use of standard PLC and modem components, as well as standard industrial interfaces and protocols.
Phoenix Contact Datalogger+ – The Choice is YOURS!
From |Public utilities and refuse disposal plants are usually equipped with numerous external stations that must be connected to a central control system. In the case of water management for example, these are pumping stations, rainwater overflow tanks, wells or even complete system plants such as sewage treatment plant and waterworks.
Fast Compact Controller with Integrated Ethernet Interface
From |As a result of the integrated floating-point unit for quickly processing floating point numbers, the ILC 190 ETH 2TX controller from Phoenix Contact is especially suitable for fast closed-loop controls and basic motion applications. It can also be used for large applications thanks to its 1MB program memory.
EASY Control with Phoenix Contact
From |EASY compact controller systems with variety of options
The easy automation solution offers the customer a unique, inexpensive price/performance ratio as well as the possibility of higher flexibility and modularity at the same time.