CT(Current transformer) Terminals are used primarily in the energy/electrical power utility industry. When the current in a circuit is too high to directly apply to test or measuring instruments, a CT reduces the current proportional to the current in the circuit.
Yearly Archives: 2011
Case Study: Provincial Water Authority (Remote Pump Control System via SMS Technology)
From |Thailand’s Provincial Waterworks Authority alias “PWA” fully owned by the Thai Government, are responsible for the collection, production, distribution and reclamation of water in provincial Thailand. Driven by a vision to ensure all citizens of Thailand receive clean drinking water from all parts of Thailand.
EASY Control with Phoenix Contact
From |EASY compact controller systems with variety of options
The easy automation solution offers the customer a unique, inexpensive price/performance ratio as well as the possibility of higher flexibility and modularity at the same time.
Easy Wireless Networking
From |Lose the wire but not the signal!
If data is to be transmitted to a moving, rotating or mobile device, Industrial Wireless solutions are the answer. They are also recommended for temporary installations. What already has been practiced in the home and office areas for years can now also be successfully used in the industrial area.
EASY Wired Networking
From |One network, Countless possibilities!
Industrial Ethernet from Phoenix Contact offers you a powerful and complete network solution. Our network products range from the ethernet switches, serial converter, and network security module even wireless over ethernet.
Phoenix Contact Catalog available on Iphone & Ipad
From |Access Phoenix Contact Catalog on the go easily and conveniently with your Iphone or Ipad!
Marking System for Simple and Fast Labeling
From |The Thermomark Line is the new printing system from Phoenix Contact to mark terminals, cables, conductors, as well as equipment. It comprises two thermal transfer printers and a laptop on which the Clip Project marking software is installed.
Double-Level Plug Connectors for Many Connections in Restricted Spaces
From |The low-profile double-level DFMC/DMC plug connector system from Phoenix Contact allows up to 40 connections to be established in a small space.
Reliable Outdoor Cabling
From |Phoenix Contact is offering a new line of signal and data plug connectors that can be used outdoors.
Continue reading
High-Speed Wireless Communication with 3G Modem
From |A powerful UMTS router is now available with the new 3G modem
belonging to the Industrial Modem Line from Phoenix Contact. With its data transfer rate of up to 7.2 Mbit/s, it can be used in applications that demand
fast data transmission.