Tag Archives: housing

Future-Proof Your Devices With Phoenix Contact Modular Housing

From |

Housing is one of the key fundamentals for every household. Having the flexibility and availability of the right home will allow one to adjust comfortably when the family nucleus changes with time. Imagine a young couple that is planning for a family but is financially strapped and cannot afford a large home, obviously they will have to settle with a home that is smaller and more affordable. After a couple of years, their parents and children start to live with them. If they are more financially sound by then, the couple would need a place that is larger to accommodate a family of 7 people. The availability of homes in the market is key for the family of this size. 20 years down the road, the children would have grown up and moved out, and the family nucleus has strung back to just the couple living together. They will have the flexibility to downsize their home, or stay where they are currently residing.

In the same way, any device will need a housing to encapsulate the PCB. PCB design changes with time and with the demands and needs of the market, the PCB can become larger or smaller. A suitable electronic housing will need to provide the flexibility to adjust to the needs of the PCB and components.

Phoenix Contact offers a wide range of housing for our customers. From DIN-rail mounted, desk or wall mounted, to outdoor applications and handheld types.

For this blog, we would like to touch on the latest addition to our electronic housing family, the modular ICS housing system mounted on the DIN-rail that is for future-oriented automation devices.

What is so special about this product compared to other housing products that are available in the market? How is Phoenix Contact ICS modular housing unique from rest in the market?

Let’s start from the beginning, from the R&D standpoint.

Say today the R&D team needs to redesign a din rail mounted controller to be integrated with their new machine, they need to come up with the concept and proof of concept within 2 months. With Phoenix Contact ICS modular housing, we can fulfil their needs, taking into consideration of their demands of:

  1. Tight timeline
  2. Unique design required with their company logo
  3. Reasonable cost

Phoenix Contact has an online configurator that allows the customer to configure and select the right housing for their needs. The available options for the R&D engineers in our online configurator would consist of:

  1. Size of the housing to fit the size of the PCB.
  2. Single or twin PCB allowed in the housing.
  3. Accessories options on the upper and lower side of the housing – such as connectors, heatsink & fillers with vent, USB, RJ45, D-sub or antenna.
  4. If customer has any customise cut out required, we can do it accordingly with our existing fillers.
  1. T-bus connector available for the requirement of additional I/O modules.
  2. Front cover design options: Hinged transparent cover, flat closed cover or individualised custom cover. Customised printing and cut outs are also available for a nominal fee.
    No additional tooling charges involved!
  1. 3D simulation and CAD files available for download together with the part numbers of all selected parts and accessories.
  2. Heat simulation available if used for IC or electronic components that generate lots of heat.
    While many other companies charge for the thermal simulation, these are all freely available online!

Only Phoenix Contact provide such extensive product offerings and services which translate to:

  1. Cost effectiveness – No tooling fee on a new housing design with the advantage of our semi-customisable housing and free thermal simulation.
  2. Unique housing designed by the customer – Custom housing with printing and individualised covers.
  3. Quick sample service – samples can be requested online or through an email to the local representative.
  4. Future-proof and full proof design – Engineers can switch to the same series of housing with different sizes for future designs and Phoenix Contact will constantly be adding more accessories and services to value-add to the customers.

After all the designs are completed, engineers will need to transfer the information to their purchasing team and prepare for mass production. From the online configurator, you can download the part numbers of every piece part in an excel spreadsheet. This will seamlessly translate the information from the R&D team to the purchaser with extensive information in terms of:

  1. Drawings
  2. Pricing
  3. Piece parts and manufacturing part numbers
  4. One supplier for the fully established housing requirements from material, printing, and customisation.

A well-thought-out product, the ease of the production process cannot be neglected. Phoenix Contact has designed a mounting device that is able to assemble all the different housing configurations, and shorten the assembly process to mere seconds. That is both innovation and cost saving. To find out more about the mounting device and the operation, see this link.

Reach out your local Phoenix Contact sales team to find out how we can help launch our new projects effective and efficiently.

Looking forward to hearing from you soon.

Display Carrier System: Enclosure for Display system

From |

Display Carrier System
The Display Carrier System protects mobile and stationary displays from mechanical impacts as well as from dust and water spray. Typical areas of application include laboratory and analysis technology as well as healthcare and building automation.

Features
Protection degree: IP54

Membrane keypad

Membrane keypad

Temperature range: -20℃ to +50℃
Display size: 5.7”, 7” and 15”
Material: shock-resistant ABS plastic
Color: light gray (RAL 7035)
Advantage for customer
Easy integration of displays

LCD Display

LCD Display

Direct entry possible via membrane keypad
Convenient handling
Battery integration
Customize versions for special requirement
Market Applications
Building automation Phoenix Contact Panel PC
Industrial
Monitoring System

If you would like to find out more about Phoenix Contact’s Display Carrier System, check out our website or leave us your contact and I will get in touch with you soon.

Importance of choosing the right PCB enclosure

From |

What is considered important when it comes to choosing the right PCB enclosure. Let us guide you through the process.

Price? Style? Service & support? Reputation of the supplier?

In the matter of fact, all of above are essential. The engineers should select the enclosure at first and then choice the mechanical & electronic components to suit the enclosure.
We need to consider

Material
The 3 common plastic enclosures are ABS, Polycarbonate, Polyester which are high functionality, light weight, flexible in design.

The Ingress Protection
The ingress protection classification DIN EN 60529 determines and rates protection against solid particle (e.g. dust) as well as liquid incursion.

The letters IP (ingress protection) is followed by a two-digit number; the first digit indicates the level of Solid particle protection and the second digit indicate Liquid ingress protection. IP Code

Environmental Considerations
How the enclosure will last over many years of operation depends on how well you evaluate the environmental impact of elements such as UV rays, temperature, airborne debris, etc.
Different materials offer varying degrees of impact resistance.

Dimensions
The internal and external dimensions of a PCB enclosure is extremely important. Sadly, in many cases, the PCB is chosen first and this makes it difficult for the engineer to source the best fit enclosure solution.

Modification of Standard Enclosures
The enclosure supplier may need to support modifications with value-added services that include drilling, milling, printing, color, etc. Some suppliers can even provide advance services like fitting membrane keypads, displays on the enclosure, etc as a complete solution.

Ease of Assembly
A complex PCB design may make it difficult to assemble electronic and mechanical components in the enclosure, which make is an important point to consider when selecting an enclosure.

Range of PCB Enclosure

Check out Phoenix Contact’s range of enclosures here

We, at Phoenix Contact, understand your problems and offer a wide range of options for shape, color, and function when it comes to choosing the right enclosure. Whether on a wall or on a DIN rail, from light gray to sky blue, narrow or wide, many many to choose from. With the two new enclosures, Universal case system (UCS)  and Environment case system (ECS) added into the selection, it is much easier to choose your enclosure.

Please view the Enclosure brochure.

Want to find out more? Feel free to contact us at marketing@phoenixcontact.com.sg!

The New UM-ALU Housing

From |

Phoenix Contact offers rugged aluminium housing HC-ALU for control cabinet and field robust electronics housing.

The new UM-ALU housing provides effective protection for your electronics against thermal and electromagnetic influences. It also features a trapezoidal cross section and is suitable for use with handheld devices for mobile data capture or wireless communication.

Continue reading →

600V Power Connector with UL Approval

From |

Suitable for the ME and ME MAX family of housings from Phoenix Contact, and in addition to the classic plug connections for 250 V, the GMSTBO 2.5 HV high-power base strips with matching GMSTBT 2.5 HV screw plugs are now available for compact device applications in the area of power electronics.

Continue reading →