So do you want to reduce installation, assembly and maintenance costs? Then convince yourself of highly efficient communication solutions based on wireless signal transmission.
Tag Archives: automation
Gigabit Modular Switch Now with Routing Function
From |The Gigabit Modular Switch from Phoenix Contact now also supports the layer 3 function in order to route communications between individual subnetworks.
As industrial networks are becoming increasingly more complex, it makes sense to segment them and split them up into different networks in order to secure the appropriate level of data availability.
Industrial PC Becomes a Control System
From |Now, a standard industrial PC can handle any control task. The PC Worx RT Basic software PLC from Phoenix Contact transforms any industrial PC into a fully fledged control system. Programming, visualization, and control can therefore be combined in just one device.
Acquire up to 50 Machine States at Once!
From |Phoenix Contact extends its PSD signaling column product range to include the WIN (Wireless Information Network) wireless system. Using this wireless system, the signal states of up to 50 signaling columns can be wirelessly transferred.
Wireless HART Adapter: Wireless Data Transfer in Process Technology
From |The RAD-WHA-1/2NPT Wireless HART adapter from Phoenix Contact simplifies and speeds up the retrofitting and expansion of systems with 4–20 mA signal cables. The adapter is connected to an existing HART device in the field to transfer HART data wirelessly into a new system, while the original system based on just 4–20 mA remains intact.
Go Lean with Phoenix Contact managed switches!
From |New Compact Lean managed switches from the Factory Line product range of PHOENIX CONTACT are compatible with fiber-optic networks and offer special management features!
FIREWALL! – Your trusted industrial security solution partner
From |Introducing the FL MGuard RS Firewall from Phoenix Contact that provides an industry firewall/router solution for individual protection of distributed automation systems.
Experience with Inline Bus Couplers IOs
From |Recently we just got an order of hundreds Modbus couplers. Since the configuration is made default factory settings, the customer requested our help to do the configuration for them.
Can you imagine hundreds of bus couplers to be set up?
You’ll need to power ON and OFF the bus couplers and set the registers that you need to change. But infact, the works were finished in just one day and there were more than 300 pieces of bus couplers to be configured! Thanks to the snap-in power connectors of the couplers itself; it does save time for us to connect the power to the device every time we need to change to the next coupler to be configured.