Category Archives: Industrial Components

Choosing the Right Signal Conditioner

From |

Basic 4-20mA current loopSensors and other devices with 4-20mA current loop output are very popular in industrial fields. We can find them from Process Control to data logging systems. A basic current loop has parts as stated below:

  • Sensor: a device which draws current from its power source in direct proportion to the value it measures (level, pressure, etc.).
  • Power source: supplies DC power to sensors or any device in the loop.
  • Reading devices: a PLC, a controller or data logger which reads the current value provided from the sensor and uses it for the next step of controlling or data logging.

In order to isolate, convert, filter and amplify or duplicate control signals we use signal conditioners. Signal conditioner makes a simple 4-20mA current loop into a field loop and control loop like below:

The devices in both the field loop and the control loop need to be powered. They can be powered by a DC Auxiliary power supply or by another active device in the loop. That being said, we have many types of Signal Conditioners (According to how it is powered or can it supply power for other device) that can be used in this scenario.

Types of sensors

The most common 4-20mA sensors in industrial fields are 4-wires sensors and 2-wire sensors. The difference lies in how they powered.

A 4-wire sensor is an active device which has a separate power supply for itself (from DC or AC power supply).

4-wire sensor

4-wire sensor

On the other hand, a 2-wire sensor is a passive device which draws power from a DC auxiliary power supply in the loop or from other active devices in the loop (like a repeater power supply signal conditioner)

2-wire sensor

2-wire sensor

Types of 4-20mA Signal Conditioners:

  • Passive Signal Conditioner: A passive signal conditioner doesn’t need a separate power supply for itself. It draws power from the field loop or control loop. This means there are 2 types: one powered by a field loop and one powered by a control loop. As passive signal conditioners can cause a drop in voltage in the loop, if there are too many passive devices in loop it could lead to inaccuracies in the measured values. In the picture below is a field loop powered signal conditioner with 2-wire sensor, where the devices in the field loop are powered by an auxiliary power supply.

  • Active Signal Conditioner: This type of signal conditioner is powered by a separate power supply so it doesn’t cause voltage drops in the loop. It can also provide power for the control loop. For example, an active mini MCR Pro signal conditioner can drive up to a 600 Ohm load in a control loop. The field loop still needs an auxiliary power supply when using a 2-wire sensor. Pictured below is an active signal conditioner and 4-wire sensor. In the control loop is a passive analog input controller.

  • Repeater Power Supply Isolator: This type of signal conditioner is powered by a separate power supply and it can supply power for the sensor’s loop and also for the control loop (with a maximum load of 600 Ohms). It can be used for 2, 3 or 4-wire sensor without the need of a power supply for the field loop.

So depending on the type of application, we can choose the right 4-20mA signal conditioner. Based on information about the type of sensor, whether the field loop has an auxiliary power supply as well as if the control loop has a passive or active controller, we can choose the suitable 4-20mA signal conditioner.

If you have any questions, feel free to contact us!

Comprehensive Solutions from Phoenix Contact

From |

In today’s market, customers are looking for vendors who can value add, making them stand out in the sea of competitors. One of the orders we often receive is to supply a complete package system from the cabinet to the components level.

Our collaboration with local partners makes Phoenix Contact the preferred solutions provider. Backed by comprehensive components from Phoenix Contact, control cabinets supplied and superior engineering services are the root of our initial success in the Process market in Indonesia.

Problems which the customer faced before are as follows:

  • Having to contact several vendors for the different scopes of supply, such as electrical components, control cabinet, wiring and installation
  • Managing the delivery time for each and every vendor
  • Complexities during the project management
  • Uncompetitive prices

With a complete solution provided by Phoenix Contact & our partners, customers will only have one point of contact related to all cabinet and components project requirements. This will ease the difficulties faced in terms of project management and therefore will ultimately reduce their overall cost.

Take a look at the example below of our recent success at this comprehensive solution.

Application: Metering Systems

Scope of supplies:

  • Control cabinet 800W x 800D x 2000H (in mm) & cabinet accessories
  • Redundant power supply system by Quint Power (QUINT-PS/1AC/24DC/10)
  • I/O Surge protection system with indicator: Termitrab Complete (TTC-6-1X2-F-M-24DC-UT-I)
  • Current splitter: MACX MCR-SL-RPSSI-2I
  • System cabling: Varioface (FLKM-D25 SUB/B + CABLE-D25SUB/B/S/100/KONFEK/S)
  • Front mounting industrial power socket and RJ 45 socket IP65
  • Interposing relay: PLC relay series (PLC-RSC- 24DC/21)
  • Accessories: fuse terminal block, AC socket power, cable duct, terminal & device marking, etc
  • Engineering services: wiring and installation, FAT supports

Below are the images of our solution:

Front mounting AC socket & RJ 45 socket

Front mounting AC socket & RJ 45 socket

Control Cabinet and wiring/installation services

Control Cabinet and wiring/installation services

Varioface system cabling

Varioface system cabling

Redundant power supply, interposing relay, fuse terminal block

Redundant power supply, interposing relay, fuse terminal block

TTC Surge protection with indicator and MACX current splitter

TTC Surge protection with indicator and MACX current splitter

If you would like to find out more, don’t hesitate to contact us!

CLIPSAFE Junction Box

From |

When you ask for a Phoenix Contact CLIPSAFE Junction Box, you receive a high quality product with a range of empty enclosures, made of stainless steel and polyester. CLIPSAFE Junction Boxes can be used in hazardous environments, and upon approval, can be installed in potentially explosive areas.

The 3 main classes of junction boxes are as follows:

  1. Ex Stainless Steel Empty Enclosures
  2. Ex Polyester Empty Enclosures
  3. Polyester Empty Enclosures

 

  1. Ex Stainless Steel Empty Enclosures

The CLIPSAFE stainless steel Ex enclosure product range provides comprehensive protection for your applications in industrial environments and in process technology. The product range consists of enclosures in sizes of up to 1000 x 1000 x 300 mm. Upon request, Phoenix Contact can provide ATEX and IECEx-approved junction boxes.

  1. Ex Polyester Empty Enclosures (GRPs)

The comprehensive range of CLIPSAFE polyester Ex enclosures provide comprehensive protection for your needs in potentially explosive areas. Upon request, Phoenix Contact can provide ATEX and IECEx-approved GRPs.

  1. Polyester Empty Enclosures

The extensive standard CLIPSAFE polyester enclosure range provides robust standard enclosures for industrial environments as well as for non-explosive areas in process industry. The enclosures are suitable for control boxes and junction boxes, suitable for most of your requirements.

We can customize the enclosures to your specifications with threads, bore holes complete with components and cable glands. And custom control boxes with electronic components are available on request.

Interested to find out more? Please send us an email at marketing@phoenixcontact.com.sg

Heavy-Duty Connector Solution for Machine Building

From |

Phoenix Contact’s Heavy-Duty Connector is an ideal solution to replace conventional cable glands if you want to have an easy and quick physical disconnection of power or signal. Many machine building system integrators are facing the following problems with regards to the cable gland design:

  • Difficult to dismantle and disconnect
  • Consumes a significant amount of panel space
  • Errors during installation

After going through the product technical information, our machine builder customer decided to replace most of the cable glands with Heavy-Duty Connectors due to their easy application. a photo of their panel is shown below.

Control Cabinet

Fig 1: Control Cabinet

Heavy-Duty Connector

Fig 2: Heavy-Duty Connector

Feature of Heavycon:

  • High corrosion resistance
  • Ensures secure power, data and signal transmission
  • Flexible single or double locking latches
  • Mounting and plug-in Compatible
  • EMC-ready
  • Ideal for operating in harsh environments

If you need any technical advice on your current project, feel free to contact us! I believe we can be your trusted partner to provide suitable solutions to fit your needs!

Three Good Reasons Why You Should TRADE IN Your Printer

From |

Phoenix Contact has a wide variety of printing systems, capable of meeting all sorts of marking requirements, ranging from terminal markings, wire & cable markings, equipment labels and plant markings!

Terminal Marking

Terminal Marking

Wire & Cable Markings

Wire & Cable Markings

Equipment Marking

Equipment Marking

Plant Marking

Plant Marking

Label On-the-go

 

Every label requirement you need for your panels, inventory, workshop or even wiring is possible with our variety of printers in place! Print at your own convenience and save the hassle of pre-ordering them. You can also customize our printers to cater to your own specific printing needs, avoiding wastage due to unused or wrong labels!

 

What’s more is that Phoenix Contact is having a TRADE IN scheme now!

Three Good Reasons Why You Should TRADE IN Your Printer:

  1. Get the most bang for your buckAll your marking needs for rolls and cards

Why not save your company some money if you can let go of your old printer, in exchange for a discount off the new one? The trade in scheme is meant to give customers more incentive to purchase a new printer from us! Speak to your local sales representative to get more information on how much discount you can get off your printer when you trade in yours now!

  1. Upgrade your current technology

High Volume Printing

Have you been using your printer for many years, unaware of how much technology has progressed? Printing speed has increased tremendously over the years, not to mention the quality of prints! So, if you are wondering if it is time to get a better printer for greater efficiency, it is still not too late! The trade in scheme is the perfect platform for you to enquire more about the technology that goes into Phoenix Contact printers.

  1. Save the environment

Instead of chucking your old printer in a corner, taking up space and collecting dust, we welcome all your used printers to Phoenix Contact, and you even get a discount when you purchase one from us!

If you still insist on disposing of your old printer, there are tons of toxins inside printers that hurt the environment! So, start thinking about our trade in scheme and do your part to save the earth!

Click here now if you are interested to get a trade in!

Cable Entry System – CES

From |

Have you ever left your earphones in your pocket and when you wanted to use them again, they emerge as a tangled ball of mess? Annoying, isn’t it?

Well, the wiring of current and conventional electrical panels brings about a similar problem. The above picture shows its set up and at a glance, three words pop up in my mind: Complex; Costly; Time-consuming.

So why is this so?

Firstly, in the current system, multiple holes of different sizes need to be drilled in accordance with the cable sizes. Imagine the hassle having to drill ten holes of different diameter just to see messy wires intertwined together.

Next, a common occurrence to such wiring systems is the need to add additional cables. If you are lucky, there will be enough space on the flange plate to drill the extra holes. However, if the space is insufficient, or if you need larger holes for new cables, you would most likely have to replace the entire electrical panel and redo the entire wiring system from scratch. Not only does this add on to the hassle, it also adds on to labour and cost.

Lastly, conventional wiring systems require more time to rectify problems in communication. This is due to the difficulty in identifying specific cables especially when they are bundled together. The troubleshooting process thus leads to longer downtime which means financial losses for the company.

The Solution

Phoenix Contact has thus come up with a solution to eliminate this problem. Our Cable Entry System (CES) comes with specific features to tackle the hassle of the conventional system.

Firstly, only one or two holes would have to be cut to enable installation of up to ten cables in the system, greatly reducing the set up time. Furthermore, the CES can cater to different cable diameters ranging from 2mm-24mm. All these can be easily installed by mounting the sleeves of varying sizes on to the robust metal reinforced frame.

Next, additional cables can be installed by removing the blind sleeves from the extra cable holes provided by the CES. In the event that the existing cable configuration has to be amended, the CES allows for easy reassembly just by replacing the sleeves with those of different cable diameters. This eliminates the trouble of cutting out new holes on the flange plate.

Lastly, the CES allows cables to be easily identified as the rectangular frame organizes the sleeves holding the cables in an orderly manner that is easy on the eyes.

Besides tackling the inconveniences of the conventional electrical panel wiring, the CES offers protection class of IP54, making it suitable for harsh environment conditions.

If your current electrical wiring system reminds you of your ball of tangled earphones, it‘s about time you switch to Phoenix Contact’s Cable Entry System. Our CES will be the solution to increasing your productivity and cost saving to your electrical panels wiring.

Interested to find out more? Contact us at marketing@phoenixcontact.com.sg!

System Cabling Solution for Process Industry

From |

One of the challenges which panel builders in the process industry face would be space saving on control cabinets. Many Process retrofitting jobs require panel builders to ensure the quantity of cabinets remain even though additional I/O’s are added. System cabling is one of the best solutions to save space in control cabinets.  One of our panel builders solved their problems by replacing terminal blocks with our VARIOFACE Interface Module for the project.

Problems:

  • Additional 150 I/O’s on current system
  • Additional Controller Module
  • Cabinet Quantities need to be remained

After going through the product technical information, panel builder engineers decided to replace most of the signals with our VIP Interface Module due to space constraints. There are a total of 115 units of VIP-3/SC/D37SUB/F installed in this project. Photos of the panel are shown below.

Control Cabinet

Fig 1: Control Cabinet

VIP Interface Board

Fig 2: VIP Interface Board

Features of Interface Module:

  • Compact design of control cabinet space
  • I/O marking for field wiring clearly identified
  • Flexible marking of modules
  • Metal mounting foot allows for easy installation and removal on din-rail
  • Allows flexible module mounting positions

In addition to the space saving advantage, the site engineer shared that it is also time saving and fault free during the wiring termination. When the panels are delivered, the end user saves valuable time when installing and troubleshooting

If you need any technical advice on your current project, feel free to contact us. I believe we can be your trusted partner to provide suitable solution to fit your application!

LV Compartment for MV Switchgear

From |

Box by box towards Smart Grid 1: LV Compartment for MV Switchgear

The gradual shift towards the much vaunted Smart Grid structure has been gathering steam in the last few years. While much of the excitement has been generated from the immense potential of what a fully completed Smart Grid system can bring (for example, higher reliability at reduced cost), Grid operators, independent power producers and their team of engineers are facing real difficulties in implementing such systems today. It is easy to talk about wanting to implement technologically advanced systems, but when it comes to actually executing the projects to implement such solutions, the complexity surrounding such implementations comes to the fore.

Much of this complexity arises because of the vast variety of applications within the industry. It is particularly difficult to find the right set of products that are suitable for the application, reliable, fast to set up and easy to manage. For example in Transmission and Distribution substations, there will minimally be systems for transformers, shunt reactors, switchboards, intrusion detection monitoring systems and each of these systems can consist of smaller sub systems. For example, in monitoring a switchboard, we can monitor downstream load current for energy balancing; micro current fluctuations for signs of partial discharge or even for predictive maintenance; door contact monitoring for physical security and the list goes on. Each of these systems will require the right set of products and will have to be linked in this web of madness. Imagine the chaos!

At Phoenix Contact, we recognise this difficulty. While we have many solutions for Energy Industry that we are always sharing with the various stakeholders, in this series of blog articles, we will be examining how we help to simplify the implementation of Smart Grid. We will do so by examining the building blocks of a system – the individual panels which form up a system; and we will do so box by box. This first article will be about LV Compartment of MV Switchgear and we will delve straight into the 3 problems switchgear builders and grid operators are facing!

Problem 1: How do I collect signals from my switchgears and transform it into IEC61850?

The completed substation topology will involve decentralised controls where IEDs are placed at high voltage equipment (on transformers and switchgears) itself. Even when it is not completed, communications from the bay control cabinets and protection devices to the substation control system are being converted to IEC61850 as IEC61850 has proved to be a superior communication protocol and standard to reduce downtime and increase reliability of the grid. Therefore, it is only a matter of time before all switchgears are converting signals from the circuit breakers and all other auxiliary signals into IEC61850 data. However, examining the LV compartment of switchgears today, the signals are still being passed out with many copper wires or connected to numerical relays. These present two clear drawbacks:

  1. There are a lot of copper wires going out of the panel or into numerical relays. The associated cost includes requiring marshalling or pilot cabinets and related components and regular maintenance to check if the connections are good. In addition, it is difficult to isolate where the fault is when there is a loss of signal. In the worst case scenario, there might even be accidental shorting resulting in severe downtime!
  2. Numerical relay and its I/O cards are expensive.

These result in higher initial cost and higher eventual maintenance cost with downtime not necessarily minimized, especially in the event of loss of signal.

Using of a Bus coupler capable of communicating via GOOSE and MMS will solve both of these problems. Using Phoenix Contact bus coupler as an example, the signals can be easily inserted and aggregated as IEC61850 data. It certainly reduces the number of cables leaving the cabinet and with the light indicators, you can see clearly which connections are good without requiring extra tests. It is also of lower cost compared to numerical relays’ IOs while communicating perfectly with them.

Problem 2: There are too many wires, how can we manage them better?

Being the founder of the original ceramic terminal block, it is already tempting to say that Phoenix Contact is the best at solving this! But in the last few years, we have developed more data connectors to put us in a better position to solve this for switchgear builders!

We have an extremely wide range of terminal blocks for every applications and needs. We have demonstrated to be able to meet each and every customers’ unique demands, be it requiring pluggable solutions, fastest connection technology, space saving, you name it, we’ve done it!

In this article, we would just like to highlight how a commonly used connector for switchgears has developed to adapt to Smart Grid. In the past, our Heavycon (heavy duty connector) was often sold to connect the LCC and Bay cabinets. This enabled quick connection on site.

However, these connectors are usually for loose copper wires only. Although you can strip an Ethernet/serial connector to use such connectors, these connectors does not cater very well for the shielding required for data connector. Therefore, Phoenix Contact has developed a modular connector, allowing you to use your data connectors directly! This modular connector even allows you to have connectors which allow for high power!

Problem 3: With more signals being collected, there will be more testing to be done. How can we ensure we are safely doing the testing all the time!

Every so often, testing needs to be done on the current transformers and voltage transformers regularly. For current transformer especially, if not done right, explosions can happen. Currently, the shorting and breaking of circuits are done manually by hand (yes you read that right) and as you can imagine, explosions lead to death.

To solve this, Phoenix Contact has developed our test disconnect system (FAME) where shorting is done automatically and it is fool-proof!

Instead of using terminal blocks that are switched manually, you can replace it entirely with FAME and from then on, every testing procedure will be done how it is meant to be done: SAFELY.

We have assembled this product into a demo box along with other products that Phoenix Contact offers for LV Compartment for MV Switchgear. If you will like to have a look at the demo box up close, do contact us at marketing@phoenixcontact.com.sg and we will get in touch!

Back to Basics – Basicline Series

From |

Phoenix Contact is well known for its terminal blocks and connectors. Phoenix Contact’s success was also partially attributed to its Back to Basics campaign, which aimed to drive the business to meet all market requirements.

One particular Back to Basics product series worth mentioning is the basicline series – great quality connectors and terminal blocks that are also cost competitive.

The basicline series had helped many Phoenix Contact customers to have reliable and robust connectors at affordable pricing. This enabled customers to produce devices that are both cost competitive and reliable.

Many customers that have faced challenges in producing cost competitive devices for building automation, door access, security etc. are satisfied with what basicline has to offer.

In addition, basicline has helped to solve problems arising from using Asian-branded connectors with lower quality and reliablity issues.

Below is an example of a basicline series product.

Advantages

  • Tin plated surface contact prevents rust overtime and provides consistent current rating
  • Non-frisky plastic housing and strong PA 66 provide robust and reliable usage
  • Strong price to performance ratio
  • Available in 3.50mm, 3.81mm, 5.00mm and 5.08mm pitch
  • Pluggable connectors and terminal block
  • Comes in green, black and grey. For other colours, kindly contact our salesperson
  • Optional marking and profiling
  • Available in 2 – 16 poles
  • Pluggable header available in horizontal and vertical positions

Interested to find out more? Contact us at marketing@phoenixcontact.com.sg!

DIN Rail Plug-in Terminal Block

From |

Today I would like to share a bit on the little guy that usually goes unnoticed in our daily life.

The UMSTBVK Series – DIN Rail Mounted Plug-In Terminal Block

This product seemingly portrays images of an underdog. It has never been in the limelight by nature. That is due to the limited exposure that the UMSTBVK connectors are exposed to.

Other products such as the “UT 2,5/1P” Terminal Blocks & “UM 25” Interface Module are more commonly used in market, whereas the UT 2,5/1P terminal blocks are mainly used for high power feedthrough, and UM 25 interface modules are mainly used for signal feedthrough.

UT 2,5/1P

“UT 2,5/1P” Terminal Block

“UM 25” Interface Module

“UM 25” Interface Module

Comparing the trio, the UMSTBVK is actually a hybrid between the two.

Where are these products commonly used?

It is commonly used as a middleman between the controller and the field devices.  As the controller is usually the “Heart” of the entire system, hence, the use of UMSTBVK will come into place as one of the essential parts of the system, being “The Bridge” between the Controller and the field devices.

It will allow easy testing, maintenance and replacement for users, minimizing the need to connect and disconnect the wires that are already installed onto the main controller and field devices.

What are the most common objections as to using the UT 2,5/1P or the UM 25 modules integrated into their systems / devices / instruments?

  • Indeed these are convenient, but take up too much space.
  • Nice products, but pricing not very competitive.
  • Connectors for UT 2,5/1P has only one direction of wire entry, it compromises on the space taken in terms of depth.
  • There are no other options except 10 / 18 position for the UM25 Interface Module.

The UMSTBVK Series terminal blocks might not be the perfect solution, but it has the best features of both of its predecessors:

  • Great Versatility – Multiple variant of different number of position to choose from, and can be used on both NS35 / G DIN Rails.
  • Time-Saving – Minimizes time needed for assembly of terminal blocks into desired number of positions & eliminates the need to purchase additional accessory like “End Covers”
  • Readiness – “Clip and Go” type of product.
  • Cost Savings – competitive pricing based on per pole, which can achieve savings up to 30% per pole for the whole set including the plug in connectors.
  • Spoilt for Choice – You have multiple types of connectors that are compatible to choose from, with various connection technologies & angle of wire entry that you may prefer.
  • Screw Connection
  • IDC Connection
  • Push In connection
  • Crimp Connection

Up to this point, I see great potential for the UMSTBVK product family to shine in coming years.

Do you agree with me? If you do…

Do feel free to contact us at marketing@phoenixcontact.com.sg for more details to help you understand this better!