Category Archives: Industry Cabinet Connectivity

System Cabling Solution for Process Industry

From |

One of the challenges which panel builders in the process industry face would be space saving on control cabinets. Many Process retrofitting jobs require panel builders to ensure the quantity of cabinets remain even though additional I/O’s are added. System cabling is one of the best solutions to save space in control cabinets.  One of our panel builders solved their problems by replacing terminal blocks with our VARIOFACE Interface Module for the project.

Problems:

  • Additional 150 I/O’s on current system
  • Additional Controller Module
  • Cabinet Quantities need to be remained

After going through the product technical information, panel builder engineers decided to replace most of the signals with our VIP Interface Module due to space constraints. There are a total of 115 units of VIP-3/SC/D37SUB/F installed in this project. Photos of the panel are shown below.

Control Cabinet

Fig 1: Control Cabinet

VIP Interface Board

Fig 2: VIP Interface Board

Features of Interface Module:

  • Compact design of control cabinet space
  • I/O marking for field wiring clearly identified
  • Flexible marking of modules
  • Metal mounting foot allows for easy installation and removal on din-rail
  • Allows flexible module mounting positions

In addition to the space saving advantage, the site engineer shared that it is also time saving and fault free during the wiring termination. When the panels are delivered, the end user saves valuable time when installing and troubleshooting

If you need any technical advice on your current project, feel free to contact us. I believe we can be your trusted partner to provide suitable solution to fit your application!

Phoenix Contact – Your Partner in Safety and Reliability for Railway Industry

From |

RailwayPhoenix Contact has been serving the railway industry for decades, especially for rolling stock and signalling. Safety and reliability has always been our number one concern when developing products for railway applications.

Safety on Board

The basic requirement for safety and reliability is standard compliance. Phoenix Contact has been certified by the International Railway Industry Standard (IRIS) since April 2008 and this standard is based on the quality management standard DIN EN ISO 9001, which has been extended with international railway-specific requirements. The ongoing tests during the development and production cycle of the products are essential to guarantee the product quality.

On top of that, all rail-specific products from Phoenix Contact fulfill the standards of DIN EN 50155, an international standard covering rolling stock; DIN EN 50121 electromagnetic compatibility; and EN 45545, fire protection on rail vehicle. Besides, shock and vibration test, material test and other fire protection is also critical for the railway application.

Safety should not be limited to the big ticket items and should even be extended to the passive component level. For example, the cable markings like shrink sleeve should be halogen-free and fulfill DIN 5510-2 with an oxygen index of 34.9%. besides being halogen-free, the cable ducts should enable individual bars to be broken without using any tools or resulting in any burr through defined breaking points according to EN 45545-2 (R22/R23:HL3). Behaviour in fire is another key concern and the plastic used for Phoenix Contact’s terminal blocks is halogen-free polyamide PA 6.6; which meets the highest safety requirement of UL 94 V0.

Push-in Terminal Blocks and Marking

Push-in Terminal Blocks and Marking

Cable Management

Cable Management

Network on Board

Nowadays, commuters demand for “Internet on board” has made the information and infotainment systems essential in trains. The M12 network connectors with a mechanically robust design, in compliance with IEC 61076-2-101, together with high quality cables meeting the requirement of EN 45545-2 will ensure reliable communications. The heavy-duty connector, compliant with IEC 61373, with modular contact inserts form a flexible and safe transmission of signal and power circuit on rolling stock carriage connection and simultaneously ensures comprehensive protection in the event of electromagnetic interference fields.

Halogen-free Polyamide PA 6.6

Halogen-free Polyamide PA 6.6

M12 Network Connector

M12 Network Connector

Surge Protection

Surge voltages and lightning strikes are common issues in signalling, hence the surge protective device (SPD) become significantly important to maintain reliable signal transmission. Phoenix Contact’s SPD has been tested according to IEC 61643-21 and the plug can be disconnected for test and maintenance by using the portable test laboratory. According to IEC 62305-3, the SPD must be tested regularly and the test values should be documented and traceable. Additional features like multi-stage monitoring (green – operating, red – fail and yellow – reach performance limit) for predictive maintenance and remote signalling for early detection of overloaded SPD can help to further enhance reliability.

HEAVYCON HPR

HEAVYCON HPR

HEAVYCON Modular Inserts

HEAVYCON Modular Inserts

Signal SPD with multi-stage monitoring (PT-IQ)

Signal SPD with multi-stage monitoring (PT-IQ)

Signal SPD with remote signalling (TTC)

Signal SPD with remote signalling (TTC)

Power Supply

The power supply unit (PSU) is used to convert main AC to low-voltage regulated DC power and it should at least be compliant with EMC Directive 2014/30/EU, IEC 60950-1, DIN EN 61558-2-16 and UL 508. To ensure smooth operation and maximum uptime, the redundancy setup of the power supply cannot be overlooked.

A redundant system can made up of two power supplies and a diode or Phoenix Contact’s O-RING to prevent back flow of current. An ORING being a more advanced and modern redundancy module compared to the diode, comes with auto-current balancing (ACB) technology which ensures the power supplies work equally hard. This enables the power supplies to have a longer and more consistent lifespan.

The redundancy status as well as the status of the ORING can be monitored, whereas this cannot be done with a DIODE. The PSU becomes more reliable and dependable when it is capable of sending analogue signals to control system on measurement values such as real time current, voltage and power for early detection of operational fault as well as critical information to the user.

QUINT 4 Power Supply With Diode

QUINT 4 Power Supply With Diode

QUINT ORING with ACB

QUINT ORING with ACB

Transporting You into the Future

Phoenix Contact will continue to develop the products or solutions that suit railway application and safety and reliability will always be the top concern on top of ease of installation, operation and maintenance.

To find out more about the solutions that Phoenix Contact has for the railway industry, check out our website or leave us your contact at marketing@phoenixcontact.com.sg and I will get in touch with you as soon as I can.

Make-before-break – Terminal Blocks for CT Test

From |

Make-Before-Break

Make-Before-Break (MBB) is a term “Denoting a switch or other device in which a new electrical connection is made before the existing one is broken”. In short, it simply means, shorting the circuit before disconnecting it.

You may know about MBB when purchasing a relay. But do you know there are terminal blocks designed with MBB in mind too? These MBB terminal blocks can usually be found in power industry applications.

For those who are familiar, you may have come across this term (MBB) during a Current Transformer (CT) testing on a protection relay. However, do you know the importance of ensuring MBB when conducting a CT test with your Terminal? Or what the consequences will be of not having a terminal blocks that comes with a MBB feature during the test?

Protection Relay

A CT will certainly be at risk of being destroyed or even worse (Explosion!) if the secondary is left open circuit while the primary current is present. This is due to the insulation failing from the “higher than rated” voltage that occurs. Therefore it is extremely important to ensure MBB before conducting a live testing. A good terminal block with MBB feature will definitely help you provide the extra mile in ensuring safety.

How does the MBB terminal blocks function and what does it look like?  Here are some good examples of a good MBB terminal block.

  1. A good MBB terminal block must have the feature where shorting is always present first before you are able to break the circuit. It would be best if the terminal blocks are able to automatically perform the short circuit for you whenever it is being disconnected during the CT test.
    Short Circuit function closed Short circuit function open
  2. Clear indication of Short Circuit and disconnection must be visible and this allows your engineers to have an ease of mind during testing.
    PTME
  3. Good MBB terminal blocks should have safe and easy to operate features. Having said that, these features can help to cut short the time while testing (shorten the risk) and ensuring the safety of the person that is conducting the CT test.
    PTME Terminal Blocks for CT Test

So where can you find good MBB terminal blocks for your applications? Phoenix Contact, of course!

With 94 years of experience manufacturing and designing terminal blocks for the Power Industry. Phoenix Contact has never stopped developing new innovative testing terminal blocks that will suits your application, at the same time ensuring safety and quality.

For more info, check out this video of our PTME terminal blocks or visit our website!

If you have more inquiries, feel free to contact us at marketing@phoenixcontact.com.sg and we will get back to you as soon as possible.

Shunt Reactor Controller

From |

Shunt reactor controller

Shunt reactor

What is a shunt reactor controller? I recall having the same question running through my head when a customer told us about what he was trying to do. Well, before knowing what a shunt reactor controller does, let us look at what exactly is a shunt reactor?

Some of you might wonder “Why does it look like a transformer?”. Yes, you are right, to a certain extent, because a shunt reactor does have similarities with a transformer in terms of its construction. However, they are both very different in terms of their functionality.

While a transformer is used to efficiently transfer power from one voltage system to another to cater for the application required, a shunt reactor absorbs reactive power generated from the source i.e. motors, generators etc.

Active and Reactive Power

What is reactive power and why do we bother to absorb? That might be the next question to ask. Before going into that, we need to understand that in an AC circuit, there are both active power (or real power) as well as reactive power, in which the active power is used to power up a system. To understand this from another perspective, think of it as a pint of beer where the beer is your active power and the reactive power is the foam.

The Beer Analogy of Active and Reactive Power

Reactive Power Analogy with Beer

Image from Electronics Tutorials (http://www.electronics-tutorials.ws)

Let’s put water piping system as an analogy to electric circuit, and voltage is the ‘water pressure’. A certain level of water pressure is required in order for the water to travel across the piping system to the designated location to perform certain task, such as flushing your toilet bowl. Similarly, voltage plays the same role in an electric circuit to ensure that active power can be supplied to run any equipment or device. In this case, reactive power is the key element to maintain the voltage level in a circuitry.

The Water Analogy of Electricity

Water Analagy of Electricity

Image by: Paul Evans (http://theengineeringmindset.com)

Hence, instead of using the word ‘absorbing reactive power’, shunt reactor is rather used to stabilize or compensate the level of reactive power in an electric system.

From Component to Solution

Rewinding back a little on how this shunt reactor controller came about. It started with a normal enquiry sent in, asking for a voltage transducer. We followed up with a visit to the customer to understand further.

He showed us the solution that he was going to implement for his end user who runs a palm oil refinery. This was an existing solution in another plant where it was used to control the output of power that being transferred back to the grid from the bio-gas generation using the effluent of palm oil.

  • During the day, when most of the equipment in the plant is running, the whole electric system is highly loaded and more reactive power is consumed. Thus the causing the voltage to drop.
  • However, whenever there is less equipment running, less reactive power is consumed and hence the voltage increase.
  • This is the time when a shunt reactor has to be switched on to compensate the reactive power in order to maintain the voltage level at a particular rating.
  • Each shunt reactor has a fixed rating. Hence, putting several shunt reactors together and adding controls to it can achieve different reactive power compensation at one time, depending on the system load.
  • This whole solution is the basic working concept behind a variable shunt reactor, however cost is always a concern when it comes to such solution.

His idea was to duplicate the same solution in his project. Looking at the pictures he showed us, we believed that it was possible to be implemented with the range of products that Phoenix Contact has to offer. Hence we came up with the solution concept diagram with a brief program flow.

Customized solution from Phoenix Contact

We finally secured the project after a few rounds of discussion and modification to suit best to his application. The list of products that are put into this solution includes:

  1. ILC 171 controller – The processing unit to control the shunt reactor via relay and contactor.
  2. MCR voltage transducer – The main component to take in voltage from the system and convert it to readable value for the controller.
  3. UNO power supply – Main power source to the controller and other peripherals.
  4. TP 3150 Touch Panel – Serve as a HMI for the user to control the shunt reactor controller and display of current value of the system.
Shunt reactor operation concept

Basic operation concept of shunt reactor controller

Shunt reactor display panel

Shunt reactor controller

Shunt reactor

From a simple transducer enquiry to a shunt reactor controller project, we believe that with the available resources and wide range of product that we have, Phoenix Contact is able to customize the solution that is fit for your application.

Want to know more about how we can help in your next solution to your customer?

Feel free to drop us a feedback or send us an enquiry at marketing@phoenixcontact.com.sg. Who knows, your simple component enquiry for your project could be our next solution to you!

Let there be Light

From |

Let there be light: Phoenix Contact Components for Reliable Power Grids

On 7 July 2017, Phoenix Contact Singapore Team organised a’ Dining in the Dark’ event as part of Corporate Social Responsibility.  In the short 2 hours without our sight, we experienced a range of emotions such as fear and helplessness. This event also allowed us to understand the challenges that persons with visual impairment faced daily. It is truly a meaningful event that we are thankful to be able to experience with the friends we made from work.

Phoenix Contact's 'Dining in the Dark' CSR Event

Phoenix Contact’s ‘Dining in the Dark’ CSR Event

In today’s world, it might not be an exaggeration to say that we will feel the fear and helplessness if we do not have access to electricity. For a start, life-sustaining equipment in hospitals will not be in operation. Many of life’s conveniences such as lights, entertainment, air-conditioning etc. will be stripped from us. For this, electrical grids are always considered critical infrastructure all around the world and efforts are made to ensure the grid is always operating. Phoenix Contact contributes to this reliability with our products. Below are some examples:

    1. Terminal blocks (Clipline Complete)Clipline terminal blocks
      Our terminal blocks are widely used in power industry. For quick installation in Marshalling/Pilot panel, our customers prefer the use of

      • Push-in connectionThis connection method is fast, do not require special tools, safe, ensure consistent and good connection for every insertion and ideal for areas with high vibration. Most importantly, unlike screw connection, over time, push-in connection does not loosen.
      • QTC connectionThere is no need to strip the wire using QTC connection, making it the fastest way for wire installations. Moreover, Phoenix Contact QTC terminal blocks do not require special tools!
    2. Protection terminal blocksURTK-6 Test Disconnect Terminal Block

      Especially for CT testing, where you have to make the testing circuit before breaking the transformer circuit, it is important to ensure that the “make-before-break” is done properly! Failure to do so results not just in power outage, but often death.

      Our solution is our range of test disconnect terminal blocks, clearly labelled to ensure operators know exactly what is being done. There are also ample spaces for accessories for you to do the necessary bridging and testing.

      Offering inspiring innovations, Phoenix Contact has come out with a test disconnect system. Instead of manually doing the switching, why not let our system take care of it for you with Fast And Modular Energy system (FAME).

    1. DC/DC Converter and Power SupplyQUINT DC/DC converter and Power Supplies

      Usually in substations, there will be 110VDC power supply. However, most electronics components (remote IO, network switch, RTU) requires 24VDC/48VDC power input.  For this purpose, many substations around the world choose Phoenix Contact Quint IV Power Supply.

      Your advantages

      • SFB Technology selectively trips standard circuit breakers, loads connected in parallel continue working
      • Preventive function monitoring indicates critical operating states before errors occur
      • signalling thresholds and characteristic curves that can be adjusted via NFC maximize system availability
      • Easy system extension thanks to static boost; starting of difficult loads thanks to dynamic boost
      • High noise immunity, thanks  to integrated gas-filled surge arrester and more than 20 ms mains failure buffer time. Moreover, Phoenix Contact Quint IV Power Supply comes IEC61850-3 certified. This means that the unit can be used even for IEC61850 applications!
    1. Interposing relays
      With a wide range of relays, Phoenix Contact has the right solution for all standard relay applications, such as interposing relays.

      Your advantages

      • Easy handling, thanks to modern wiring and potential distribution concept
      • Easy extension to a timer relay, thanks to plug-in special function module
      • Complete product range covering all standard relay applications
      • Reliable system for high machine and system availability
      • Available as a complete module or modular system
Easy Wire Termination  Easy Power Distribution  Complete Product Range

Test Disconnect Push-in Connection

Our relays with push-in termination technology provide fast and easy tool-free wiring. Simply push the wire into the terminal , using very little force. Remove the wire by pushing done on the release button, using a screwdriver or ballpoint pen.

Test Diconnect Terminal Block Jumper

Reduce your wiring time up to 70 percent by using our modular terminal block plug-in bridges. These time-saving bridges ensure a reliable connection and reduces the possibility of wiring errors.

RIFLINE Complete

Switch currents up to 16 A. From coupling relays to a replacement for small power contactors; the product range offers the right relay for every application. Benefit from a uniform and consistent system

  1. Heavycon (Heavy-Duty Connector)
    Substations have high EMC and electrostatic interferences. They are also generally not places that people like to hang around in! Heavycon can help to reduce installation/maintenance time and at the same time, ensure reliable power/data/signal transmission. With a modular system, you can combine Fibre, Ethernet, Serial, signals, power all in 1 connector!

HEAVYCON Modular Connector

For example,

  1. the Local control cabinet can be connected quickly to the bay cabinet
  2. The Circuit breaker compartment can be easily disconnected/connected to the switchgear

The Revolutionary Test Plug Redux – FAME , FAME 2 and now FAME 3!

From |

Phoenix Contact's FAME 3

It was 2 years ago when I have first blogged about our revolutionary panel testing system – FAME systems that helped many of our customers worldwide in simplifying their protection relay panel testing procedure and at the same time ensuring the safety of the person who is conducting the test.

Do check out my previous blog “FAME 2- Enter, Push, Twist and Remove”, I did explain why Phoenix Contact FAME system is such a revolutionary testing system.  If you are dealing issues with your protection relay testing or any needs of installing a panel testing component, make sure you stay with us in this blog as I will review some updates and features that might be beneficial  to you.  No worries if you have missed out the previous blog, you can still read it here. Continue reading

Living in a Singapore HDB flat

From |

As a Malaysian, I grew up living in landed property houses; we are lucky in the sense where we have more land area for the individual to enjoy. Why do we love landed property so much? Well, you can easily associate the lifestyle of living in landed properties with building your control panel with single of double deck terminal blocks. Let me show you why. Continue reading

Electric Power and Renewable Energy 2016 Myanmar

From |
Exhibition Image

Electric Power and Renewable Energy 2016 Myanmar

We will be participating at the 4th International Electric Power and Renewable Energy 2016 Myanmar Exhibition from the 13th – 15th of October at the Myanmar Event Park (MEP) in Yangon.

Come down and join us to find out more about what we can do for you in the area of Power generation and transmission and solar. We are located at G16, Singapore Pavilion.

Click here to register at the event’s website.

CLIPSAFE – Your one-stop junction box solution

From |

The “Blame Game”

Have you ever been bothered by such a situation?  Picture this, you have just completed your run on a beautiful day only to return home and realize that your feet are full of blisters. Should you put the blame on the shoe manufacture for using a material that is too tough, or would you blame the socks company for using a material that is too soft?

shoes

Things can potentially get uglier when it comes to planning for or executing a project. Have you had the unfortunate experience of opening a ‘Brand X’ junction box, to find yourself having ‘Brand A’ terminal blocks and maybe some ‘Brand C’ cable glands or markings inside. If there is a fault, who you should go to?

You may potentially find yourself being trapped in the “Blame Game” if you are having two or more different suppliers involved.  And if you have ever been trapped in one, you will know that the chances of successfully finding a solution and getting out is very minuscule.

What if there was a supplier who could provide you with a one-stop shopping experience?

CLIPSAFE – Your one-stop junction box solution

Over the years, many of our customers have requested Phoenix Contact to provide one-stop services where they not only purchase standalone components but are able to purchase a solution. We realized it made perfect sense for us to develop a portfolio of “basket or box” which would allow us to further improve our customers’ buying experience. This was the genesis of our CLIPSAFE range of junction boxes.

CLIPSAFE family of boxes

CLIPSAFE Family

 

As we all know, a junction box is just like the body. A healthy body needs a healthy heart – the components to be installed in the junction boxes. With more than 92 years of component manufacturing experience, you are assured we have maintained, and improved, on the quality of our ‘hearts’ over the past 9 decades.

Phoenix Contact’s CLIPSAFE junction boxes offer you the flexibility in choosing various hassle-free solutions.

Ex and NEMA 4X junction boxes equipped according to customer specifications

You can obtain CLIPSAFE enclosures fully equipped with terminal blocks and cable glands on request. Terminal boxes are delivered with the corresponding equipment approval in accordance with ATEX and IECEx for use in potentially explosive areas.

Steel CLIPSAFE box

CLIPSAFE Hi-grade Steel

 

Ex control boxes according to customer specifications

Individual control boxes with electronic components are available on request. With detailed engineering and planning, we will be able to support you in any complicated field-bus or control boxes requirements.

CLIPSAFE Control Box - Steel

CLIPSAFE Control Box – Steel

Empty Enclosure Ex or NEMA 4X

Still unable to make up your mind as to which components need to be installed in your junction boxes? Fret not.

You can always maintain the flexibility to design and assemble your own components as required by selecting our CLIPSAFE empty boxes.

Choose the right junction box housing for your application; from Stainless Steel to GRP material. We have more than 140 Ex-approved and NEMA 4X versions. Custom dimensions and surface treatments for Stainless Steel are available on request. The delivery is carried out with the corresponding components’ approval in accordance with ATEX and IECEx.

CLIPSAFE Empty Box - Steel

CLIPSAFE Empty Box – Steel

Empty Ex or NEMA 4X enclosure machined to customer specifications

Simply means junction boxes with pre-treated holes and cut outs. We adapt the housing to your request to include threads, drilled holes and rectangular cutouts while taking into account Ex-standards in accordance with ATEX and IECEx. The delivery is carried out with the corresponding components’ approval.

Empty box with flange plates and cover

Empty box with flange plates and cover

With all four types of CLIPSAFE offers, Phoenix Contact believes we will be able to address your needs. Not to forget, a good solution always comes with good quality and design. Do check out our CLIPSAFE Quality and Introduction videos below!

https://youtu.be/n9sEkLNADOQ

Long Awaited BT Terminals!

From |

Ladies and Gentlemen, Wait no further!

The long awaited Phoenix Contact BT terminal blocks are finally ready!

Allow me to present to you what we have to offer. Continue reading