Yearly Archives: 2012

Industrial-Grade Operator Panels for Basic Applications

From |

Phoenix Contact rounds out its range of web-based operator panels with 10- and 15-inch versions. This means that more display area is available for visualizing basic applications.

The larger display area has the advantage that fewer process diagrams have to be configured to display all operating data. For operator panels with small displays, information is distributed across various process diagrams.

Continue reading

Fiber Optic Patch Cables with High Flexibility

From |

Phoenix Contact is expanding its glass fiber optics product line to include the M12 circular plug connector. Now it is possible to fit indoor, flex and outdoor cables in variable lengths with all available connectors. In addition to our standard products, we also offer customized solutions tailored to our customers’ individual requirements.

Continue reading

Fast Profibus Extender with Surge Protection

From |

The new Profibus extender from Phoenix Contact enables straightforward integration of remote Profibus devices at data rates of up to 1.5 Mbps. The extender has two DSL connections per device. This means that in addition to point-to-point connections the extender can also be used to easily establish line structures with up to 30 devices.

Continue reading

A Visit to Newater

From |

30th Nov 2011 marks a special and important day for Phoenix Contact (SEA) Pte Ltd. What is so important and special? Hear this, we hosted 4 VIPs from Germany who are, Mr Frank Stuehrenberg, our Executive Board Member, Mr Ulrich Leidecker, our General Manager of Phoenix Contact Deutschland GmbH, Mr Hanno Hardt, Director Media of publish-industry, Mr Thomas Rilke, Director Metropolitan Solutions at Singapore Newater Visitor Center.

Continue reading