Tag Archives: sunclix

Photovoltaic Plug Connector Featuring a Large Conductor Cross-Section

From |

The custom-assembly Sunclix plug connector (available up to 16 mm²) from Phoenix Contact makes it possible to contact conductor cross-sections from 6 mm² to 16 mm².

It was developed to answer the needs of ever-larger PV units in which the distance between module or string and the generator junction boxes or inverters is steadily increasing. Conductors with a large cross-section are required to minimize the transfer loss in the solar cable.

Continue reading

Junction Box for Crystalline or Thin-Film Photovoltaic Modules

From |

The new photovoltaic module junction boxes from Phoenix Contact for crystalline or thin-film photovoltaic modules have been developed to supplement the Sunclix product range at the module interface.

Our developers paid special attention to automation and process safety. Using the junction boxes contributes to the optimization of module production processes.

Continue reading

Keep Cool!

From |

Its January and this is probably the only month in Singapore that we do see much of the Sun. I am starting to miss the warmth from the sunlight.

I don’t think much of us would enjoy the scorching sun in the month of March and April either. However, as much as projects goes, installation of the Solar panels takes place all year round.

Continue reading