Category Archives: Tools

5 Reasons Why Thermofox is a Must-have

From |

Phoenix Contact is proud to have our handy printer where you can label your panels/wires anywhere, any time. And here are 5 good reasons why you should own one today.

  1. Convenience

It is more than just a labeller; it brings you the convenience that you need such that you can carry it everywhere you go. Weighing as light as 650 grams, compact in size, this handy and portable printer gives you all your printing needs with ease. Additionally, it comes with accessories for you to carry it everywhere you go!

  1. Variety of prints

Printing of sticker labels is nothing interesting… It is the most basic material that a printer can print our sticker labels on. We have catered for different textures such as rough or curved surfaces. On top of sticker labels, our handheld printer can print self-laminating wire markers as well as shrink sleeves wire markers! This is really a small printer with a big capacity of printing varieties.

  1. Power efficient

This is the only handheld labeller in the world that you will find “ECO-MODE” inside! Once the printer detects that it is running low on battery, it will automatically enable this eco mode, which allows printing at a slower speed but of equally good quality.

It comes with a rechargeable battery in the full Thermofox set, or can be fitted with 6 normal AA batteries.

  1. Smart keyboard

This printer has a smart keyboard with an alphanumeric number pad. It has easily understandable buttons such as “symbols”, “templates”, “print” and “preview” that can be selected from the printer. The buttons are made such that they are self-intuitive and anyone will know how to use it without prior training needed.

  1. Resistance of the markings after printing

The last thing you would want is that all your labels start fading away and you being left with an unclear label. You can try scratching the prints or pouring some water or oil on it, but trust me, the ink will still be in a good condition!

Our prints are qualified with certain test industry standards to assure the quality of each and every single print. In fact, we have test laboratories!

If you would like to know more about Thermofox, feel free to contact us at marketing@phoenixcontact.com.sg!

Marking Materials for Solar Photovoltaic Application

From |

With the implementation of large scale solar projects in Malaysia, there are more and more inquiries on special marking materials for cable marking, equipment marking, and plant marking that can withstand long hours of sunlight and harsh environments.

If you ever come across such a request from the project consultants or clients, Phoenix Contact marking materials are what you are looking for. We have various product offers that are UV-resistant and weather resistant, ranging from stainless steel to aluminium to high-quality thermoplastic polyether urethane.

Here are two examples of solar cable markers with different types of printing methods.

1) Stainless Steel and Aluminium markers:

Phoenix Contact LS-WMTB product range is available in stainless steel (V4A) or aluminium. It provides simple and fast installation with cable binders. This marker is suitable for the most demanding industrial requirements because it not only fulfils the harsh requirement in the solar industry, but it can also be applied in areas that require high resistance against salt water, chloride, and solvents.

With the use of modern laser technology, it creates highly resistant and permanent markings on these markers.

Examples of stainless steel cable markers

2) Polyether Urethane (PUR) markers:

An example of a polyether urethane cable label

An example of a polyether urethane cable label

Phoenix Contact WMTB HF range of product is suitable for both indoor and outdoor applications. It is made of high-quality thermoplastic polyether urethane, halogen-free and flame-retardant material, with high tensile strength that is able to adapt to the bending of the cable conductors.

WMTB HF comes with an exciting selection of colours, from the commonly-used white, to yellow, red, blue, and green. Unlike the stainless steel marker, WMTB HF is printed using thermal transfer technology.

Other than the marking materials, Phoenix Contact also offers UV-resistant cable ties that work with the markers, as well as high quality printers with laser and thermal transfer technology. Please feel free to contact the Phoenix Contact sales team if you wish to know more about these products.

Three Good Reasons Why You Should TRADE IN Your Printer

From |

Phoenix Contact has a wide variety of printing systems, capable of meeting all sorts of marking requirements, ranging from terminal markings, wire & cable markings, equipment labels and plant markings!

Terminal Marking

Terminal Marking

Wire & Cable Markings

Wire & Cable Markings

Equipment Marking

Equipment Marking

Plant Marking

Plant Marking

Label On-the-go

 

Every label requirement you need for your panels, inventory, workshop or even wiring is possible with our variety of printers in place! Print at your own convenience and save the hassle of pre-ordering them. You can also customize our printers to cater to your own specific printing needs, avoiding wastage due to unused or wrong labels!

 

What’s more is that Phoenix Contact is having a TRADE IN scheme now!

Three Good Reasons Why You Should TRADE IN Your Printer:

  1. Get the most bang for your buckAll your marking needs for rolls and cards

Why not save your company some money if you can let go of your old printer, in exchange for a discount off the new one? The trade in scheme is meant to give customers more incentive to purchase a new printer from us! Speak to your local sales representative to get more information on how much discount you can get off your printer when you trade in yours now!

  1. Upgrade your current technology

High Volume Printing

Have you been using your printer for many years, unaware of how much technology has progressed? Printing speed has increased tremendously over the years, not to mention the quality of prints! So, if you are wondering if it is time to get a better printer for greater efficiency, it is still not too late! The trade in scheme is the perfect platform for you to enquire more about the technology that goes into Phoenix Contact printers.

  1. Save the environment

Instead of chucking your old printer in a corner, taking up space and collecting dust, we welcome all your used printers to Phoenix Contact, and you even get a discount when you purchase one from us!

If you still insist on disposing of your old printer, there are tons of toxins inside printers that hurt the environment! So, start thinking about our trade in scheme and do your part to save the earth!

Click here now if you are interested to get a trade in!

Cut, Strip and Crimp – Tools to Ease Your Cabling Pains

From |

Today, we enjoy the fruit of technology as we turn on our television, air-conditioner, lights or our smart devices. Have we thought about what are the nitty-gritty details that have led to our enjoyment in this day and age?

What is common amongst all this technology is the need for electricity, and more importantly, what carries electricity around are wires.  Wires and cables are the root that carries electricity all round; it allows current to flow from one point to another. What is often missed out is the hard work spent by the electricians who, behind the scenes, manages this labyrinth of wires.

Messy cables

Photo by: Derek (https://www.flickr.com/photos/dcmorton/2446443103)

Cutting, Stripping and Crimping are steps that are very familiar to our electricians. However, they are not just merely steps; but in fact, they are techniques that we need to offer much respect to the electricians who handle them. Providing the right tools for the job makes it even more crucial to ensure they put their techniques into the right place.

Cutting, Stripping and Crimping of wires sound easy and effortless. However, using it on a daily basis requires the tool to be designed more than just a normal tool. Phoenix Contact takes ergonomics, usability into consideration and provides the optimal tools for its end users.

Tools to Cut, Strip & Crimp

Cut – CUTFOX 18

Phoenix Contact Tools - CUTFOX 18
  1. Safety Lock
    Safety is a true concern in a workplace, and every effort to keep the workplace safe is extremely important. Slip guards are attached in our cutter which keeps the blades closed.
  2. Less Fatigue
    Spring-loaded pliers opens up automatically, which means users spend lesser energy. With the pivot near the cutting edge, it provides optimum power transfer.
  3. Cutting Quality
    Cut your wires perfectly with the special curved metal giving your wires a nice and squeeze-free cut.
  4. Reliable Material
    The steel material of the cutter has gone through heat and surface treatment ensuring your tool to be long lasting and corrosion resistant.
  5. Comfort
    Consisting of both soft and hard parts, meant for the best comfort for any hands. The curved designed of the handles and the angled head for the ultimate ergonomics.

Strip – WIREFOX 10

Phoenix Contact Tools - WIREFOX 10
  1. Easy Adjustment
    Depth of the blades can be easily adjusted as required. Length of the stripped length can also be easily adjusted with the small measurement ruler and the stopper in place.
  2. Flexibility
    Interchangeable knife cassette gives you the option for all different wire sizes as required. One casing for all wire sizes!
  3. Stopper
    A wire stopper equipped in the knife cassette helps you to position your wire at the stripping length you need.
  4. Convenient Cutter
    Equipped with a cutter at the side, it gives you the convenience to cut your wires any time.
  5. Comfort
    Consisting of both soft and hard parts, meant for the best comfort for any hands. The curved designed of the handles and the angled head meant for the best stripping experience.

Crimp – CRIMPFOX CENTRUS 6S

Phoenix Contact Tools - CRIMPFOX CENTRUS 6S
  1. Multi Range Die
    Self-adjusting principals of the die covers a large cross section (0,14 – 6mm²), so you can use one tool for most of your needs.
  2. Good and Complete Crimp
    Built in ratchet mechanism is the key for a good crimp as it doesn’t allow the pliers to open until the process is complete. In this way, it ensures a proper and complete crimp.
  3. No need for recalibration
    Due to the special die closing process and its ball bearings, it reduces wearing out. Thus, eliminating the time and effort you need for re-calibration.
  4. Less effort
    Equipped with a rotating crimp mechanism, together with the tool size, ensures an optimum power transmission. In other words, you use less energy!
  5. Comfort
    Consisting of both soft and hard parts, meant for the best comfort for any hands. Its small size of 18cm tall, 6.5cm wide, and weighing at 380g serves as a compact and handy tool. The optimal positioning of the pivots gives the smallest opening handle angle in the market. Not forgetting the soft non-slip pressure pad supports your force transmission, so you can, for example, have it sit against a table surface!

After introducing the key features and ergonomically designs of our Phoenix Contact tools, would you like to experience it first hand on its comfort and ease of usage?

Cut, Strip & Crimp Toolkit Promotion

Get a “Cut, Strip & Crimp” Toolset kit today with our current promotion in Phoenix Contact!  For more information on the promotion, just leave us your contact details at marketing@phoenixcontact.com.sg and we will get back to you soon.