Many times when we are working on projects whether it in is design, development or maintenance stage, we may have doubts, new ideas of technology or problem which we will need to confirm, test or to find a solution.
Category Archives: Industry Cabinet Connectivity
Installation terminals with Screw Connection Technology
From |Phoenix Contact’s new generation of UTI installation terminals is tailored to the requirements of electrical installation and distributor construction.
Compact monitoring relays for quick wiring
From |The new EMD-BL compact monitoring relays from Phoenix Contact monitor current, voltage, and phase sequence efficiently and reliably. In the space-saving installation housing and equipped with the Push-in quick connection technology, the devices allow for quick, tool-free wiring. They are particularly suitable for simple monitoring tasks from series production through to building installations. Continue reading
Rotary switches for use in the field of energy technology
From |Phoenix Contact has moved one step closer to become a complete switch cabinet component provider with the introduction of CAM switch!
The product range of compact rotary switches up to 20 A has been designed for the switch programs which are available for application in energy technology.
Complex Testing Done Safely and Economically
From |Complex testing tasks in switching systems can now be completed quickly and safely using Phoenix Contact’s new FAME testing system. Alongside the testing block built into the cabinet door, this offers a range of operating, testing, and dummy plugs.
Time for a NEW TOOL Part 2
From |The CRIMPHANDY is an innovation that will revolutionize the tool market.
PT Power 95
From |PTPOWER 95 – The new product family closes the product gap of high-current terminal blocks for larger cross-sections in the PT-series. The comfortable direct plugging of lines is now also possible for larger cross-sections of 25 mm² to 95 mm² with no additional tools needed. The eccentric allows a simple handling without risk of injury. The product range of pre-assembled terminal blocks reduce installation time to the customer.
Time for a NEW TOOL
From |Stripping, fitting with a ferrule and crimping are carried out in one work step.
The entire process is completed in approximately two seconds and the next conductor can be inserted for processing.
Watch out for this tool !
The POWER is NOW
From |The PTPOWER 95 family will be the first high-current terminal block with Push-In technology for direct plugging in the market.
The comfortable direct plugging of cable is now possible for larger cross-sections of 25 mm² to 95 mm².
The eccentric allows a simple handling without risk of injury.
Stay on and come back for more information.
Now the time to reveal the power! Click on the link below for more information:
Flexibility for Wiring Emergency Lighting
From |With a width of 5.2 mm, Phoenix Contact’s compact PTB 2,5 three-level terminal blocks provide high flexibility when wiring emergency lighting.
In commercial buildings, standard lighting is often also used as emergency lighting, which provides flexibility, for example, when modifying building utilization.