Yearly Archives: 2015

Heavy-duty connectors for every application

From |

Heavycon complete heavy-duty connectors from Phoenix Contact offer a reliable seal up to degree of protection IP69K. There are matching plug-in connections for every requirement with housings from three series types and matching contact inserts which can be combined.

4727

The standard series offers a wide range of robust metal housings with various different cable outlet directions and locking mechanisms. The flexible, swiveling bayonet locking of the EVO series allows the cable outlet direction to be freely selected and reduces the number of versions and thereby the warehousing costs by up to 70%. Not only does the direct screw locking without panel mounting base result in cost savings, it also means that the Advance housings are particularly durable and robust.

All components can be individually combined and flexibly modified, extended or exchanged. The standard and EVO housing is pin-compatible with the market standard and the Heavycon metal housing is “EMC-ready” thanks to conductive surfaces and seals. Combined with shielded cable glands, they offer you reliable protection in electromagnetic surroundings. All housing series fit standard panel cutouts.

Embrace – Mistake

From |

Admit it… who has never made any mistake in his/her life.

Successful person holds the attitude of embracing mistake, they know that mistakes are part and parcel of life. Therefore, if you want to lead a successful career, firstly you need to accept your embrace your own mistake. Do not finger point, saying it was result of others or certain event that happen, you may end up just searching for an excuse to cover your mistake and you may not achieve the result you want.

One good example I had read online was Thomas Edison and his invention of Light Bulb.

He did approx 10,000 times of attempts before he successfully invented light bulb, he did not give up or find excuses not to continue. What he did was to embrace the mistake he made, and moved on… through his perspective, I quote “I have not Failed, I ‘ve just found 10,000 ways that won’t work” he also comment that “Many of life’s Failure are people who did not realize how close they were to success when they gave up”

In our daily life, there are something within ourselves that we can control and by making a little changes to our attitude towards mistake, we may receive something unexpected. Therefore, I would like to share the following points towards how one should feel about mistake:

  • Change our attitudes to mistakes so that mistakes become something we no longer ashamed of
  • Dare to admit on your mistakes and learn from it
  • Without mistakes there would not be progress and no success
  • It’s ok to fall… but remember to pick yourself up positively

Everyone knows that it is sometime hard to admit your own mistake, and the easy way out is to point outwards. But when you are brave enough to stand up for the mistake you done, you also build your trust and honesty within your friends and team.

If mistake was created by your colleague, friend, or even family member. You must be sensitive about it, no one like to make mistake… they might already be feeling bad and by continuously blaming them would not change any outcome. Why don’t you consider talking to them and tell them about the ways they could have done for the benefit of future should the same situation rise again. In short, my recommendation would be:

  • Eliminate fears of admitting mistakes –
    • Be approachable
    • They know they are wrong, make discussion not whining
    • Embrace them
  • Support them, take risk together and learn together –
    • Discuss and agree on decision
    • One for all, all for one
  • Encourage to make mistakes, and make sure they learn from it –
    • Respect them for their position and critical thinking
    • Allow space for decision and let them be successful

There are many other ways to approach a similar situation…

I hope this article give you a slight change of perspective towards mistake, to embrace or blame, you make your own decision. Remember, before pointing out the flaws in others… look into yourself. 🙂 Spare a thought for others.

 

Valueline Industrial PC – The Red Dot Design Award Winner 2015

From |

PC Red dot design

The next-generation Valueline Industrial PC from Phoenix Contact is a combination of functional design and high-performance technology. This impressed the Red Dot jury which awarded the Industrial PC (VL2) as the winner for the Red Dot Design Award 2015.

Industrial PCs with touch display, commonly known as Panel PCs, are increasingly becoming the main interface between humans and machines. This Human Machine Interface HMI) combines all the operating and monitoring requirements allowing the operator to effectively manage the production processes.

At the same time, a high-performance computer could be required for all the control, data storage and reporting tasks in the system. Thus, a combination of modern computer technology and user-friendly design is all the more important.

With its clean and sleek design, the IP65-compliant front with multi-touch capabilities acts as the interface for every system.

As a manufacturer of innovative automation technology, Phoenix Contact develops robust panel PCs tailored to the requirements of industrial production processes. Equipped with modern Intel® Core™ i processors, combined with flexible RAM and storage extension that can be adapted to the requirements; the latest generation of Valueline panel PCs is able to smoothly display ever complex system processes in detail.

The rear panel of the housing was optimized for quick maintenance access as shown below; allowing easy access to all essential components.

Equip

The spring loaded retractable latch shown below temporarily holds the IPC in place, allowing it to be easily installed by 1 person. This increases manpower efficiency as it is no longer required for 2 people to do the installation – one person to hold the IPC in place, while the other screws the mounting brackets.

Back of the pc

Do contact us via email at info@phoenixcontact.com.sg if you would like to find out more about the innovative and reliable next-generation Valueline IPC from Phoenix Contact!

 

 

Phoenix Contact expects revenues of eight percent for 2015, a sign of excellent growth

From |

Bent_Stührenberg_PK2015

Chief Executive Officer Frank Stührenberg expressed his “delight at the results for 2014” during a press conference on Phoenix Contact’s economic growth for the past year. The corporate group’s revenues grew by 8.5 percent to €1.775 billion. “We have tripled our revenues within 15 years,” says Stührenberg, highlighting the successful results. The industrial electronics manufacturer invested €125 million in the expansion of the corporate group. An 11,000-m² innovation and production center was opened in the U.S., where 250 employees work in research and development, marketing, and production. The global workforce increased by approximately 1,100 new employees.

Phoenix Contact is expecting revenue growth of eight percent for the current year. Stührenberg is optimistic in his outlook. “We are seeing a growth in the markets where Phoenix Contact already has a strong presence and our products have already been in use for a long time.” These include the market segments of infrastructure, energy distribution, and renewable energy. The company wants to invest approximately €150 million in national and international expansion activities. A new building in Bad Pyrmont, Germany, will provide an office and lab space of 18,000 m² for the corporate group’s ability to provide expert solutions. Completion is slated for the end of 2016. Phoenix Contact E-Mobility GmbH will establish a subsidiary in China, the world’s largest electromobility market, in the third quarter of 2015. An investment of €20 million will increase production volumes at the site in Nowy Tomy?l, Poland. On 1 September, 100 trainees will embark on a new career, and almost half of them will start in July already as part of their dual education study program.

Touted as the economic barometer of consumer confidence, the Hanover Trade Show begins on 13 April. India is the partner country this year. The electronics specialist will present its innovations and forward-looking technologies at the 2,300-m² exhibition space. One of the main topics will be Industry 4.0, a guiding principle that demonstrates how digitalization is changing not only society but industrial processes, as well. Visitors can experience the continuous data flow live in Hall 8. Here the companies Eplan, Rittal, and Phoenix Contact will be demonstrating a continuous, automated process, from the digitization of an item to its engineering and production. “The Hanover Trade Show has traditionally been a key international trade show for us,” explains Stührenberg. “This year, we will be exhibiting more than 100 innovations and are expecting delegations from more than 50 countries with over 1,000 visitors.”

New Phoenix Contact catalogue app can be downloaded in App Store

From |

Our new version of our Phoenix Contact catalogue app can be downloaded in App Store. Initially, the new version is offered in English and German for iOS devices. A version for Android devices and additional languages are being prepared for the course of 2015.

Find information quickly with the new catalog app

With the new catalog app, you can access our complete product range by navigating through the familiar Phoenix Contact product structure. Intuitive navigation and different check lists will make it a lot easier for you to place your order. Always find the right contact person, and the information fitting your needs.

New functions:

Our product portfolio at a glance:

You can easily navigate through our product range with the new catalog app. Exportable checklists make it easier for you to place your order.

Your advantages

• Navigating, browsing, searching: there are many ways to find the product you need

• Find information quickly in the familiar Phoenix Contact product structure

• Knowing what‘s new: we‘ll keep you informed about new products

• Fast, easy, and modern: accessing information via QR codes

• Up to date: receive the latest information from the Phoenix Contact world

• Exportable check lists: save time when placing your order

Download it now!

PxC App phoneQR Code for App

Connect motors quickly and easily

From |

For easy motor connection, space-saving four-level terminal blocks are now available from Phoenix Contact with push-in connection technology for nominal cross sections up to 4 mm², 32A, and 600 V UL. Easy potential distribution via a function shaft on every level reduces wiring costs. A large-surface marking option clearly identifies every motor connection. Each terminal point can be marked and is equipped with an easily accessible test opening.

freistellen mit Pfad CD-Inlay einbauen Network Interfaces fg

Thanks to 50 percent less insertion force, it is possible to insert solid and stranded conductors with ferrules and cross sections from 0.25 to 6 mm² without tools. The built-in actuation lever allows fully insulated releasing with any tool. The orange-colored button indicates the actuating element and prevents the terminal from being activated accidentally. Connection of stranded conductors from 0.2 mm² without ferrules is possible.

The motor terminals were developed within the CLIPLINE complete terminal block range for use of cross-system accessories. In addition to the same bridge system, the entire accessory range for marking and testing is identical to the push-in, screw, spring-cage, and IDC fast connection technology.

New EH Housing from Phoenix Contact

From |

Introducing the latest addition to housing family, EH housing – the universal housing system with modular concept which is tailored for your electronic application needs.

EH housing offers you simple design-in, thanks to its variable housing form factor – high and flat design!

Pic 1                        Pic 2

Let us look into details of this marvelous housing family. For a functional device concept, PCBs can be installed in all three space direction. Free choices of PCB connection technologies are available from Phoenix Contact. We have them all incorporated seamlessly into our latest EH housing. From conventional terminal blocks, plug and headers, to RJ 45, or even USB ports, to cover your wide range of today’s electronic application!

Pic 3

Pic 4

Do you want to house your PCB?

Do you want to save more to maximize your profit for your product?

Do you want your PCB to be covered within Phoenix Contact superb quality and reliable housing?

Talk to us now! We are always available for you!

 

Happy Easter Day!

From |

Easter2015-D4-v2

Do you know…

Easter is understood to include Good Friday and Easter Sunday, which are three days apart. However Easter truly refers to Easter Sunday – the day on which the resurrection of Jesus is remembered and celebrated.

Easter is the most ancient of Christian festivals, it is older than Christmas, and is considered the most important date in the Christian calendar.

Happy Easter Day! Cheers

Pluggable terminals for fast starts

From |

Phoenix Contact’s Combi product range now includes PT 2.5-HEXA multi-conductor terminals with up to six contact points. For example, these can be configured as three push-in contacts for internal wiring and three PIN contacts for pluggable external wiring. This flexible concept facilitates fast starting up of modular system sections, as well as fast replacement of system components during servicing.

The high count of contact points makes the terminals particularly suitable as compact, pluggable marshalling distributors. Large, identically contoured labeling surfaces with end mounting facilitate easy-to-read matrix labeling. The components are very safe, thanks to the touch-proof design of both the terminal and the plug connectors. A double pluggable bridge shaft additionally facilitates simple voltage distribution and marshaling.

freistellen mit PfadCD-Inlay einbauenNetwork Interfaces fg

Thanks to the universal Combi plug zone, a range of different types of plug connectors can be used. Individual coding increases the wiring safety and reliability as it helps to avoid erroneous plugging. An extensive range of optional snap-on accessories, such as connector catch mechanisms, strain relief elements, and shield connections ensure the wiring process is fully versatile.