The RAD-WHA-1/2NPT Wireless HART adapter from Phoenix Contact simplifies and speeds up the retrofitting and expansion of systems with 4–20 mA signal cables. The adapter is connected to an existing HART device in the field to transfer HART data wirelessly into a new system, while the original system based on just 4–20 mA remains intact.
Yearly Archives: 2011
New String Current Monitoring Increases Efficiency of Photovoltaic Installations
From |The new Solarcheck monitoring system from Phoenix Contact is a new reliable instrument for monitoring string currents in large-scale photovoltaic installations. The easy-to-integrate system detects losses in power caused by dirty or damaged panels. This enables targeted remedial measures to be taken so as to increase system availability and thus revenues.
M12 Hybrid Plug Connectors in a Compact Design
From |The M12 hybrid connector from Phoenix Contact is the first hybrid connector in the market with a compact design fit to address industrial applications.
Connection Concepts for Pre-Assembled Encoders
From |Phoenix Contact presents a complete product line that offers new connection concepts to address the requirements of the new encoder generation. The two-part modular system comprises the M12 connection block and a rectangular flange. The dimensions of the rectangular flange are harmonized with the existing rotary encoder housings, so that encoder manufacturers do not have to redesign their devices.
Preventive Maintenance with Lightning Current Monitoring
From |The Lightning Monitoring System LM-S from Phoenix Contact provides information online about lightning strikes in plants and systems. As a consequence, service call planning can be optimized. This new system identifies and analyzes all of the important parameters of lightning surge currents based on the Faraday effect.
Lightning Arresters for LTE and WiMax Antennas
From |The demand for mobile Internet services is forever on the rise. Thanks to WLAN, it is possible to surf in the global network in nearly all buildings and major metropolitan areas. However, network coverage can be spotty outdoors, in public spaces, and especially in rural areas.
The Right Tool for Any Job
From |Phoenix Contact’s extensive range of professional tools has now been expanded to include a series of cutters for electronics and electromechanics. The new Microfox tools are especially suited for working with small electronic parts and components.
Thermomark – Coming this Fall.
From |Sentosa Development Corp for Sentosa Golf Course
From |Sentosa is a popular island resort in Singapore , visited by some five million people a year. The attractions include a two-kilometre long sheltered beach, Fort Siloso , 2 golf courses, 2 five star hotel , a World class Casino in Resort World Casino and featuring the theme park from Universal Studio.
What does this have to do with Phoenix Contact?
Read more after the jump.
Installation Terminals with Push-In Connection Technology
From |Phoenix Contact’s new generation of installation terminals is tailored to the requirements of electrical installation and distributor construction. The terminals are available in various designs as three-level and N disconnect terminals with the matching feed-through, disconnect, and ground terminals. Conductors with cross sections ranging from 2.5 to 10 mm² can be connected. These compact space-savers with widths starting at 5.2 mm offer many advantages in terms of handling, especially in installation technology.