Tag Archives: wireless

Wireless Technology: the Industry 4.0 Backbone

From |

Industry 4.0 is the 4th generation industrial revolution. This world-changing principle enhances productive efficiency in smarter and faster ways by utilizing the state of the art technology of data analysis software alongside powerful computerized hardware capabilities.

The key to the success of Industry 4.0 is to connect thousands of devices to the central system in order to allow exchanging of various parameters to the processing unit, such as humidity, temperature, status, level, etc. Not only is data transmitted, but devices also receive commands for further actions.

Actually, the powerful hardware and advanced software capabilities have existed for over 20 years. However, the increased number of devices connected to the system means a higher cost of investment. In the past, the only reliable connectivity was through wired cables, which investment cost was directly related to the complexity of the number of devices.

This key obstacle has been rapidly resolved by the advent of reliable wireless technology. Today, various applications of wireless technology have been proven and widely used, such as:

NFC: Near Field Communication

RFID: Radio-Frequency Identification

Wi-Fi: Wireless Fidelity

What makes people trust wireless technology?

Security: New advancements in data encryption technology protects data from intruders.

Speed: The new standard of network 802.11ac helps increase data transmission speed to 10 times faster than the old standard which is sufficient for industrial control systems.

Savings: All stakeholders follow the wireless markets trend. Therefore, new hardware for wireless technology has been introduced daily. This brings significant reduction in the price of wireless devices which mean tremendous savings during investments.

Phoenix Contact offers a huge portfolio of products under the category of wireless technology, as shown below.

Why Wireless?

From |

In the conventional method of data communication we often use wired systems. In the setting up of such systems involving data communication, we would need to plan the cable routes very carefully, and it is often very costly when the wires are required to be routed up and down such that obstacles are avoided in order to get connected. Usually the cost of the cables, labour, special tools for terminating etc. would be a considerably huge amount.

Besides the significant installation cost, physical degrading of the cable is a common issue faced (for example, wear and tear due to weather conditions, accidental cuts, scratches and bites by animals such as mice and ants). Especially when the system is down as a result of this, nobody would know which part of cable is broken or damaged.

In wireless technology, we could eliminate such worries and the less hardware used means that the risk of a breakdown would be lower. Aside from this, wireless technology has the following advantages:

  • More flexibility
  • Interference-free communication
  • Mobility and freedom of movement of participants/devices.
  • No wear and tear of the transmission medium
  • Able to bridge long distances and problematic areas
  • Neat looking

Applications of Wireless Techonology:

Some of our Industrial Wireless products are shown below:

An example of a typical setup:

Radioline Wireless Network

Wireless HART Network

Bluetooth Wireless Ethernet

Radioline Signal Strength

From |

FAQ About Radioline

Question: Which wireless technology is used in the Radioline devices?

Answer: A proprietary wireless protocol is used in the Radioline wireless system. The wireless technology is called Trusted Wireless and is specifically designed for the reliable transmission of data and signals over long distances. The new Version 2.0 offers adjustable data rates, encryption, extended diagnostics, and parallel operation of multiple networks.

 

Question: Is Trusted Wireless really suitable for industrial use?

Answer: The frequency hopping spread spectrum enables reliable data transmission even in industrial environments and in the event of interference.

 

Question: What range can be achieved with the Radioline wireless system?

Answer: Depending on the set data rate and the antenna used, the following ranges can be achieved with a line of sight:

  • 4 GHz: up to 5 km
  • 868 MHz: up to 20 km
  • 900 MHz: up to 32 km

The above specifications is according to the product design, but sharing with you the test made in point to point configuration, having trees and structure as obstructions between two points.

At no line of sight, Radioline still transmits and receives analog and digital signals. Thus, Radioline works!

App for finding the right marking solution

From |

The Marking system app from Phoenix Contact provides a mobile and structured search assistant for finding the right marking material for the relevant application.

Even customers who are unfamiliar with the marking range can therefore find suitable marking solutions for their application.

Continue reading →

Easy Wireless Networking

From |

Lose the wire but not the signal!

If data is to be transmitted to a moving, rotating or mobile device, Industrial Wireless solutions are the answer. They are also recommended for temporary installations. What already has been practiced in the home and office areas for years can now also be successfully used in the industrial area.

Continue reading →

Phoenix Contact Wireless showcased in Globaltronics 2010

From |

For the first time, Phoenix Contact has the opportunity to showcase the Bluetooth Wireless Communication with YOKOGAWA’s Data recorder.

When I received a call from Mr. Ng, I was glad to hear from him that he would like to showcase our Phoenix Bluetooth AP together with his data recorder. Immediately, I went to Emmy to get her latest Bluetooth APs and we managed to prepare two units for him to showcase at Globaltronics this week.

Continue reading →