Tag Archives: profinet

Certified Profinet Engineer Course to be held in Phoenix Contact (SEA)

From |

The Certified PROFINET Engineer course is a world wide recognized training program. It’s standardized by PROFIBUS/PROFINET International to create a quality platform for PROFINET qualified persons who are acknowledged by an official exam.

Now for the first time in South East Asia, you can participate in this training course right here in our premises at Phoenix Contact!

Continue reading

Ethernet Switch for Harsh Environments

From |

Phoenix Contact is now offering a five-port Ethernet switch with IP67 protection for use in harsh industrial environments. This switch sets itself apart as a result of the compact design and its ease of installation that makes it ideal for the machine construction sector. Its housing is only 30 mm wide so that it can be installed on a standard structural element completely and without any protrusion.

Continue reading