Tag Archives: ip 65

Revolutionizing the Field Industrial PC – The Designline IPC

From |

Whenever an industrial PC has to be installed in the field along a manufacturing line for operator interaction, it has to be panel mounted onto an enclosure for ingress protection against dust and/or water.

This is because the typical industrial PC is designed with IP65 only on the front face where the screen is and IP20 at the rear resulting in the need of an enclosure to protect the rear.

Continue reading

Routing Pre-Assembled Cables through the Housing Wall

From |

The new CES cable entry system from Phoenix Contact allows pre-assembled cables to be routed into control cabinets in a safe and space-saving manner.

The cut-outs and mounting dimensions of the CES system match the standard dimensions of heavy-duty plug connectors, which are installed in the control cabinet in a standard manner.

Continue reading