We are all familiar with the computer at home but is your home computer drastically different from the computer used in the industrial world ? Continue reading
Tag Archives: industrial pc
Revolutionizing the Field Industrial PC – The Designline IPC
From |Whenever an industrial PC has to be installed in the field along a manufacturing line for operator interaction, it has to be panel mounted onto an enclosure for ingress protection against dust and/or water.
This is because the typical industrial PC is designed with IP65 only on the front face where the screen is and IP20 at the rear resulting in the need of an enclosure to protect the rear.
Configurable IPC Concept for Customized Solutions
From |Phoenix Contact introduces a new industrial PC to meet rising demands in the areas of process visualization, robotics, and industrial automation: The Valueline P7000 industrial PC is a powerful, configurable solution that is maintenance-friendly and favorably priced.
Compact, Energy-Saving Embedded Box PC for the DIN Rail
From |Phoenix Contact is launching the new VL BPC 1000 industrial PC product line of embedded box PCs for especially harsh industrial environments.
These devices are suited for simple control and communication tasks and for data collection in mechanical engineering, systems engineering, building automation, traffic engineering, and energy data transmission applications.
The IPCs are designed to meet high temperature, vibration, shock, and EMC requirements and thus ensure maintenance-free 24/7 operation.
Industrial PC Becomes a Control System
From |Now, a standard industrial PC can handle any control task. The PC Worx RT Basic software PLC from Phoenix Contact transforms any industrial PC into a fully fledged control system. Programming, visualization, and control can therefore be combined in just one device.
Compact Embedded Box PC for an Extended Temperature Range
From |Phoenix Contact now offers a new product line of embedded box
PCs for harsh industrial environments.