The CRIMPHANDY is an innovation that will revolutionize the tool market.
Tag Archives: hanover fair 2013
PT Power 95
From |PTPOWER 95 – The new product family closes the product gap of high-current terminal blocks for larger cross-sections in the PT-series. The comfortable direct plugging of lines is now also possible for larger cross-sections of 25 mm² to 95 mm² with no additional tools needed. The eccentric allows a simple handling without risk of injury. The product range of pre-assembled terminal blocks reduce installation time to the customer.
Monitoring Relays Part 2
From |The EMD monitoring relays can be used to detect deviations in important system parameters at an early stage. These can be indicated or system parts can be shut down selectively.
RIFLINE complete Part 2
From |The complete relay system, with a consistent plug-in design, ensures high machine and system availability.
PCB Terminal Blocks with Push-In Connection for LED Applications
From |Benefit from the advantages of the just 5mm high PTSM series plug-in connectors, which are optimized for LED applications. This means that more components and functions fit into the PCB’s compact space and time is saved when connecting thanks to the push-in connection.
Small Plug-in Connectors For Flexibible LED PCBs
From |The new plug-in connectors from the PTF series enable you to quickly and easily connect LED PCBs with the smallest external dimensions for 8mm LED Strips.
My experience with Phoenix Contact at the Hanover Fair 2013
From |I was invited by Phoenix Contact South East Asia to visit the Hanover Fair and also a tour of their Factory in Blomberg. This was my maiden trip to Germany so I was very excited about it!
Phoenix Contact at the Hanover Fair 2013 – Part 2
From |Yesterday we published part 1 of the special Hanover Fair coverage of Phoenix Contact where we gave an overview of the Hanover Fair 2013 and the significance of it to Phoenix Contact.
In our final part of the coverage today, we will go a little deeper into the booth layout and some of the special sights Phoenix Contact has to offer.
Phoenix Contact at the Hanover Fair Part 1
From |Today was the first day for the Phoenix Contact delegation from South East Asia at the Hanover Fair 2013. Read on to find out more about the Hanover Fair and the significance of it for Phoenix Contact.
Time for a NEW TOOL
From |Stripping, fitting with a ferrule and crimping are carried out in one work step.
The entire process is completed in approximately two seconds and the next conductor can be inserted for processing.
Watch out for this tool !