Tag Archives: device connectors

Miniature Connectors

From |

Small yet high-powered connectors

Application specific and miniaturized connectors have come on rapidly. Fueling this rapid change is a combination of advances in technology. The control cabinets are getting smaller. This in turn reduces the available space for the devices and their boards. In addition, the functional density of devices is steadily increasing. Thus, PCB connectors must also be based on the new size specifications.

What we can offer

Phoenix Contact has launched two new 2.54 mm printed circuit board connectors: the FMC 0.5 and DFMC 0.5 connectors. It is designed to meet the miniature & quick connection requirement, boasting a compact plastic housing and push-in spring connection. The direct connection is possible for solid and flexible conductors with or without wire end ferrules. The wiring can be easily released without the aid of a screwdriver and the connectors can hold conductors with cross sections from 0.14 to 0.5 mm².

Figure 1. Low height profile – the FMC 0.5 connector family offers a push-in spring connection with spring opener.

This connector makes it ideal for designers who face the challenge of keeping up with the trend towards miniaturization.

The FMC 0.5 connector is a single-row connector with a height of only 5.4 mm whereas the DFMC 0.5 connector is a double-row connector with a low height of only 10.5 mm. Plugs in the same grid with push-in spring connection and spring openers that were previously available on the market were twice as high. Both connectors follow the trend of miniaturization – and the associated trend towards a high contact density in a small space.

https://www.youtube.com/watch?v=K0C_x4vATnI

It is designed for automated soldering processes (SMD and THR soldering processes). The two product families’ pin headers are made of LCP (liquid crystal polymer) plastic to withstand the high temperatures in the convection oven.

The applications for the two new connectors are extremely versatile. Possible target groups include measurement and control technology, automation technology and energy technology. Conceivable applications include controllers and inverters. The focus of the application areas is on industrial applications where signals are transmitted to the PCB.

Conclusion – the answer to new market requirements

The new FMC 0.5 and DFMC 0.5 plug connectors and the associated pin headers from Phoenix Contact meet the market requirements in the field of printed circuit board connection technology. Device manufacturers now get powerful connectors that require little space on the circuit board and in the device. For the end customer, the connectors also provide a quick, easy and convenient connection option. Processing in highly automated SMD processes is not a problem, and a gold-plated contact system provides additional security for the transmission of signals in industrial environments.

If you would like a sample board, or would like to know more, don’t hesitate to contact us at marketing@phoenixcontact.com.sg!

Reduce the Cost of Manufacturing A Printed Circuit Board Assembly (PCBA) with THR technology

From |
Pick and place machine

‘Pick and Place’ Machine with THR components.

Do not judge a connector’s cost-effectiveness just by its price. Its ability to improve the overall efficiency of the manufacturing process counts as well. This is where THR technology shines.

The most common method of manufacturing  a PCBA (Printed circuit board assembly) typically requires 2 process flows. Reflow soldering is used to mount the Integrated chip (IC) and passive components in the first process flow. This is then followed by a second flow utilizing wave soldering to mount the terminal blocks and connectors.

The process can be optimized but that usually comes at a cost, e.g. installing a new machine. Hence, that eventually translates into a higher manufacturing cost in the short term. Is there a way to achieve higher efficiency in PCBA manufacturing without the accompanying costs?

Higher efficiency at Lower Or No Cost?

Yes. It can be done.

This is achieved by introducing connectors that are suited for the existing process line yet reduce the process flows to just one.

This is made possible by the integration of Through Hole Reflow (THR) components in Surface-mount technology (SMT) installations, which dominate today’s assembly manufacturing process.

Through Hole Reflow (THR) – Assembly In Just One Process

The benefit of THR is to use the existing Surface-mount device (SMD) machines and remove the 2nd process, the wave soldering, thus reducing the manufacturing a complete PCBA into a single process.

While it is the ideal situation to switch to an all-THR component solution, some components will still require wave soldering. Even so, there can still be a significant cost savings to make the switch.

Through Hole reflow Connector (THR)

Through Hole Reflow Connector (THR)

While there will not be a need to make changes to the existing equipment, some modifications will be required. For example it may require a change in the PCB design, an adjustment in the reflow profile, etc.

These changes, however, will reduce the amount of man-hours required for wave soldering. Based on a typical PCBA consisting of 80% of ICs and 20% of terminal blocks & connectors, the switch could achieve up to 20% of cost savings as THR components fully supports ‘pick and place’ machines.

https://www.youtube.com/watch?v=XY8jEz2AiWo

If you would like to know more about Phoenix Contact’s THR connectors, get in touch with us at marketing@phoenixcontact.com.sg.

Dear Junction Box, I Met Someone New…

From |

Dear Junction Box

I have been with you since the first day I started my lighting business. You have been a great provider of industrial power distribution and many of my friends knew you, there were simply no one else that could do the job that you could.

I was drawn to you because of your petite size and your attractive figure. Although we have problems but we could not part ways. You were important to my electrical installation.

However, I met someone new from Phoenix Contact and her name is ‘QPD’.

Continue reading →

The New UM-ALU Housing

From |

Phoenix Contact offers rugged aluminium housing HC-ALU for control cabinet and field robust electronics housing.

The new UM-ALU housing provides effective protection for your electronics against thermal and electromagnetic influences. It also features a trapezoidal cross section and is suitable for use with handheld devices for mobile data capture or wireless communication.

Continue reading →