Tag Archives: contactron

Contactron – Protection for Your Motor

From |

Everyone has tangible or intangible possessions that are close to our heart.

We will purchase insurance for our loved ones or get a mobile phone cover to protect our latest mobile equipment against impact. When the world was hit by COVID, we protect ourselves with masks and so on.

How do we protect our three-phase asynchronous motor from overloading and on and off switching procedures? Failure to protect these motors would result in downtime, production delays etc.

Phoenix Contact offers various CONTACTRON hybrid motor starters that combine up to four functions in one device:

CONTRACTRON also eliminates the usual way of wiring by integrating all the important functions into your safety chain.

We have various specifications to suit your motors’ needs.

Get in touch with us and we will provide the best protection for your motor needs.

CONTACTRON Hybrid Technology

From |

What happens when relays and transistors are used as one function?

Electric motors are used in a variety of industrial applications for controlling movements. The motors are often started using classic, mechanical contactor circuits. Besides the advantage of the low price, the conventional contactor technology also has major disadvantages such as high space requirements, limited service life and the need for considerable wiring.

The innovative CONTACTRON hybrid technology combines semiconductor and relay technology and thus offers a cost effective and technically superior alternative to the conventional contactor technology. The CONTACTRON solid-state reversing contactor “4 in 1” is the first CONTACTRON product that already works with the hybrid technology. It offers motor protection and a safety function, as well as a complete reversing contactor circuit for a motor – all this integrated in a single device no wider than your thumb.

The wide range includes devices which implement either a simple motor start function (“1 in 1”) or two functions (“2 in 1”, e.g. motor start + safety) or three functions (“3 in 1”, e.g. forward running + reverse running + motor protection).

From the CONTACTRON range, the customer can choose the device that offers the functions required for the respective motor (forward running / reverse running / emergency stop / motor protection).

More importantly, the Contactron has 10 times the service life of the normal contactors.

You will be surprised how much cost savings you will have when you start replacing those faulty contactors within the lifespan of our Contactron.

https://www.youtube.com/watch?v=Ap0iBA-BiqQ

Hybrid Contactors = CONTACTRON from Phoenix Contact.

If you want to know more about this product, please feel free to send us an enquiry at marketing@phoenixcontact.com.sg and a product presentation can be arranged to discuss in more detail.

Hybrid Motor Starters – CONTACTRON

From |

Phoenix Contact’s Contactron is a range of hybrid motor starters that is engineered and design to replace the traditional way of starting, stopping and managing the motor. And with that, it comes with numerous advantages and benefits to the system integrator, contractor and end user.

https://www.youtube.com/watch?v=Ap0iBA-BiqQ&t=63s

The most obvious advantage is the space savings it brings if one chooses to use Contactron instead of the using the usual contactors and thermal overload relay. The space savings can range from 50% to 89% depending on the motor configuration.

With space savings, one can design their panel or cabinet to be smaller. This is useful for sites where space is limited such as on top of a shipping port cranes. An even more remarkable savings can be achieved by using the Contactron to shrink the size of an Ex d explosion proof box by replacing the contactors and thermal overload relay.

Contactron comparison with traditional motor starter

Contactron setup compared to traditional motor starter setup

Secondly, the Contactron can very much reduce the downtime of a plant or factory as it can perform on average 10 times the typical service life of the traditional contactors. This is because, rather than depending on the ‘prone to failure’ nature of mechanical parts of the contactors, the Contactron uses a combination of solid state and electromechanical relay. Therefore, for motors that are subjected to frequent start stops, the Contactron is an obvious winner.

Besides that, the Contactron can be connected and communicated to a higher level control and monitoring system. This allows crucial information on statuses of the Contactron to be sent to the control system using common protocols such as Modbus, Profibus and Internet IP. This is crucial for visibility and productivity of the plant or factory operators. The traditional contactors with no intelligence have no possibility of being connected to a control system.

Besides, the above, there are many more advantages of using Phoenix Contact’s Contactron over traditional motor starters.

You can click here find out more about our Contactron Hybird motor starters

However, it will be best to be able to feel and learn about this with a face-to-face direct demonstration and presentation. If there is any interest, please feel free to leave us your contact at marketing@phoenixcontact.com.sg and we will arrange a visit to your office.

Motors Intelligently Switched and Simply Wired

From |

With hybrid motor starters from Phoenix Contact, users switch and reverse motors quickly and reliably.Contactron switching technology enables smooth switching and relieves the load on relay contacts.

Hybrid motor starters therefore last up to ten times longer than purely mechanical switching devices.

Continue reading