Tag Archives: cable entry system

5 Ways to Terminate Cables into an Electrical Panel

From |

There are several criteria when it comes to choosing the right cable entry method into an electrical panel, such as ingress protection (IP) rating, ease of connection/ disconnection, cost of the connector etc. In this post, we have sorted out 6 different cable entry methods that Phoenix Contact has to offer.

  1. Cable Gland

The most common way to terminate cables into an electrical panel would be to use a cable gland. It is easy to use and comes in many variants such as different sizes, materials and with additional certifications such as ATEX. Cable glands are probably one of the most affordable cable entry methods mentioned in this article.

However, cable glands have its limitations too. It is difficult and time consuming to do multiple connections/disconnections with cable glands as the cables are terminated directly into the components within the electrical panel. In addition, the pre-cut holes on the gland plate are irreversible. It provides limited flexibility for mistakes and modifications.

  1. Heavy-duty Connector

As the name suggests, it is rugged and enables fast and easy connection/disconnection to the electrical panel. Cables are prewired into the connector base, which is mounted onto the panel while the field cables are prewired into the connector hood. The hood is then plugged into the base on the electrical panel for a complete connection up to IP 69K.

Heavy-duty connector is especially useful for portable applications and testing facilities as it allows quick connection and disconnection. Although heavy-duty connectors are more expensive than cable glands, it minimises time and labour needed for onsite installation and commissioning up to 80%. It also reduces errors that could occur during onsite installation.

Heavy-duty connectors are typically made from Aluminium. However, Heavycon EVO from Phoenix Contact also comes in plastic (polyamide with reinforced fibre glass) to support applications that do not require metal housings and provides cost savings of up to 30%. Besides that, the dual entry cable gland enhances the flexibility for onsite installation. Phoenix Contact’s well known Push-in Technology is also used in Heavycon to further reduce the installation time.

  1. Cable entry system

Cable entry system (CES) is similar to cable glands. However, it helps to arrange the cables neatly and systematically into the electrical panel. By better managing the cables, the gland plate can be better utilised. It works in a modular form where the cable sleeves can be flexibly combined depending on the wiring. The slotted sleeves also allow the use of sensor actuator cabling while cone sleeves come in handy when the cable diameter is not predefined.

The cut-out of CES is the same as that of heavy-duty connectors. Thus, they are interchangeable. However, CES is not a pluggable connector. Thus, it is not suitable for applications that require frequent connecting/disconnecting.

  1. CES Multigate

Similar to CES, multigate offers great cable management. However, unlike CES, multigate has prefixed cable entry. Each cable entry is a cone-shape membrane that is able to accommodate a range of cable diameters. This is especially suitable for panels with defined cable specifications. As the cables are well arranged, it is easier to isolate faulty lines, if any.

  1. Service interface

Service interfaces make maintenance, servicing, and diagnostics easier than ever. The front plate comes in different configurations of D-SUB, RJ45 and USB, offering numerous combinations.  The mounting frame offers up to IP 65 protection with locking mechanism for extra security. This reduces the need to open up the panel during programming or configuration.

There are many factors to consider when it comes to choosing the most suitable cable entry method to your electrical panels. Let us help you with the selection by leaving us an email at marketing@phoenixcontact.com.sg!

Cable Entry System – CES

From |

Have you ever left your earphones in your pocket and when you wanted to use them again, they emerge as a tangled ball of mess? Annoying, isn’t it?

Well, the wiring of current and conventional electrical panels brings about a similar problem. The above picture shows its set up and at a glance, three words pop up in my mind: Complex; Costly; Time-consuming.

So why is this so?

Firstly, in the current system, multiple holes of different sizes need to be drilled in accordance with the cable sizes. Imagine the hassle having to drill ten holes of different diameter just to see messy wires intertwined together.

Next, a common occurrence to such wiring systems is the need to add additional cables. If you are lucky, there will be enough space on the flange plate to drill the extra holes. However, if the space is insufficient, or if you need larger holes for new cables, you would most likely have to replace the entire electrical panel and redo the entire wiring system from scratch. Not only does this add on to the hassle, it also adds on to labour and cost.

Lastly, conventional wiring systems require more time to rectify problems in communication. This is due to the difficulty in identifying specific cables especially when they are bundled together. The troubleshooting process thus leads to longer downtime which means financial losses for the company.

The Solution

Phoenix Contact has thus come up with a solution to eliminate this problem. Our Cable Entry System (CES) comes with specific features to tackle the hassle of the conventional system.

Firstly, only one or two holes would have to be cut to enable installation of up to ten cables in the system, greatly reducing the set up time. Furthermore, the CES can cater to different cable diameters ranging from 2mm-24mm. All these can be easily installed by mounting the sleeves of varying sizes on to the robust metal reinforced frame.

Next, additional cables can be installed by removing the blind sleeves from the extra cable holes provided by the CES. In the event that the existing cable configuration has to be amended, the CES allows for easy reassembly just by replacing the sleeves with those of different cable diameters. This eliminates the trouble of cutting out new holes on the flange plate.

Lastly, the CES allows cables to be easily identified as the rectangular frame organizes the sleeves holding the cables in an orderly manner that is easy on the eyes.

Besides tackling the inconveniences of the conventional electrical panel wiring, the CES offers protection class of IP54, making it suitable for harsh environment conditions.

If your current electrical wiring system reminds you of your ball of tangled earphones, it‘s about time you switch to Phoenix Contact’s Cable Entry System. Our CES will be the solution to increasing your productivity and cost saving to your electrical panels wiring.

Interested to find out more? Contact us at marketing@phoenixcontact.com.sg!

Routing Pre-Assembled Cables through the Housing Wall

From |

The new CES cable entry system from Phoenix Contact allows pre-assembled cables to be routed into control cabinets in a safe and space-saving manner.

The cut-outs and mounting dimensions of the CES system match the standard dimensions of heavy-duty plug connectors, which are installed in the control cabinet in a standard manner.

Continue reading →