Phoenix Contact presents a complete product line that offers new connection concepts to address the requirements of the new encoder generation. The two-part modular system comprises the M12 connection block and a rectangular flange. The dimensions of the rectangular flange are harmonized with the existing rotary encoder housings, so that encoder manufacturers do not have to redesign their devices.
Preventive Maintenance with Lightning Current Monitoring
From |The Lightning Monitoring System LM-S from Phoenix Contact provides information online about lightning strikes in plants and systems. As a consequence, service call planning can be optimized. This new system identifies and analyzes all of the important parameters of lightning surge currents based on the Faraday effect.
Lightning Arresters for LTE and WiMax Antennas
From |The demand for mobile Internet services is forever on the rise. Thanks to WLAN, it is possible to surf in the global network in nearly all buildings and major metropolitan areas. However, network coverage can be spotty outdoors, in public spaces, and especially in rural areas.
The Right Tool for Any Job
From |Phoenix Contact’s extensive range of professional tools has now been expanded to include a series of cutters for electronics and electromechanics. The new Microfox tools are especially suited for working with small electronic parts and components.
Thermomark – Coming this Fall.
From |Sentosa Development Corp for Sentosa Golf Course
From |Sentosa is a popular island resort in Singapore , visited by some five million people a year. The attractions include a two-kilometre long sheltered beach, Fort Siloso , 2 golf courses, 2 five star hotel , a World class Casino in Resort World Casino and featuring the theme park from Universal Studio.
What does this have to do with Phoenix Contact?
Read more after the jump.
Installation Terminals with Push-In Connection Technology
From |Phoenix Contact’s new generation of installation terminals is tailored to the requirements of electrical installation and distributor construction. The terminals are available in various designs as three-level and N disconnect terminals with the matching feed-through, disconnect, and ground terminals. Conductors with cross sections ranging from 2.5 to 10 mm² can be connected. These compact space-savers with widths starting at 5.2 mm offer many advantages in terms of handling, especially in installation technology.
Case Study: PTT UT
From |Southeast Asia’s oil and gas giant PTT from Thailand run their projects actively in Thailand Province “Rayong”. As PTT UT commonly build water treatment process plant along with their existing Oil and Gas plant. Electrical panels installed at site, commonly face with difficulty such as space limitation Therefore, all components installed must me space saving and yet reliable in functionality
Ethernet Switch for Harsh Environments
From |Phoenix Contact is now offering a five-port Ethernet switch with IP67 protection for use in harsh industrial environments. This switch sets itself apart as a result of the compact design and its ease of installation that makes it ideal for the machine construction sector. Its housing is only 30 mm wide so that it can be installed on a standard structural element completely and without any protrusion.
600V Power Connector with UL Approval
From |Suitable for the ME and ME MAX family of housings from Phoenix Contact, and in addition to the classic plug connections for 250 V, the GMSTBO 2.5 HV high-power base strips with matching GMSTBT 2.5 HV screw plugs are now available for compact device applications in the area of power electronics.