Category Archives: Uncategorized

PTSM – Phoenix Contact’s most versatile and powerful low pitch connectors

From |
PTSM Connector

PTSM Connector

Phoenix Contact is well known for the high current terminal blocks and connectors which are widely used in the power devices such as frequency converters, inverters, power supplies & many more.

These connectors are able to support large size wires such as 10mm cross-section, 10mm pitch and high current capabilities. However, many are not aware that in the market of 2.5mm pitch connection, Phoenix Contact has a versatile product family, PTSM, and they are available as  Terminal Blocks and Plug-able Connectors.

The PTSM series offer

PTSM PCB to PCB Connection

PCB to PCB Connection

PTSM Wire to Wire Connection

Wire to Wire Connection

PTSM Wire to Board Connection

Wire to PCB connection

Furthermore, it has Through Hole Mounting and SMD mounting as well. So what is so special about this series of connectors? When should you choose such connections?

  • PTSM are the only 2.5mm pitch connectors capable of handling up 6A/pole.
  • These are small connectors, only up to 5mm in height.
  • The small size is critical when there is limited space on the PCB.
LED Lighting Application

LED Lighting Application

The PTSM series was initially developed for the LED Lighting market in 2012. Since then, the product has seen much improvement and has expanded its range within this Product family.

Recently, we managed to introduce the PTSM to a multi-national OEM company in Penang, Malaysia. They used to produce Test Measurement system that was well known globally. But have since re-focused their products to the areas of Life Sciences/Health and Medical solutions.

Every year, Phoenix Contact Sales personnel will arrange product road-shows to our existing and potential new customers. With 15 sets of sample boxes and 8 pieces of Demo PCB, I paid this customer a visit.

During the roadshow, one particular customer showed a specific interest in the PTSM. Which prompted him to ask what was this connector developed for? According to our product brochures, the PTSM was designed for T8 lighting or down lights.

Instinctively, I continued our probing and explored ideas with that R&D Specialist.

Eventually, he began to share his worries and concern for his design, and now that he has found the PTSM, he was relieved. He had been looking for a 3~6 pin connections to a DC Stepper encoder board that he was developing. This DC stepping solutions would be used in certain robotic functions in the Medical/Healthcare solutions.

He had been looking at conventional connectors of most of the known brands. All of them only offered up to a max current of 1.5 or 2 A per pin and were also not designed for reflow process.

This customer had been under the impression that we only had the FK-MCP or SPT series which they have been using in their solutions. The Road-shows has proved to be effective in bringing the new products and solutions to the customer.

The PTSM provided the solutions to this customer’s problem despite being originally designed for lighting applications. Finally, this connector has become a standard library solutions, that is adopted in this MNC for most of their DC Stepping/Encoding application.

The message I’m sharing is that, opportunities are created by having the right product and the right attitude. Even if the product was not develop for a particular industry, it does not mean that there will not be a demand for it. Create the Demand!

If you would like to know more about Phoenix Contact’s PTSM connector, check out our website or leave us your contact and I will get in touch with you shortly.

Quality of Service: Phoenix Contact Thailand

From |

Quality ServicePhoenix Contact strives to deliver excellence in both product quality and customer service.
Our team mission is for our customers to achieve optimal satisfaction when they use Phoenix Contact products.

I’ve never imagined that I would be writing an article for the company’s official blog. I did not consider myself a good writer; even curating a short post was not easy for me.

However, one cannot avoid challenging tasks forever.

Phoenix Contact is an electrical engineering company. We manufacture our own industrial-grade electronic devices and solutions. Our core products are our terminal blocks!
Most of our blog articles are technical or solution-based in nature. Thus, I felt that articles should be written by our product managers or engineers.

I had to crack my brain to figure out what article to write. It took me a whole week to think of something! Since I serve customers directly, I decided to write about why customers choose to work with us. From a salesperson’s point of view, customer relationships are key. We always do our best to figure out their likes and dislikes, and understand more about their needs.

QUALITY IS OUR PRIORITY.

Our Design and Engineering Team back in Germany ensures that all products are high-quality and user-friendly. The best proof? Our customer satisfaction feedback for product quality is always 100%, and they never have to worry about quality issues! We are extremely grateful for the constant effort that our German colleagues invest in product quality.
Additionally, we emphasize on providing great customer service to every client, and we work together as a team, from colleagues to our Southeast Asia headquarters back in Singapore, to each individual subsidiary sales office around the region. Every team member has a common goal – which as our team mission states: optimal satisfaction from start to finish with every purchase.

How do we define excellent service?

Here’s the breakdown:

Our sales team responds promptly to each customer regarding any kind of purchase, or project, regardless of size or nature. We understand that time is precious, so we try our very best to get back to our customers ASAP.

Our product managers are always on standby to assist and support any technical issues that may arise. They are also responsible for price negotiation. At Phoenix Contact, we try to make our product prices fair and reasonable to all customers. We suggest only what they need and we don’t upsell. We take pride in making our customers feel comfortable about what they are purchasing.

Our customer service team supports any order enquiries, while our logistics team handles the rest of our requests which are deemed as “almost impossible to be solved”. Almost impossible – but not completely!

We are not just a company that is solely about profit generation. We genuinely would like our customers to work with us to establish long-term friendships and working relationships.

If you are looking for a solution, a product, or an answer to your industrial problems, do not hesitate to contact us. We’re always here to help!
Just drop me an email or text at:

Rattakarn Chartnakrop, DC sales Division (Thailand)
Mobile : +(66) 81 782 8826
Email : rattakarnc@phoenixcontact.co.th

Phoenix Contact IIOT – Overcoming Challenges Together

From |

In the last few months, we have shared on how IIOT is useful for Power, Oil and Gas and Water Industry: In Power Industry, IIoT is intricately linked to the implementation of Smart Grid and IEC61850. In Oil and Gas where profitability is a bigger concern than ever, IIoT can help to reduce operations cost and minimizes downtime by allowing for predictive maintenance. For the water industry, we shared a possible scenario whereby IIoT is adopted by a facilities manager to understand about his systems.

If you have not already read those articles, click on the images below.

Products for IEC 61850

IIOT for Power

Reservoir

IIOT for Water

Process Plant

IIOT for Oil and Gas

How Phoenix Contact IIOT can help you get started

After engaging our customers in this topic, we have gained further insights and in this article, we will like to share some of these concerns and how we have helped customer overcome them.

  1. How do we know for sure that we will have returns of investment from implementing IIoT?
    There are indeed risks when it comes to Industrial Internet of Things, especially when data mining (finding patterns from database of data with no seemingly no use) is involved. Compared to traditional engineering methods where an engineer spot a problem or area of improvement and work to improve it, Big Data and IIoT is very much about not knowing problems, not knowing areas of improvements, yet hoping for some “miracle” to happen.Phoenix Contact reduces this risk in several ways:

    1. We provide free demos for customers to try.
    2. We provide data analytical and preparation services for customers to greatly enhance the odds of IIoT succeeding. This may seem easy, but data preparation and combination from disparate sources with different formats and different headers is really a tougher challenge than many expected. At least that’s what we gathered from feedbacks anyway
    3. We encourage our partners to start with a system that is well known to benefit from IIoT. For example: Energy Savings, Predictive Maintenance and we help our partners along the way to achieve it.
    1. How do I collect data from many sources and combine them together! It’s so complicated. How about reliability, cybersecurity, electrical surge ……
      Phoenix Contact addresses this by:

      1. Our Phoenix Contact IIOT Connectivity Solution is a portable, plug and play box including softwares that are able to ingest data of any format.
      2. PICS is fully customizable, which means that you can add Phoenix Contact reliable and extensive range of products to form a solution just right for you. This includes a wide range of data connectors including IP67 rated connectors for wet/dusty/oily industrial areas!
      3. Phoenix Contact will partner you along this journey and overcome these difficulties with you!
  1. IIoT is expensive!!Phoenix Contact products are not only inexpensive, but the ROI it provides is way more than the initial cost! And as explained in point 1, we even provide you with full working demo and data analysis so you don’t have to spend till you are convinced!

To help you get started, we have a Phoenix Contact IIOT Quick Start Guide. Get your copy today!

If you will like to consult with us with regards to implementing IIoT, leave us your contact at marketing@phoenixcontact.com.sg and we will get in touch with you shortly.

5 Reasons to Consider an Industrial PC

From |

In most companies, the Information Technology (IT) departments are usually the team responsible for hardware configuration, physical implementations, software installation and many other services in relations to PCs within the company.

As a business, having downtime and substandard quality in their PCs or IT-related infrastructure could affect overall performance.

This may not bode well as lacking behind could open up advantages to competitors and slow reaction time to meet customers’ demands.

To ensure that your business keeps up with the Joneses or perhaps even outperforms against competition, you need to rely on Industrial PCs.

Why, you asked?

Simple! Because off-the-shelf solutions may not work for some as there could exist limitations.

Here are 5 reasons:

  1. Form Factor
    Industrial PC is an option you should consider because it comes in multiple form factors. If a 19” rack mount solution is required, various options are available.

    Rack-mounted PC

    Rack-mounted PCs

    In instances where a smaller cabinet or tight space limit the size of the PC, you can utilize a 6-slot/8-slot Wall Mount or Desktop.

    If space and air flow both play a major factor in your decision-making, you can go with a Din-Rail, Stand mount or Wall mount Embedded PC. If you’d like to combine a HMI with the Embedded PC, there are a myriad of 4:3 and widescreen touch/multi-touch solutions available.

    If a stand-alone HMI is preferable, you can configure a Touch Panel ComputerPanel PC or Industrial Panel PC to meet your specific requirements.

    For Phoenix Contact, we offer varying types of PCs and HMI to suit different applications. Again, because it’s designed to be space saving and comes in different form factors, you won’t have any issues selecting the right solution for the right task.

 

Industrial PC

Industrial PC

  1. Performance
    There is a common misunderstanding that Industrial PCs can’t run as fast as some of the off-the-shelf PCs.In reality, performance is the forefront of most Industrial Computer manufacturers. The majority of industrial computer manufacturers partner with CPU providers (such as Intel) to continuously develop product lines based on CPU trends and long-term availability.Our CPU comes suited for the application, with the latest generation of high-performance and energy-efficient Intel® Atom™, Celeron® or Core™ i processors.
    Not to mention, running on operating systems for every application from Windows® 7 or 10 and even Windows® Embedded Standard 7.

 

Panel PC

Panel PC

 

  1. Endurance & Durability
    Industrial computers are characterized by long hours of operation, resistance to vibration and shock from occasional thumps.Commercial-grade computers are not designed to withstand long operating hours without overheating and potentially damaging its internal components.On the other hand, industrial grade computers have integrated cooling “fans” or device to help dissipate heat efficiently. In fact, the most common reason for failure in consumer-grade computer is the low grade power supply and electronics used.
    If you plan on acquiring commercial grade computers for your industry to be used more than 25 hours per week or even 24 x 7, you should definitely reconsider an industrial PC.

    Designline PC

    Designline PC

  2. Display Technology
    Display is one key technology that is most often neglected. A display that is suitable for indoor use is not necessarily suitable to be used in the outdoor environment.One might argue that you can increase the brightness of the display to the maximum when used outdoors, however it will never be enough to compensate for the brightness of the sun. Thanks to optical bonding, the displays of our outdoor HMIs and industrial PCs can be read effectively at any time.In addition to this, they are provided with an anti-reflection coating (AR coating) and can therefore even be read in dazzling sunlight. An integrated UV and IR filter also ensures a long service life for the industrial PCs.

    Designline PC

    Designline PC

  3. Customization
    The ability to customize your Industrial PC configuration to tailor exactly to your application’s specifications is valued more than everything else.Many, if not all, of the off-the-shelf PCs are limited in customization and although they provide the minimal performance, they generally do not allow various customizations.
    Users require configuration flexibility due to the multiple CPUs, varying amounts of memory and multiple I/O card required.With an Industrial PC, you could provide hundreds of “one-off” solutions that can enable you to fulfill your every requirement; for each task without costing you additional on hardware/software configuration.If you still doubt the quality of our HMI, you can watch the physical test we ran (*We highly advice you not to try such stunts as we won’t be responsible if you hurt yourself).

Want to find out more? Feel free to contact us at marketing@phoenixcontact.com.sg!

UPS IQ – Smart Power for Intelligent Transport System

From |

The Land Transport Authority (LTA) recently awarded a tender for the Intelligent Transport System (ITS) to one of their system integrator to setup effective system for monitoring of traffic situation at junctions. The system, which is part of the Smart Nation Initiative Program, will automatically alert the operator of the traffic volume so that remedial actions can be taken promptly.

Traffic Camera

Intelligent Transport System (ITS)

The Intelligent Transport System (ITS) is at the heart of what keeps us safe on the roads and tunnels system in our city. In land-scarce Singapore, ITS’s sophisticated traffic and control system will maximize road network efficiency capacity as well as monitor and manage the traffic flow.

The ITS infrastructure spans over 164km of expressways and road tunnel system, including Kallang-Paya Lebar Expressway(KPE), Marina Coastal Expressway (MCE), Central Expressway (CTE), Fort Canning Tunnel (FCT) and Woodsville Tunnel (WVT).

Our partner in Singapore has worked wholeheartedly with this system integrator, from design to testing and finally, to the implementation with our UPS-IQ.

Solution

Together with our partner, we set up the actual UPS and communication system to show to the system integrator. This was to provide the proof of concept to simulate the system. A demonstration of the UPSconfigure software allowed the UPS system to be integrated seamlessly into the innovative application from the special system by the system integrator. The system will be manned by LTA.

UPS IQ

UPS IQ

Key Features

  1.  High MTBF – Higher MTBF (>600,000 hours) as compared to most of our usual competitors ensures more reliabilty.
  2. Modbus Enabled – This has enabled the system to be communicated within the same network. It allows the system to be monitored from the main control room without additional hardware which translates into lesser points of failure and eventually to cost savings.
  3. Monitoring software (UPS Config) – The UPSconfigure feature allows the innovative application of the system integrator proprietary software to be integrated seamlessly into their application. This speeds up the deployment process and allows the system integrator to make more efficient time, labour and tools deployment.

If you would like to find out more about our UPS-IQ, check out our website or just leave us your contact at marketing@phoenixcontact.com.sg and I will get in touch with you.

QPD in Conveyor Systems

From |

QPD is a product that was launched few years back. While this “forgotten child” is hiding somewhere in the dark recess of Catalogue 2, I feel that the QPD deserves some credit and limelight.

When we present QPD, we always talk about the concept of it and how it benefits the customers in time & cost saving. QPD was never meant to be in the “cheap” category and I think all of us know that good & fast things aren’t cheap!

I would like to share my recent experience with a customer who was deals in warehouse management system. Generally, this system is actually automated conveyors ‘pick & place’ goods and deliver to a designated area.

Conveyor System

A typical conveyor system consists of 2 zones. Firstly, there is the Safe Area (controls) and then the field area (site). The Safe area usually houses the main PLC, whereas the field area is the sensors, motors, e-stops, etc. There will be multiple stations at the field area which usually stations the motors, isolators, e-stops, etc. The number of stations is very dependent on the size of the system itself. These stations are quite a distance apart from each other and power cables are necessary to be laid across the conveyor system to power up the motors, electrical components, etc.

Conventionally, power distribution boxes are used in each station to split the main power to the respective individual stations. This power distribution box has one main requirement; at least IP65 rated. This is where QPD comes into the picture where it fulfills the IP requirement and while offering even more compared to the conventional junction boxes.

Conventional way
 Din Rail

+

 PT Terminal Block

+

 Junction Box

+

 Cable glands
Din rail Terminal Block Box Glands

QPD – The Phoenix Contact way!!

QPD H Distributor QPD T Distributor

This solution require either the QPD H- or T- distributor only! No special tools needed!! No cable stripping & crimping process. This saves you up to 80% of installation time.

https://www.youtube.com/watch?v=4HPZ1P-1NVU

In conclusion, yes you might need to pay a premium for QPD but I am very confident that the gains you get outweighs what you paid.

Check out our website for more information or leave us your contact and we will get in touch with you.

Make-before-break – Terminal Blocks for CT Test

From |

Make-Before-Break

Make-Before-Break (MBB) is a term “Denoting a switch or other device in which a new electrical connection is made before the existing one is broken”. In short, it simply means, shorting the circuit before disconnecting it.

You may know about MBB when purchasing a relay. But do you know there are terminal blocks designed with MBB in mind too? These MBB terminal blocks can usually be found in power industry applications.

For those who are familiar, you may have come across this term (MBB) during a Current Transformer (CT) testing on a protection relay. However, do you know the importance of ensuring MBB when conducting a CT test with your Terminal? Or what the consequences will be of not having a terminal blocks that comes with a MBB feature during the test?

Protection Relay

A CT will certainly be at risk of being destroyed or even worse (Explosion!) if the secondary is left open circuit while the primary current is present. This is due to the insulation failing from the “higher than rated” voltage that occurs. Therefore it is extremely important to ensure MBB before conducting a live testing. A good terminal block with MBB feature will definitely help you provide the extra mile in ensuring safety.

How does the MBB terminal blocks function and what does it look like?  Here are some good examples of a good MBB terminal block.

  1. A good MBB terminal block must have the feature where shorting is always present first before you are able to break the circuit. It would be best if the terminal blocks are able to automatically perform the short circuit for you whenever it is being disconnected during the CT test.
    Short Circuit function closed Short circuit function open
  2. Clear indication of Short Circuit and disconnection must be visible and this allows your engineers to have an ease of mind during testing.
    PTME
  3. Good MBB terminal blocks should have safe and easy to operate features. Having said that, these features can help to cut short the time while testing (shorten the risk) and ensuring the safety of the person that is conducting the CT test.
    PTME Terminal Blocks for CT Test

So where can you find good MBB terminal blocks for your applications? Phoenix Contact, of course!

With 94 years of experience manufacturing and designing terminal blocks for the Power Industry. Phoenix Contact has never stopped developing new innovative testing terminal blocks that will suits your application, at the same time ensuring safety and quality.

For more info, check out this video of our PTME terminal blocks or visit our website!

If you have more inquiries, feel free to contact us at marketing@phoenixcontact.com.sg and we will get back to you as soon as possible.

How IIoT Solutions Make You Look “Smart and Cool” for the Water Industry?

From |

ReservoirThe term Internets of Things (IoT) was coined by Kevin Ashton in 1999 and the big corporate players like Google, Facebook, Apple, Samsung and LG have been practicing it for years. In recent years, it has become a hot topic and IoT ‘tech’ has started to flood the market.

Now, every ‘Thing’ would need to look smart and cool, hence not only has the phone started to “think and talk”, the Smart Devices, Smart Appliances, Smart Home, Smart Car, Smart Factory, Smart City are starting to form a Smart World.

How can the Water Industry catch up with this “smart” trend?

Let’s see what have the big players done so far. GE has launched Predix, a cloud-based platform that enables asset functionality monitoring.  IBM® Intelligent Water software has been developed to deliver smarter water management through insights from data to help utilities manage pressure, detect leaks, reduce water consumption, mitigate sewer overflow, and better manage their water infrastructure, assets and operations. According to US Environmental Protection Agency (EPA), the researchers at Clemson University are building the “Intelligent River” to provide real-time monitoring, analysis and management of water resources.

Of course, it would be cool if we can apply Industrial Internet of Things (IIoT) across entire assets, collect the big data from all the facilities perform a thorough analysis in order to find out the insights to improve operational efficiency, enhance productivity and create new opportunities. However, this ideal case unlikely to happen due to the limitations of knowledge, budget, risk, standardization and legacy installed base.

I believe a lot of people will agree with me that we need to “start small” for new ventures in order to gain experience, take the calculated risk and predicted outcome. Let me share a case here to demonstrate how we can achieve that in the water industry.

IIoT Implementation

A reservoir is surrounded by a few pumps / lift stations; the reservoir is 100km away from the centralized SCADA system. A standalone PLC and Ethernet Remote I/O is in place to control and monitor the water level of both reservoir and pump stations.

Kelvin, the Facilities Manager is being assigned to explore the implementation of IIoT within a timeframe of 3 months with budget of less than US$7,000. It should have low cyber security risk, justifiable benefits and consideration of future extension.

Kelvin has decided to pursue a simple IIoT project by partnering with an IIoT service provider. They deploy more sensors at field (e.g. weather stations, thermistors, BTU meter) and install a connectivity box next to the PLC. The sensors will collect more data such as temperature, humidity, energy consumption and water quality.

The connectivity box can take in additional signals and the I/O is expandable for future extension and the box is designed with unique connector for easy plug and play. The box is also equipped with 4G router in order to send the data back to the centralized SCADA and subsequently send to the IIoT platform securely (data is encrypted).

The collected data is in real-time and can be analysed individually (e.g. pump energy usage) and interoperability (e.g. pump can run at lower speed during the hot weather). The analysed data can be used to predict pump failure, save pump energy, early detection of the contamination or give early flood sign.

IIoT for Water Industry

Kelvin has accomplished his mission and now his ‘THINGS’ look ‘smart’. In addition, he can easily communicate with his team about the current status, problem or performance of each facility by using the dashboard and generate a report in the structured data format (e.g. text, graph, image, video) for his management to discuss further improvement or to identify new opportunities. Do you think now Kelvin also looks “smart and cool”?

There are plenty of ways for you to implement the IIoT platform depending on your current situation (e.g. remote area, existing with or without SCADA system, multiple sites) and technical and commercial requirement (e.g. cyber security, cloud-based, redundancy, future expansion, budget).

Phoenix Contact offers flexible and customize IIoT solutions inclusive of the connectivity box, please feel free to drop me an email eexinchong@phoenixcontact.com.sg for clarification or discussion.

or register for our free e-book.

Data Exchange Between Enterprise and Automation Control Level

From |

Phoenix Contact's ILC for easy data exchangeAt present, control applications focus not only on reliability but also flexibility. Following current automation trends in automation 4.0, many vendors will need to improve market share in this market segment.

Interface data between third-party functions might be considered to develop parallel to improve the product quality. For controller device, we can classify its interface levels into field level and enterprises level.

Usually, there are no issues when various controller vendors need to transfer data between one to another at the field control level.  This is because there are many common protocols like MODBUS, PROFIBUS and etc to exchange data easily between third-parties. However, it is a different story when there is a need to exchange some data at a higher level like in an enterprise system.

A couple of constrains when designing interface system is the data exchange rate and also the time lag which occurs. In order to maintain a high quality data exchange rate, it is often deemed necessary to utilize high-end hardware and software, resulting in a very expensive solution.

Easiest Controller for Data Exchange between Enterprise and Automation Control Level

Phoenix Contact’s controllers, right up from our basic series, have a library which is able to connect directly to a RDBMS database by providing query string patterns like common SQL script. In comparison, other controllers require additional equipment or other APIs to collect data from controller first before sending it to the target database.

Easily enable data transfer from the sensor directly to a DB with Phoenix Contact’s Controllers.

Reference product

System overview

System overview

For more information on Phoenix Contact’s Controllers, leave us a message and I will get in touch with you soon.

Data Connector – RJ45

From |

As more factories go into automation, more networks and fieldbuses are used for communicating between machines and people.

RJ45 is one of the most commonly used connector.

What is this RJ45?

It is a type of standard connector for network cables, especially Ethernet.

RJ45 CableSome of the common issues faced with RJ45 connector include intermittent data. Most RJ45 connectors in the market come with a plastic clip.

RJ45 Connector clip

The plastic clip helps to form a secure connection between the connector and the socket. It also ensures that the connector stays seated on the socket.

You would need to exert some pressure on the plastic clip in order to unplug the connector. However, the plastic clip is usually fragile.

It breaks easily when bend backwards or when the connector is dropped on the floor. Without the plastic clip, the transmission of data is not guaranteed. The RJ45 would then be used with the nearest trash bin – if you know what I mean.

E-Waste in bin

Often times, even when the plastic clip is intact, intermittent data could occur due to vibration from the surrounding machines.

Other issues surrounding the RJ45

Moreover, the process of crimping a RJ45 can be tedious. In order for the connector to function properly, the cable (with as many as 8 cores) has to be crimped into specific standards, namely T568S and T568B, with a special crimping tool.

T568A and T568B wiring

Crimping is a manual process and depends very much on the workmanship of the person who is doing the job.

If it is not done properly, the crimp contact will not sit properly within the connector and the data transmission will be affected.

Crimping is an irreversible process. If the connector is crimped wrongly, it cannot be un-crimped (word of caution).

It has to be scrapped and the damaged cable has to be cut which causes wastage.

CAT 6 Twisted Pairs

Problems, problems and more problems. So what’s the solution?

At Phoenix Contact we build innovations based on issues that every day people, like you and me, have.

Phoenix Contact Industrial RJ45 is equipped with 2 springs at the top of the connector to ensure that the connector is sitting snuggly within the socket, even during high vibration applications (yes, even the extreme ones).

Phoenix Contact's RJ45 Connector

Phoenix Contact plastic RJ45 connector is made of special plastic. It could not only bend 180 degree without breaking but it could also resist the impact of dropping on the ground.

QUICKON RJ45 Connector

Phoenix contact QUICKON RJ45 connector allows you to terminate cable without the need to strip the cable and the use of expensive crimping tool.

The connector is colour-coded so there is no need to memorise the standards.

IDC Conenction

In addition, the connector is able to reconnect up to 10 times. Meaning to say, there is no need to scrap the connector if it’s connected wrongly. Just follow the simple steps below to terminate the cable.

RJ45 Quickon assembly step-by-step

Or alternatively, if reading is a chore, you can watch this video right here:

https://www.youtube.com/watch?v=Pm2wNf9DUCk

See how easy that was? At this rate you’ll be producing thousands of RJ45 within seconds.

So if you’re looking for a reliable and problem-free RJ45 cable, look no further.

Leave us an email at marketing@phoenixcontact.com.sg to request a product demo today!