Category Archives: Industrial Electronics

Preventive Maintenance with Lightning Current Monitoring

From |

The Lightning Monitoring System LM-S from Phoenix Contact provides information online about lightning strikes in plants and systems. As a consequence, service call planning can be optimized. This new system identifies and analyzes all of the important parameters of lightning surge currents based on the Faraday effect.

Continue reading

Ethernet Switch for Harsh Environments

From |

Phoenix Contact is now offering a five-port Ethernet switch with IP67 protection for use in harsh industrial environments. This switch sets itself apart as a result of the compact design and its ease of installation that makes it ideal for the machine construction sector. Its housing is only 30 mm wide so that it can be installed on a standard structural element completely and without any protrusion.

Continue reading

Intelligent Energy Data and Motor Management

From |

Phoenix Contact combines distributed I/O stations and interface modules to create a seamless and integrated solution for energy and motor management. Whatever the requirement – be it the monitoring of the active power of server cabinets in a data processing center, energy-saving monitoring and switching of motors in production plants, or the management of standby functions in machines – all of these tasks can now be solved even more intelligently.

Continue reading

Universal Temperature Transducer with Switching Outputs

From |

Phoenix Contact’s new universal temperature transducers belonging to the MACX Analog family of isolating amplifiers have been developed and produced in accordance with the functional safety standard in all steps of the product lifecycle. The modules include a signal input for a resistance thermometer, thermo elements, resistance-based transmitter, potentiometer, millivolt sources, as well as for customer-specific characteristics.

Continue reading

Easy Wireless Networking

From |

Lose the wire but not the signal!

If data is to be transmitted to a moving, rotating or mobile device, Industrial Wireless solutions are the answer. They are also recommended for temporary installations. What already has been practiced in the home and office areas for years can now also be successfully used in the industrial area.

Continue reading

EASY Wired Networking

From |

One network, Countless possibilities!

Industrial Ethernet from Phoenix Contact offers you a powerful and complete network solution. Our network products range from the ethernet switches, serial converter, and network security module even wireless over ethernet.

Continue reading