IO Link

From |

Have you ever encountered the following situations?

  • Machine stops suddenly due to contaminated sensor/actuator
  • Stopping the machine in order to change to another color detection (or other parameters) on the sensor
  • Stopping the machine when replacing a faulty sensor in order to set the parameter of the new sensor

What if you can…

  • Re-parameterize the sensor without shutting the machine down
  • Replace a new sensor with the previous parameters automatically downloaded without shutting the machine down

The above is made possible due to the IO Link technology. IO Link is a standardized IO-technology (based on IEC 61131-9) focusing the communication between field devices and sensors & actuators. This enables the exchange of both process data and service data between the connection and sensor/actuator. With the IO Link technology, devices can now identify and configure themselves automatically. This will enable an easy replacement of defective components and reduces downtime significantly.

An IO-Link system consists of the following basic components:

  • IO-Link master
  • IO-Link devices
  • Standard 3-wire sensor cable/actuator cable

Phoenix Contact offers a comprehensive IP20 and IP67 portfolio of IO-Link masters, IO-Link devices, cabling, and software.

If you need further consultation on your next IO-Link application, please do not hesitate to drop us an email at marketing@phoenixcontact.com.sg!

Avatar photo

About Jiang

Jiang helps customers in providing effective automation solutions to reduce costs and improving overall efficiency.

Share

Share

Tell your friends about us!

Contact

Leave a Reply

Your email address will not be published. Required fields are marked *