Pluggable Compact PLC Relay
Is space and cost a concern for you when designing-in relays for automation?
Phoenix Contact’s PLC Relay eliminates the need for extra terminal blocks, helping you reduce both space and cost. Let us see how.
PLC Relay Actuator Series

Relay-Actuator Setup
In applications where only one normally-open(N/O) contact function is required, you can use Phoenix Contact’s PLC to Actuator output relays to interface with actuators, such as motors, contactors or solenoid valves.
You can connect all actuator connections, including the load return line, directly to the relay. Hence, eliminating the need for additional output terminal blocks to transfer power.
The benefit is daisy-chaining or looping the wiring for the power will not be necessary. This is illustrated in the wiring layout below.

Relay-Actuator Interface

Relay-Actuator Schematic
PLC Relay Sensor Series

Relay-Sensor Setup
Likewise, Phoenix Contact’s PLC to Sensor input relays can be used to interface with sensors, such as proximity switches, limit switches or auxiliary contacts, where only one normally-open(N/O) contact function is required.

Relay-Sensor Interface

Relay-Sensor Schematic
Similar to the Actuator Series, you can also connect all sensor connections, including the supply voltage for the sensors/switches.
As you can see, available with screw, spring or push-in field terminals, Phoenix Contact’s relays will:
- Open up Space on the DIN rail
- Reduce Labor and components costs
- Eliminate an extra point of failure
Ultimately, you can save approximately 80 Pecent on your DIN rail and approximately 60 percent less time on installation.
To find out more, click here





Did you know that in the Process Industry, there are more than 40 million devices that are running on the HART Protocol and more than 75% of them are HART-enabled. However, up to 90% of these HART-enabled device are being under-utilized, used only to read the 4…20mA signal.