My previous article on Handling Objections was very well received by most of you. If you have not read it, I strongly advise you to read it.
Since I am on a roll, I have decided to write another article on a topic: Bouncing Back!
My previous article on Handling Objections was very well received by most of you. If you have not read it, I strongly advise you to read it.
Since I am on a roll, I have decided to write another article on a topic: Bouncing Back!
It has been almost 6 months with the launch of our new website. I am sure that the new interface of the website is much nicer looking and easier to navigate.
Our new website has been completely redesigned from the ground up, and with so many new functions and information on our website, it can get a little bit confusing. But once you get used to the new interface, you will find that it is actually very easy to navigate around the website!
Contact us at marketing@phoenixcontact.com.sg to find out more!
Day 3
William kicks off the day’s training with a session on our Interface products.
And follows up after lunch with a ‘Powerful Session’ showcasing our power supplies; reinforced with plenty of live demos for the trainees to have a hands-on experience.
Every year, we conduct a basic training for new staff from our various Southeast Asian subsidiaries, rep offices and select distributors. This year is no different. However, we made sure that the participants got a totally new experience.
2014 is the year of the Brazilian World Cup so in line with this, we decided to use the World Cup theme as a basis for this training. Continue reading
The new M23 Hybrid round plug-in connector from Phoenix Contact is an all-in-one connector that securely transfers signals, data, and power.
The compact M23 plug-in connector can handle currents up to 30 A and voltages up to 850 V DC or 630 V AC. Continue reading
Uno Power power supply units, now available in 15 different modules, offer output voltages from 5 to 48 V DC. Their high power density and compact control cabinets speak for themselves, and they can reliably handle loads of up to 100 W.
Uno Power has also significantly reduced energy consumption as compared to other commercial products, with low no-load losses of under 0.3 Watts and a degree of efficiency optimized at over 90%. Continue reading
Phoenix Contact provides heavy-duty components for network infrastructure in energy systems. Our components conform with both IEC 61850-3 and the comparable IEEE 1613 standard. Continue reading
The new ME-IO housing system from Phoenix Contact is expanding its electronics housing line to include front connection technology.
The modular system, just 18.8 mm wide, can accommodate up to 36 connection terminals. The lock-and-release system makes locking and releasing the plug from the housing system easy as pie. Continue reading
PLC logic, Phoenix Contact’s new programmable logic relay system, is particularly well suited for small automation tasks. It combines the strengths of established relay technology with logic functions in a single package. Continue reading