Phoenix Contact is expanding its glass fiber optics product line to include the M12 circular plug connector. Now it is possible to fit indoor, flex and outdoor cables in variable lengths with all available connectors. In addition to our standard products, we also offer customized solutions tailored to our customers’ individual requirements.
Monthly Archives: January 2012
Fast Profibus Extender with Surge Protection
From |The new Profibus extender from Phoenix Contact enables straightforward integration of remote Profibus devices at data rates of up to 1.5 Mbps. The extender has two DSL connections per device. This means that in addition to point-to-point connections the extender can also be used to easily establish line structures with up to 30 devices.
I/O Communication Terminal Integrates Profibus Devices
From |The IB IL PB-MA-PAC inline I/O communication terminal now enables the integration of Profibus devices into the Phoenix Contact automation solution.
A Visit to Newater
From |30th Nov 2011 marks a special and important day for Phoenix Contact (SEA) Pte Ltd. What is so important and special? Hear this, we hosted 4 VIPs from Germany who are, Mr Frank Stuehrenberg, our Executive Board Member, Mr Ulrich Leidecker, our General Manager of Phoenix Contact Deutschland GmbH, Mr Hanno Hardt, Director Media of publish-industry, Mr Thomas Rilke, Director Metropolitan Solutions at Singapore Newater Visitor Center.