Tag Archives: wireless technology

Wireless Technology: the Industry 4.0 Backbone

From |

Industry 4.0 is the 4th generation industrial revolution. This world-changing principle enhances productive efficiency in smarter and faster ways by utilizing the state of the art technology of data analysis software alongside powerful computerized hardware capabilities.

The key to the success of Industry 4.0 is to connect thousands of devices to the central system in order to allow exchanging of various parameters to the processing unit, such as humidity, temperature, status, level, etc. Not only is data transmitted, but devices also receive commands for further actions.

Actually, the powerful hardware and advanced software capabilities have existed for over 20 years. However, the increased number of devices connected to the system means a higher cost of investment. In the past, the only reliable connectivity was through wired cables, which investment cost was directly related to the complexity of the number of devices.

This key obstacle has been rapidly resolved by the advent of reliable wireless technology. Today, various applications of wireless technology have been proven and widely used, such as:

NFC: Near Field Communication

RFID: Radio-Frequency Identification

Wi-Fi: Wireless Fidelity

What makes people trust wireless technology?

Security: New advancements in data encryption technology protects data from intruders.

Speed: The new standard of network 802.11ac helps increase data transmission speed to 10 times faster than the old standard which is sufficient for industrial control systems.

Savings: All stakeholders follow the wireless markets trend. Therefore, new hardware for wireless technology has been introduced daily. This brings significant reduction in the price of wireless devices which mean tremendous savings during investments.

Phoenix Contact offers a huge portfolio of products under the category of wireless technology, as shown below.

Safe Wireless Installation for Hazardous Areas

From |

a_0064853_intWireless technology has improved by leaps and bounds over the last decade. Intermittent, unstable and slow wireless connections are gradually becoming a thing of the past. At the same time, wireless technology brings about tremendous convenience to everyone, reducing clutter caused by messy wires and making hard to reach places reachable. Continue reading