Tag Archives: power

Power Reliability for the ‘New Normal’

From |

With the backdrop of COVID-19, the new reality taking shape is made of complexity, uncertainty and opportunities. Industries are rapidly adjusting, and as the crisis unfolds, it is important for us to adapt to the new ways of business and life in this ‘new normal’.

The 4th Industrial revolution has picked up its pace, with the pandemic highlighting the role of technology, such as the Internet of Things, artificial intelligence, robotics and big data. To adapt and thrive, automation industries must accelerate and transform with more resilient, reliable and agile power solutions.

In Phoenix Contact, we have a comprehensive range of technologically leading products, ensuring your system and machine power reliability.

SPDs with effective power surge protection
Market leading power supplies for superior system availability
Device Circuit Breakers protect system devices from fault current

True power reliability is putting together the technologically leading products, with specialized, well-coordinated features and meeting customer application needs in 4 main key different aspects.

Continuous Power – Market leading power supplies solutions to safeguard control system with seamless operation. Examples include AC & DC Uninterruptible power supplies (UPS), battery-less UPS, and redundancy power.

DC & AC Uninterruptible Power Supplies / Redundancy Power Supplies

Robust Protection – The power solution works reliably in harsh operating environments. For example, during electrical power surges & over-currents, mechanical shocks, vibrations, extreme climatic temperatures and dusty operating conditions.

Power SPDs / IP67 Power Supplies / Device Circuit Breakers

Energy Efficient – Reliable products featured with high MTBF, long lifetime expectancy, energy savings and are environmentally friendly.

Intelligent Monitoring – Market-leading innovative products, enabling the smart connected power solution with preventive, predictive info.

Surge Monitoring-Impulsecheck / UPS – Intelligent IQ / Device Circuit Breaker (IO-link)

We aim and strive to help our customers to embrace the ‘new normal’ for their systems, and ensure their machines’ maximum availability.

Contact us now. Your trusted partner for reliable power.

Phoenix Contact Bluetooth

From |

Wireless connectivity replacing rotary slip ring technology

The Rotary Slip Ring is the oldest technology used to transfer power and signals between stationary and rotating structures/equipment. The Rotary Slip Ring allowed free rotation even when the rotating side was at high speeds. Many machines that involve rotation movement, for example in the cable, packaging, paper & tissue industries have utilized slip ring to transmit & receive power and signals.

Rotary Slip Ring is made up of stacks of several rings which are normally made from copper in the rotary side, with a carbon brush touching the ring on the fixed side. This combination allows electricity to flow between the fixed side and the rotating side.

Rotary Slip Ring technology was the only solution in the past for transferring power & signals from rotating equipment, but at the same time, it also brought about the consequences of higher maintenance effort & cost.

The carbon brushes will erode during the operation and need to be replaced regularly. Any impurities such as dust and oil on the surface of the ring will caused greater resistance or even will prevent electrical current from flowing.

Signal transmission requires a stable and constant flow of electrical current. Due to this reason, the digital signal will have a pulse effect when impurities are present and analog signal will have a voltage/current drop.

Factoryline Bluetooth EPA in combination with ILC series can become the solution to these problems. Signal transmission from the rotary slip ring can easily be retrofitted with a short implementation time. Customers can forget about maintenance and the analog & digital signal will flow seamlessly 24/7.

The Bluetooth EPA modules enable fault-free parallel operation with other WLAN systems, thanks to efficient use of frequency gaps. In addition to the automatic coexistence mechanism of Bluetooth, the EPA modules also offer the following:

  • Low emission mode: for low interference emissions when establishing connections
  • Black channel listing: allows configuration of up to three WLAN channels whose frequency ranges will not be used by the EPA module

The Ethernet port adapter is the simple solution for enabling the Bluetooth capability of industrial automation devices with Ethernet connection quickly and easily. The IP65 turnkey solution is installed directly in the field and connected to the automation device via an M12 Ethernet cable.

Your advantages:

  • Compact IP65 module with integrated antenna
  • M12 connections for Ethernet and power
  • Easy installation in the field

Axioline E – fast, robust, easy

Axioline E is the I/O system with a block design for field installation. Open to all Ethernet-based communication protocols and available in two different housing versions, Axioline E offers maximum flexibility.

The SPEEDCON fast locking system ensures quick and

easy installation, thereby minimizing assembly times. Axioline E is particularly robust when it comes to mechanical loads, EMI, and environmental influences. The M12 power connector simplifies installation thanks to the reduced number of terminal points and 2 x 12 A in just one cable.

Extend Axioline E in a distributed and flexible way in the field using IO-Link I/O boxes.

If you would like to find out more, feel free to contact us!

T-LOX – The new dimension in power transmission

From |

Device connection for high currents

Device connection for high currents

Improve efficiency and productivity is a common mission all companies want to achieve.  A company with high efficiency can produce more results while maintain it’s overhead, thus increase its profit margin. Through a switch of screw to spring connection technology,  it is possible to achieve the desired result.

Let’s take a look at the connectivity trends, the demand for quick-connection technology is steadily growing. Today, the spring-cage-based connection technologies allow convenient conductor connections within seconds, and the defined contact force makes them safe as well. In addition, terminal failure due to improper torque can be avoided this way. Until now, there is no device connection with quick-connection technology for cross sections of more than 35 mm².

https://youtu.be/vyOhe1wVD_c

The panel feed-through terminal blocks TW 50 and TW 95 with the new T-LOX connection technology from Phoenix Contact, connectivity has been comes simple and convenient. It even can support multi-strand connectors still ensuring a flexible and safe connection. The T-LOX connection principle is based on a spring that generates a programmed contact force with just a conventional screwdriver.

TW 50 TW 95
Cable Cross-section 16 mm² – 50 mm² 25 mm² to 95 mm²
Current capacity Up to 150 A Up to 232 A
Voltage capacity Achieve a voltage of 1000 V according to IEC 60947-7-1 and unlimited 600 V UL approval in Use Group C according to UL 1059.
Wall thickness 1 mm to 5 mm 1 mm to 5 mm

To find out more about our TW 95, click here

A Glass of Beer

From |

Picture the following scenario. It’s a hot and sunny day and the weather is absolutely scorching. Just then, you are offered 2 glasses of beer – one foamy and one non foamy.

Which glass of beer would you choose?

beer3

Continue reading