Tag Archives: modbus

Photovoltaic Monitoring System With Visualisation – A Project with ITE College East

From |

Photovoltaic (PV) Monitoring System With Visualisation

The Photovoltaic (PV) monitoring system was designed to monitor the performance of the PV panels’ output versus the temperature on the PV panel. There were two different types of PV panels used for monitoring, namely the mono-crystalline and amorphous silicone (Thin Film). The data that was collected were the DC output and the temperature on the PV panels.

Continue reading →

New String Current Monitoring Increases Efficiency of Photovoltaic Installations

From |

The new Solarcheck monitoring system from Phoenix Contact is a new reliable instrument for monitoring string currents in large-scale photovoltaic installations. The easy-to-integrate system detects losses in power caused by dirty or damaged panels. This enables targeted remedial measures to be taken so as to increase system availability and thus revenues.

Continue reading →