Tag Archives: marking and installation

Easier Maintenance, Easier Troubleshooting with Phoenix Contact

From |

If you were to connect one or more wires, you may simply think of connecting them from one point to another. Well, you can do that technically. However, things could get messier than expected.

Image from: https://www.flickr.com/photos/belleville/59234524/in/photostream/

YES, without any prior planning on how wires are to be connected and a proper design of control cabinet layout, you may face the cable jungle, just like what you see in the photo. If you have to perform maintenance or troubleshooting on the control cabinets, this will possibly be one of your worst nightmares! It’s not only about complexity of your job but also your safety.

Not to worry, we are here to help!

Firstly, terminal blocks could be positioned in your control cabinet layout design. Terminal blocks, as a central termination point between the field wiring, provide you an easy and convenient method to group and/or distribute the wirings. This means terminal blocks could provide you with a neater control cabinet with cables.

The wide product range of terminal blocks can be found in Phoenix Contact and you can choose based on your requirements and standards.

Once terminal blocks are in your control cabinets, you can finally escape from the cable jungle. Troubleshooting should be much easier for you to manage now than ever before.

Image from: https://smartcsm.com/25-of-the-worst-electrical-panels-weve-ever-seen

Do you still think that your control cabinet is messy?

You may see the disorganised cables running around the area unmanaged. It might even look dangerous.

If this is what you see, it’s time to use cable ducts.

Even for cable ducts, Phoenix Contact provides many different types according to different situations and environments. The wide range of cable ducts enable flexible and optimum use of available space in your control cabinets.

Your working space will be significantly less cluttered with the use of terminal blocks and cable ducts now. All you need to do for maintenance and troubleshooting will then be straightforward and trouble-free.

Wait! Don’t bounce off yet! We have one more suggestion for easier maintenance, easier troubleshooting with Phoenix Contact. Let’s do a ‘Spot the Difference’ exercise! Can you find the difference between the two photos below?

Apart from messier layouts, the main difference is missing labels. Did you manage to spot those? During testing and troubleshooting, you may realise that you can’t differentiate the cables, especially when they are routed from same location. The labels will be able to help you figure out where each cable is from just by looking at the control cabinet; you won’t have to manually route back where the cable is from. Labelling not only for the wires but for the terminal blocks and other components will benefit you for your routine maintenance and repairs. Easy identification of all the components will reduce your time and effort on handling the control cabinets.

Phoenix contact has launched a series of marking materials and printers. Our printers are made user friendly with ‘simply easy’ motto. Our marking materials are developed with printing services that are widely available for:

  • Terminal blocks (not limited to Phoenix contact terminal blocks)
  • Wires (self-adhesive, clip type & with binder type)
  • Equipment (control panels, equipment tag, temp resist/proof labels, etc.)
  • Plant markings (warning labels)

Your worries and challenges for maintenance and troubleshooting of your control cabinets can now be tackled with ease.

Transmission and Distribution Industry – Solutions and Products

From |

Phoenix Contact Transmission and Distribution industry has lots of products and solutions tailored for different global industries. Customizing the solution to individual customers’ specific requirements, we discover new innovative solutions.

Reliable, intelligent, future-proof

Highly available systems are based on reliable components that interact seamlessly with one another – just like the components from Phoenix Contact. We use innovative products and sophisticated solutions to help our customers operate highly available systems, implement efficient processes and establish a technical infrastructure that is fit for the digital future.

Electrifying since 1923

We brought the first modular terminal block for power plants to the market nearly 100 years ago. Since then, we have successfully installed these terminal blocks in countless energy industry projects. Together with our customers, we have broken new grounds and driven innovative developments forward time and again. Because as a global market leader in electrical engineering, we want to offer our customers tomorrow’s solutions today.

Testing

Regular device and interface testing are crucial to critical infrastructures, such as energy switching devices. Whether meters, measuring devices, or protective relays – with our special terminals or our pluggable FAME system, you can connect, test, and replace all devices quickly and safely.

Power supply and protection

Station control technology is essential in order to guarantee safe and reliable operation of a substation. Supplying these devices with failsafe voltage, while at the same time protecting them, is one of the most important tasks of the power transmission and distribution system. For this purpose, we offer special power supply units for 24 V DC that can be installed redundantly, and compact device circuit breakers that can be used to protect each function separately. With their broad range of protection, control, and measurement functions, our compact protection and control devices are well-suited for a wide variety of applications.

Remote control

Connecting decentralized process and grid stations in different locations to one central control centre requires the use of modular remote control systems that are capable of utilizing a range of communication protocols. However, to ensure that the connection, evaluation, and parameterization of data remains functional, we offer solutions that can be configured, operated, and maintained safely and economically, and require no programming knowledge. Moreover, these solutions guarantee reliable monitoring and access via a wide range of standardized communication protocols.

Signalling

Annunciator relays are used for reliably signalling danger and operating states in control rooms, in mimic diagrams, and on control panels. Our range of alarms notifies users of a variety of system states clearly, and in good time. Malfunctions and faults are quickly and reliably detected, which in turn allows them to be addressed immediately.

Networking

In times of volatile energy generation and new digital trends, providing a stable energy supply can be challenging. We are here to help you master this challenge, with intelligent technologies for processing and transmission of all relevant data while ensuring compliance with IEC 61850.

Measurement, conversion, and coupling

Isolate, convert, and filter signals and monitor and control processes: our MCR components cover all the tasks required for interference-free signal transmission from sensor level to control level. Discover our energy measuring devices, current and voltage transformers, and relays.

Connecting

Whether in a control cabinet or in the field – the energy industry places a large number of demands on connection technology. It must be as safe and secure as it is durable, and it must also be easy to operate. Connection technology from Phoenix Contact meets these demands, from screw connections, to insulation-displacement contacts, right through to Push-in connections.

Marking

A consistent plant marking system forms the basis for efficient maintenance, repairs and troubleshooting in substations. And we offer comprehensive, uniform system solutions for this purpose: from marking materials to labelling systems all the way to software, all from a single source.

Interested to find out more? Leave us an email at marketing@phoenixcontact.com.sg!