Tag Archives: managed switches

3 Key Reasons Why a Managed Switch Is Required in a Network Topology

From |

Most of us should know that there are 2 main categories of network switches, the Unmanaged Switch & the Managed Switch. However, sometimes we struggle to understand when to use a managed switch.

In this article, we will look at 3 key reasons why a managed switch is required in a network topology. Hopefully, after this, you can make use of these 3 key reasons to identify when a managed switch should be used.

Reason 1 – Building network redundancy

Not every type of network topology provides a redundancy mechanism. And what that means is that they will often have a single point of failure – where if one network switch fails, it will stop the entire network from working. Some examples of network topology without redundancy include Bus, Star and Tree etc.

To provide more than a single point of failure, network topology with redundancy mechanisms such as the Ring, Mesh and Hybrid must be used. Managed Switches can support such network topologies through different network protocols. Examples of the protocols include Media Redundancy Protocol (MRP), Rapid Spanning Tree Protocol (RSTP), etc.

Reason 2 – Acquire and provide data for network diagnostics

As Lord Kelvin puts it, “To measure is to know. If you cannot measure it, you cannot improve it.” Similarly, we need to know the diagnostic data of our network topology, to understand its status and improve it.

A Managed Switch provides important information that can help us to monitor the network topology and call for maintenance before full failure of the system happens. This could be classified as predictive maintenance, which brings great reliability benefits.

Some key diagnostic information includes:

  • Port connection status 
  • Redundancy connection status
  • Power supply status (Interruptions)  

The acquisition of these information could also be achieved through different automation protocols such as MODBUS, Profinet, Ethernet/IP etc.

Reason 3 – Security features

Managed switches offer security features such as user-interface & port security.

A user-interface security prevents any unauthorised access into the switch management and configuration. While port security allows only devices with a registered MAC-address to send and receive data packets through the network switches.

Summary

There are many other applications of Managed Switches, such as the use of Layer 3 & VLAN applications, which are critical for big networks. In Phoenix Contact, we provide a good range of network switches for different applications that you might have. Find out more in the following link or contact us at Phoenix Contact SEA.

FL 2000 Managed Switch for Railway Applications

From |

Highspeed commuter trainFor many years, Phoenix Contact has been a reliable partner of the Railway Industry, supplying products such as Power Supply Unit, Terminal Blocks, Heavy Duty Connectors for railway applications. In the recent years, Phoenix Contact has invested a significant amount of effort to create innovative products such as controllers and ethernet switches for automation applications.

Ethernet-based communication medium/protocols are becoming the norm in modern automation environments. Traditional serial-based communication medium/protocols are unable to support the requirements for transmission speed and data size; especially for time-critical applications.

FL 2000 Managed Switch

Phoenix Contact's FL 2000 Managed SwitchThe new FL 2000 Managed Switch was officially launched in April 2017 during the Hannover Fair. This new series of Ethernet Switch was specifically developed to bridge the gap between simple unmanaged switches and complex managed switches which are already available within Phoenix Contact product portfolio.

In railway applications, data integrity is especially critical to ensure the smooth and safe operations of the system. Transmission distances from various subway station control systems to the main control center are often in the range of kilometers, which conventional copper-based medium cannot handle. The only way to transmit the data over long distance is via Fiber Optic technology.

Our sales team spotted an opportunity to propose our FL 2000 Switch in one of the railway system upgrading project in this region. We managed to overcome several challenges despite facing strong competitions from various industrial giants. The main unique selling points of our FL 2000 Switch that met with approval of the end user and system integrators were:

  • Feature important automation features with attractive price/performance ratio
  • Easy/Flexible Configuration/Setup
  • Comprehensive approvals to meet stringent industry-specific approval requirements
  • Various connection port options: Copper and Fiber Optics; Gigabit network possible

In addition, we are also able provide a bundle offer including our UPS and Power Supply Unit.

If you would like to find out more about our FL2000 switches, check out our website or you can leave us your contact and we will get in touch with you as soon as we can.

Realizing the Potential of the Spare Fiber Core

From |

In a typical fiber installation, laying extra fiber cores as spares is an industry practice. Whenever there is any failure, these spares can be swapped over to form the new ring instead of having to lay new replacement cables. Since these spare cores are already available, wouldn’t it be great if they can be providing a automatic backup ring.

Continue reading

Gigabit Modular Switch Now with Routing Function

From |

The Gigabit Modular Switch from Phoenix Contact now also supports the layer 3 function in order to route communications between individual subnetworks.

As industrial networks are becoming increasingly more complex, it makes sense to segment them and split them up into different networks in order to secure the appropriate level of data availability.

Continue reading