Tag Archives: iecex

ATEX & IECEx Comparison

From |

ATEX and IECEx are common standards for equipment intended for use in potentially explosive atmospheres.

Phoenix Contact has a wide range of products that are certified according to IECEx and ATEX standards.

At a glance, both standards seem similar, but there are still some significant differences between ATEX and IECEx.

Comparison between ATEX & IECEx

  IECEx ATEX
Acceptance Global Europe Countries
Organisation Industry Representative

 

Standard Driven

E.U. Commission

 

Law Driven

Conformity Assessment Third certification party certify all products with IECEx Test Report (ExTR) and IECEx Quality Assessment Report (QAR).

 

Self-certification not permitted.

Declaration of conformity by manufacture required. For equipment category 1 and 2, certificate for Ex Notified Body required.

 

Self-certification allowed for equipment category 3.

Marking Equipment group & equipment category not present in the marking.

 

 

Example

Equipment group & equipment category defined in the marking.

 

 

Example

Field of application – Electrical and Non electrical products and systems

 

– Gas / Dust Industries

– Equipment & Service Industries e.g. Repair and Overhaul

– Electrical and Non electrical products and systems

 

– Gas / Dust Industries

– Equipment only

Want to find out more? Feel free to contact us at marketing@phoenixcontact.com.sg!

CLIPSAFE – Your one-stop junction box solution

From |

The “Blame Game”

Have you ever been bothered by such a situation?  Picture this, you have just completed your run on a beautiful day only to return home and realize that your feet are full of blisters. Should you put the blame on the shoe manufacture for using a material that is too tough, or would you blame the socks company for using a material that is too soft?

shoes

Things can potentially get uglier when it comes to planning for or executing a project. Have you had the unfortunate experience of opening a ‘Brand X’ junction box, to find yourself having ‘Brand A’ terminal blocks and maybe some ‘Brand C’ cable glands or markings inside. If there is a fault, who you should go to?

You may potentially find yourself being trapped in the “Blame Game” if you are having two or more different suppliers involved.  And if you have ever been trapped in one, you will know that the chances of successfully finding a solution and getting out is very minuscule.

What if there was a supplier who could provide you with a one-stop shopping experience?

CLIPSAFE – Your one-stop junction box solution

Over the years, many of our customers have requested Phoenix Contact to provide one-stop services where they not only purchase standalone components but are able to purchase a solution. We realized it made perfect sense for us to develop a portfolio of “basket or box” which would allow us to further improve our customers’ buying experience. This was the genesis of our CLIPSAFE range of junction boxes.

CLIPSAFE family of boxes

CLIPSAFE Family

 

As we all know, a junction box is just like the body. A healthy body needs a healthy heart – the components to be installed in the junction boxes. With more than 92 years of component manufacturing experience, you are assured we have maintained, and improved, on the quality of our ‘hearts’ over the past 9 decades.

Phoenix Contact’s CLIPSAFE junction boxes offer you the flexibility in choosing various hassle-free solutions.

Ex and NEMA 4X junction boxes equipped according to customer specifications

You can obtain CLIPSAFE enclosures fully equipped with terminal blocks and cable glands on request. Terminal boxes are delivered with the corresponding equipment approval in accordance with ATEX and IECEx for use in potentially explosive areas.

Steel CLIPSAFE box

CLIPSAFE Hi-grade Steel

 

Ex control boxes according to customer specifications

Individual control boxes with electronic components are available on request. With detailed engineering and planning, we will be able to support you in any complicated field-bus or control boxes requirements.

CLIPSAFE Control Box - Steel

CLIPSAFE Control Box – Steel

Empty Enclosure Ex or NEMA 4X

Still unable to make up your mind as to which components need to be installed in your junction boxes? Fret not.

You can always maintain the flexibility to design and assemble your own components as required by selecting our CLIPSAFE empty boxes.

Choose the right junction box housing for your application; from Stainless Steel to GRP material. We have more than 140 Ex-approved and NEMA 4X versions. Custom dimensions and surface treatments for Stainless Steel are available on request. The delivery is carried out with the corresponding components’ approval in accordance with ATEX and IECEx.

CLIPSAFE Empty Box - Steel

CLIPSAFE Empty Box – Steel

Empty Ex or NEMA 4X enclosure machined to customer specifications

Simply means junction boxes with pre-treated holes and cut outs. We adapt the housing to your request to include threads, drilled holes and rectangular cutouts while taking into account Ex-standards in accordance with ATEX and IECEx. The delivery is carried out with the corresponding components’ approval.

Empty box with flange plates and cover

Empty box with flange plates and cover

With all four types of CLIPSAFE offers, Phoenix Contact believes we will be able to address your needs. Not to forget, a good solution always comes with good quality and design. Do check out our CLIPSAFE Quality and Introduction videos below!

https://youtu.be/n9sEkLNADOQ

Safe Wireless Installation for Hazardous Areas

From |

a_0064853_intWireless technology has improved by leaps and bounds over the last decade. Intermittent, unstable and slow wireless connections are gradually becoming a thing of the past. At the same time, wireless technology brings about tremendous convenience to everyone, reducing clutter caused by messy wires and making hard to reach places reachable. Continue reading

Stainless steel housing for the ex area

From |

The new Clipsafe stainless steel empty housing and terminal boxes from Phoenix Contact are suitable for use in extreme conditions. The 140 robust ATEX and IECEx-approved standard housings are available as door or cover versions in nine depths with sizes up to 1000 x 1000 x 300 mm and provide comprehensive protection for applications in industrial environments and in process technology.

freistellen mit Pfad CD-Inlay einbauen Network Interfaces fg

Designed with practicality in mind, the door stop can be changed to suit the specific installation situation. The same applies to the mounting bracket. The special door and cover seal ensures a secure seal, even after opening multiple times. At the same time, the seal support forms a drainage channel which reliably prevents the ingress of moisture and dirt. A door opening angle of 135° ensures comfortable work in case of service and maintenance. Flange plates are possible on four sides of the housing with patented seal protection and captive mounting screws.

The Clipsafe empty housing is completely equipped with terminal blocks and cable glands according to customer requirements and customized with threads, bore holes, and rectangular cut-outs.

EX Pluggable Fuse & Knife Disconnect Terminal Blocks

From |

Introducing the new EX Pluggable Fuse and Knife Disconnect Terminal Blocks from Phoenix Contact. Do you require it for your applications and systems?

The checklist below will help you decide!

  • Explosive Area application?
  • Corrosion free component needed for robust application?
  • Limited Space?
  • Complicated design and needed flexibility if design changes?
  • The clock is clicking and rushing for project completion?

If you have answered Yes to most of the questions above, then you must read more!
Continue reading

Universal Temperature Transducer with Switching Outputs

From |

Phoenix Contact’s new universal temperature transducers belonging to the MACX Analog family of isolating amplifiers have been developed and produced in accordance with the functional safety standard in all steps of the product lifecycle. The modules include a signal input for a resistance thermometer, thermo elements, resistance-based transmitter, potentiometer, millivolt sources, as well as for customer-specific characteristics.

Continue reading